12.1. Common Errors
Each entry gives the symptom (message text as produced by the code), the cause and the fix. Messages marked “from a 1.5.0 test run” were captured from the ModelMaker functional test logs; the others were checked against the source code.
12.1.1. Setup and configuration
12.1.1.1. Unknown model name
Symptom
ValueError: could not find pretrained model for <model_name>
Cause training.model_name is not in the enabled_models_list of any model description. Only the listed
models are selectable, so an older 1.4.0 name, a typo, or a model you defined but did not enable gives this error. The
lookup is case sensitive.
Fix Use a name from Model Zoo Reference. For your own model either set
training.custom_model_path to a .py file that defines a class with that name, or add it to the description
file and to enabled_models_list, as described in Bring Your Own Model (BYOM). If you already set
custom_model_path and still get please check if the given model_name is a supported one, the installed
tinyml-modelmaker predates that option. A related error is
task_type: <x> does not match the pretrained model: the model belongs to a different task than
common.task_type.
12.1.1.2. Custom model file (custom_model_path) errors
Symptom
training.custom_model_path does not exist or is not a file: /path/to/my_model.py
ValueError: BYOM: model 'MyModel' not found in '/path/to/my_model.py'. Define a class named 'MyModel' or a get_model() function in that file.
UserWarning: BYOM model 'MyModel' __init__ did not accept variables/num_classes/input_features kwargs. Instantiating with no arguments.
Cause The first message means the path is wrong (use an absolute path). The second means the file has no class
whose name equals training.model_name (the match is exact and case sensitive). The warning means a plain
torch.nn.Module has an __init__ that does not take variables, num_classes and input_features, so it was
built with no arguments and the model will not fit your data.
Fix Correct the path or the class name. Declare
def __init__(self, variables=1, num_classes=2, input_features=512, **kwargs). The model must return
(batch, num_classes). If the run instead stops with
please check if the given model_name is a supported one: <name>, the installed tinyml-modelmaker predates
custom_model_path; update it. See Bring Your Own Model (BYOM).
12.1.1.3. Python 3.11 or newer cannot compile
Symptom Training runs, but the compilation step fails with an import error for the TI compiler package
(ti_mcu_nnc / tvm), or pip did not install it.
Cause ti_mcu_nnc is only published for Python 3.10 (cp310 wheels). The dependency has the marker
python_version < '3.11' in tinyml_modelmaker/pyproject.toml, so on Python 3.11 to 3.14 everything else installs
(requires-python = ">=3.10,<3.15") but the compiler does not.
Fix Create a Python 3.10 environment for the whole flow (see Installation). If you only need training and ONNX export, newer
Python versions work; set compilation.enable: False.
12.1.1.4. No examples/ folder after a wheel install
Symptom ./run_tinyml_modelzoo.sh examples/... or examples/<name>/config.yaml does not exist.
Cause The wheel (pip install ...tinyml_modelzoo-1.5.0-py3-none-any.whl) installs the Python package only. The
examples and the run_tinyml_modelzoo scripts are in the Git repository.
Fix Either clone https://github.com/TexasInstruments/tinyml-modelzoo and run pip install -e . there, or run
your own YAML directly with the ModelMaker entry point:
python -m tinyml_modelmaker.run_tinyml_modelmaker config.yaml
See Wheel Installation.
12.1.1.5. Compiler tools not found (TOOLS_PATH)
Symptom Training and testing succeed, then compilation fails because the cross compiler cannot be run
(for example the cl2000, c29clang or tiarmclang binary is missing). The exact text comes from the
compiler step and is not produced by ModelZoo code, so it varies.
Cause ModelMaker looks for the TI code generation tools in $TOOLS_PATH (default ~/ti). The folder names
expected in 1.5.0 are ti-cgt-c2000_25.11.1.LTS (C28x), ti-cgt-c29_2.2.1.LTS (C29x) and
ti-cgt-armllvm_5.1.1.LTS (MSPM0 and other Arm targets); see ai_modules/timeseries/constants.py. Each root can be
overridden with C2000_CG_ROOT, CG_TOOL_ROOT and ARM_LLVM_CGT_PATH.
Fix
export TOOLS_PATH=$HOME/ti # folder that contains the ti-cgt-* folders
ls $TOOLS_PATH
Install the compiler for your device family and use the exact versions above. See Environment Variables.
12.1.2. Training
12.1.2.1. NaN or infinite loss
Symptom (from a 1.5.0 test run, motor bearing fault anomaly detection for MSPM0)
RuntimeError: Training encountered NaN/Inf loss at Epoch 0. This indicates training instability.
Common causes and fixes:
1. Learning rate might be too high, try reducing learning_rate
2. Batch size might be too large, try reducing batch_size
Cause The loss became NaN or Inf during training. 1.5.0 stops immediately instead of continuing.
Typical causes are a too high learning rate, unnormalized inputs, or a feature extraction chain that overflows.
Fix Lower training.learning_rate, reduce training.batch_size, check the dataset values and the feature
extraction settings (Feature Extraction).
12.1.2.2. Training stops before all epochs
Symptom
Early stopping at epoch <N>: no improvement for <patience> epochs.
Cause Early stopping is on by default in 1.5.0 (training.early_stopping: True, patience 5, min delta 0.0).
This is not an error.
Fix To train all epochs set early_stopping: False; to be less strict increase
early_stopping_patience or set a small early_stopping_min_delta. See Early Stopping.
12.1.2.3. ONNX export fails at AdaptiveAvgPool
Symptom ONNX export stops with a PyTorch message of the form
Unsupported: ONNX export of operator adaptive_avg_pool2d, output size that are not factor of input size
(wording depends on the PyTorch version).
Cause In a custom model, AdaptiveAvgPool2d (AdaptiveAvgPoolLayer in the spec layers) can only be
exported when the input height is a multiple of the output size. For example, with output_size=(4, 1) the input
height must be a multiple of 4. This often happens when pooling layers pad the height (for example 256 to 129 to 65).
Fix Use padding=(0, 0) on the pooling layers or change the layer sizes so the height stays a multiple of
the output size. Worked example: Bring Your Own Model (BYOM).
12.1.2.4. QAT: scale and zero-point dimension error
Symptom (from a 1.5.0 test run, DC arc fault anomaly detection config_anomaly_detection_dsk.yaml)
RuntimeError: dimensions of scale and zero-point are not consistent with input tensor
The traceback ends in tinyml_torchmodelopt/quantization/base/fx/fake_quant_types.py (forward), calling
torch.fake_quantize_per_channel_affine.
Cause Known 1.5.0 failure in quantization-aware training of the anomaly detection model used by that config. It was observed in test logs; the root cause was not analyzed here.
Workaround Train the float model and quantize later with PTQ (training.quantization_method: PTQ), or set
training.quantization: 0. Check the release notes of a newer version for a fix.
12.1.2.5. QAT: tensors on different devices
Symptom (from a 1.5.0 test run, generic anomaly detection with an NPU model)
RuntimeError: Expected all tensors to be on the same device, but got scale is on cpu, different from other tensors on cuda:0 (when checking argument in method wrapper_CUDA__fake_quantize_per_channel_affine_cachemask)
Cause Known 1.5.0 failure: the quantization scale tensor stays on the CPU while the model runs on CUDA during QAT.
Workaround Run on CPU with training.num_gpus: 0 (and training_device: cpu). On a CUDA machine this also stops the
automatic compile_model / native_amp switch-on.
12.1.2.6. Dataset download: File is not a zip file
Symptom (from a 1.5.0 test run, hvac_indoor_temp_forecast)
zipfile.BadZipFile: File is not a zip file
raised in utils.extract_files (download_utils.py).
Cause The file downloaded to common.download_path (default ./data/downloads) is not a valid zip, for
example an HTML error page from a proxy, a failed or partial download, or a wrong URL.
Fix Delete the file in data/downloads, check the network or proxy, and re-run. For a local dataset set
dataset.input_data_path to the extracted folder.
12.1.2.7. IndexError: list index out of range when loading the dataset
Symptom (from a 1.5.0 test run, bms_soc_estimation for MSPM0)
list_to_load = glob(joined_path)[0]
IndexError: list index out of range
Cause The dataset loader looks for a file list (train/validation/test list) with glob and found none. The
dataset folder does not have the expected layout, or the split lists were not created.
Fix Check the dataset layout for your task (Bring Your Own Data) and that dataset.dataset_path or
input_data_path points to the right folder. Delete a half-created data/projects/<project>/dataset folder and
re-run.
12.1.3. Compilation and model design
12.1.3.1. NPU layer constraint violations
Symptom Compilation for an NPU device (F28P55, AM13E2, MSPM0G5187) fails or falls back to the software path with a message from the TI neural network compiler about a layer that is not supported by the NPU. The exact text comes from the compiler and depends on its version.
Cause NPU models must follow layer rules: channels in multiples of 4, kernel height limits, fully connected input of at least 16 features (8-bit), and others.
Fix Use a model whose name ends in _NPU (see Model Zoo Reference), or adapt your model with
NPU Configuration Guidelines for TI Neural Network Compiler. To compile an NPU device model with the software NPU, use
compilation.compile_preset_name: forced_soft_npu_preset.
12.1.3.2. Golden vector mismatch on the device
Symptom The output of the model in the SDK example differs from the golden vectors generated by the run.
Cause Usual reasons: the four generated files (model, feature extraction, test vectors) come from different runs,
the SDK example uses different feature extraction settings or input scaling, or the quantization output type
(output_int) does not match the code reading the result.
Fix Copy all generated files from the same run folder and follow Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check). Check the deployment pages for your task, for example Project Compilation Guide: Timeseries Classification Examples.
12.1.4. Platform
12.1.4.1. macOS (Apple Silicon, MPS)
Symptom Training on a Mac is slow, or an operator is reported as not implemented for the MPS device.
Cause The MPS backend does not implement every operator. ModelMaker sets PYTORCH_ENABLE_MPS_FALLBACK=1 by default
(run_tinyml_modelmaker.py), so unsupported operators run on the CPU, which can be slower. torch.compile on MPS
uses the aot_eager backend.
Fix If MPS causes trouble, set training.training_device: cpu. Update to the latest PyTorch that the wheel
allows. See macOS Setup.
12.1.5. Other tips
ModuleNotFoundErrorfortinyml_modelmaker,tinyml_tinyverseortinyml_torchmodelopt: reinstall withpip install -e .from thetinyml-modelzoofolder, or reinstall the wheel. No other repository needs to be installed. The older multi-repository install is no longer used.Out-of-memory on GPU: reduce
training.batch_size, or run withnum_gpus: 0.