7.10.3. Generic Timeseries Forecasting
A “Hello World” introduction to timeseries forecasting with Tiny ML ModelZoo, using a simulated thermostat dataset.
Example folder: examples/generic_timeseries_forecasting
(GitHub)
7.10.3.1. Overview
Task: timeseries forecasting (
generic_timeseries_forecasting), predict future values from past valuesDataset: simulated thermostat, room temperature controlled by an ON/OFF heater with hysteresis
Device: F28P55 (
config.yaml)Model:
FCST_LSTM10(single-layer LSTM with hidden size 10, 542 trainable parameters according to the readme)
7.10.3.2. The Dataset
The heater turns ON when the temperature drops below 20 C and OFF when it rises above 24 C. Because of thermal inertia the temperature oscillates gradually, which makes it a good first forecasting problem.
Column |
Description |
|---|---|
|
Time index |
|
Room temperature in degrees C |
The split is 10 training files (thermostat_01.csv to thermostat_10.csv), 2 validation files
(thermostat_11.csv, thermostat_12.csv) and 3 test files (thermostat_13.csv to
thermostat_15.csv). Each file has 1000 time steps. The config downloads
https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/generic_timeseries_forecasting.zip automatically.
7.10.3.3. Dataset Format
Forecasting always requires annotation files that assign each file to the train, validation or test set.
The data folder is named files.
{dataset_name}.zip/
|
|-- files/
| |-- {file1}.csv
| |-- {fileN}.csv
|
|-- annotations/
|-- file_list.txt
|-- instances_train_list.txt
|-- instances_val_list.txt
|-- instances_test_list.txt
To use your own data, see Forecasting Dataset Format.
7.10.3.4. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from
the tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/generic_timeseries_forecasting/config.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\generic_timeseries_forecasting\config.yaml
7.10.3.5. Configuration
common:
task_type: generic_timeseries_forecasting
target_device: F28P55
dataset:
dataset_name: generic_timeseries_forecasting
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/generic_timeseries_forecasting.zip
data_processing_feature_extraction:
data_proc_transforms:
- SimpleWindow # mandatory for forecasting
frame_size: 32
stride_size: 0.1
forecast_horizon: 2 # number of future time steps to predict
variables: 1 # only the temperature column (after the timestamp)
target_variables:
- 0 # column index 0 = temperature
training:
model_name: FCST_LSTM10
model_config: ''
batch_size: 32
training_epochs: 50
early_stopping: true
early_stopping_patience: 5
num_gpus: 0
quantization: 2
optimizer: adam
output_int: false
testing: {}
compilation: {}
Key points for forecasting configs:
SimpleWindowmust be indata_proc_transformsandframe_sizeis mandatory.stride_sizeis a fraction of the frame size andforecast_horizonis the number of future steps.variablesis the number of input columns after the time column.target_variablesselects what to predict. It accepts a list of column indices (0-based after the time column), a list of column names, a single index or name, a comma-separated string of names, or an empty list to predict all columns.output_intmust befalsefor forecasting.Feature extraction is not supported for forecasting.
7.10.3.6. Evaluation Metrics
SMAPE (symmetric mean absolute percentage error): percentage error normalized to avoid bias toward large or small values. Range 0% to 200%, lower is better.
R2 score: how well predictions match actual values. Range (-infinity, 1], higher is better.
For each epoch SMAPE is computed across all target variables and all predicted time steps; the epoch with the lowest average SMAPE is the best epoch. R2 and SMAPE are reported per time step of each target variable.
7.10.3.7. Results
The example readme reports these float-model results (best epoch 48 in that run):
Metric |
Timestep 1 |
Timestep 2 |
Overall |
|---|---|---|---|
SMAPE |
0.60% |
0.88% |
0.74% |
R2 |
0.9811 |
0.9563 |
0.9687 |
Warning
Quantized accuracy is not reliable in the current release. The readme lists quantized results close to the
float ones, but in the automated 1.5.0 config test run (short, early stopped) the quantized
FCST_LSTM10 model reached only an R2 of 0.74 and a SMAPE of 2.23% on the validation set and a
test SMAPE of about 12.9%, far worse than the float model. Always compare the float and quantized results
in your own run before deploying.
7.10.3.8. Output Location
Results are written to ./data/projects/generic_timeseries_forecasting/run/<date-time>/FCST_LSTM10/.
training/base/best_epoch_<n>_results: float model best epoch resultstraining/quantization/best_epoch_<n>_resultsandtraining/quantization/test_results: quantized modelcompilation/artifacts/:mod.aandtvmgen_default.h
See Understanding the Run Output for details.
7.10.3.9. Running on Device
Follow Deploying Forecasting Models from ModelMaker to Device.
7.10.3.10. Next Steps
PMSM Rotor Temperature Forecasting: real-world motor temperature forecasting
HVAC Indoor Temperature Forecasting: indoor temperature forecasting
Forecasting Dataset Format: use your own forecasting data