8.12.3.15. Integer Model Configuration: Deep Dive

8.12.3.15.1. Table of Contents


8.12.3.15.2. 1. Overview

integer_model_config.h and integer_model_config.c are the two auto-generated files that fully describe your model to the integer ODT C library. Together they contain:

  • All INT8 weights and INT32 offsets extracted from the QAT ONNX

  • Static buffers for activations, ReLU masks, and gradient ping-pong

  • Layer descriptors connecting every buffer and array pointer

  • The IntModelCtx_t context struct that the three public API functions operate on

After these files are compiled into your project, you never need to initialize or configure the model. INT_MODEL is statically initialized and ready to use immediately.


8.12.3.15.3. 2. integer_model_config.h

#ifndef INTEGER_MODEL_CONFIG_H
#define INTEGER_MODEL_CONFIG_H

#include "integer_odl.h"

The header always includes integer_odl.h so that IntLayerDesc_t, IntModelCtx_t, and IntLayerType_t are in scope everywhere integer_model_config.h is included.


8.12.3.15.3.1. IS_FULL_MODEL_RETRAIN

#define IS_FULL_MODEL_RETRAIN  1   // 1 = full model, 0 = partial model

Tells main.c how the model is split:

  • 1 (full model): TVM outputs INT8 to the C library. In main.c, pass raw float training inputs directly to TVM; TVM does the quantization.

  • 0 (partial model): TVM outputs UINT8 to the C library. In main.c, similarly pass raw inputs to TVM, but TVM runs the frozen compute layers too before passing UINT8 to the C library.

Your main.c can use this define to branch behavior, or always pass floats to TVM and let TVM handle the type conversion. The difference is how much computation TVM does before the C library takes over.


8.12.3.15.3.2. INPUT_SIZE

#define INPUT_SIZE  128

The flat size of one raw input sample before feature extraction.


8.12.3.15.3.3. FROZEN_OUTPUT_SIZE

#define FROZEN_OUTPUT_SIZE  128

The size of TVM’s output, the input to INT_LAYERS[0]. For full model ODT where TVM only does PREQUANT, this equals the PREQUANT output size, which is the same as INPUT_SIZE. For partial model ODT, this is the spatial size of the last frozen layer’s output.


8.12.3.15.3.4. N_CLASSES

#define N_CLASSES  2

Number of output classes, equal to INT_LAYERS[N_INT_LAYERS-1].out_size.


8.12.3.15.3.5. BATCH_SIZE

#define BATCH_SIZE  8

How many samples are processed together in one forward+backward call. All act_buf, relu_mask, and grad_buf static arrays are sized as BATCH_SIZE * element_count.


8.12.3.15.3.6. TARGET_MAG_CORRECT and TARGET_MAG_WRONG

static const int8_t TARGET_MAG_CORRECT[N_CLASSES] = {  24,  20 };
static const int8_t TARGET_MAG_WRONG[N_CLASSES]   = { -31, -28 };

These are the per-class loss targets derived from the model’s actual output distribution. They answer: “what does the model typically output for class c when the input belongs to class c (CORRECT), and when it belongs to some other class (WRONG)?”

How to interpret them:

  • TARGET_MAG_CORRECT[0] = 24: when a class-0 sample is correctly classified, logit[0] is typically ~24

  • TARGET_MAG_WRONG[0] = -31: when a class-1 sample is misclassified, logit[0] is typically ~-31

The loss function computes gradient = logit - target and pushes each logit toward its target.


8.12.3.15.3.7. MU_WEIGHT_DEFAULT and MU_OFFSET_DEFAULT

#define MU_WEIGHT_DEFAULT  1
#define MU_OFFSET_DEFAULT  1

Initial NITI learning rate parameters. Written into INT_MODEL.mu_weight and INT_MODEL.mu_offset at initialization.

You can change these at runtime in main.c after initialization:

See Overview: The NITI Algorithm for the effect of different mu values.


8.12.3.15.3.8. N_TRAINABLE_LAYERS

#define N_TRAINABLE_LAYERS  3

N_TRAINABLE_LAYERS: Number of trainable layers


8.12.3.15.4. 3. IntLayerDesc_t: Layer Descriptor Structure

Each entry in INT_LAYERS[] is an IntLayerDesc_t. Here is the complete structure from integer_odl.h:

8.12.3.15.4.1. 3.1 Common Fields

typedef struct {
    IntLayerType_t type;    // Layer type enum
    uint16_t       in_size; // Flat input element count (per sample, excluding batch)
    uint16_t       out_size;// Flat output element count (per sample, excluding batch)
    int32_t        clip_lo; // Lower bound for output saturation (from ONNX Clip node)
    int32_t        clip_hi; // Upper bound for output saturation (from ONNX Clip node)
    void    *act_buf;       // [BATCH_SIZE * out_size] activation buffer
    uint8_t *relu_mask;     // [BATCH_SIZE * ceil(out_size/8)] bitmask; NULL if no ReLU
    union { ... };          // Layer-type-specific parameters
} IntLayerDesc_t;

type, one of:

INT_LAYER_PREQUANT    = 0  // float→int8 quantization
INT_LAYER_CONV2D      = 1  // Conv2D with OSS, no ReLU
INT_LAYER_CONV2D_RELU = 2  // Conv2D with OSS + ReLU
INT_LAYER_LINEAR      = 3  // Linear/MatMul with OSS, no ReLU
INT_LAYER_LINEAR_RELU = 4  // Linear/MatMul with OSS + ReLU

8.12.3.15.4.2. 3.2 PREQUANT Sub-struct

struct {
    const float *offset;  // Per-channel offset [n_ch]
    const float *scale;   // Per-channel scale [n_ch] (combined mul1*mul2)
    uint16_t     n_ch;    // Number of channels (1 for global scale/offset)
} prequant;

Not present in INT_LAYERS[] for ModelMaker-generated artifacts, PREQUANT lives in TVM. Present for any future use

8.12.3.15.4.3. 3.3 Conv Sub-struct

struct {
    int8_t       *weights;   // [n_filters × in_ch × kH × kW] flat row-major
    int32_t      *offset;    // [n_filters] per-filter bias — mutable
    const int8_t *mult;      // [n_filters] OSS multiply factor — const, all 1 currently
    const int8_t *k;         // [n_filters] OSS right-shift amount — const
    uint16_t      n_filters;
    uint16_t      conv_out_h;  // output spatial height
    uint16_t      conv_out_w;  // output spatial width
    uint8_t       kH;          // kernel height
    uint8_t       kW;          // kernel width
} conv;

weights layout: [filter_idx, in_ch_idx, krow, kcol] stored contiguously:

weights[filter * (in_ch * kH * kW) + in_ch * (kH * kW) + krow * kW + kcol]

This is standard ONNX/PyTorch Conv2D weight layout.

offset: INT32 per-filter bias.

k: per-filter right-shift. Derived from the ONNX OSS chain as k = round(-log2(|shift_mult|)). For example, if the ONNX Mul constant is 0.03125 = 2^-5, then k = 5. The C forward pass computes (acc + offset[f]) >> k[f]. See Section 5.4.

8.12.3.15.4.4. 3.4 Linear Sub-struct

struct {
    int8_t       *weights;  // [in_size × out_size] row-major — mutable
    int32_t      *offset;   // [out_size] per-output bias — mutable
    const int8_t *mult;     // [out_size] — const, all 1
    const int8_t *k;        // [out_size] — const
} linear;

weights layout: weights[in_idx * out_size + out_idx]


8.12.3.15.5. 4. IntModelCtx_t: Model Context

typedef struct {
    uint16_t        n_layers;
    IntLayerDesc_t *layers;
    int8_t         *grad_buf[2];  // ping-pong delta buffers
    int8_t          mu_weight;    // NITI learning rate for weights
    int8_t          mu_offset;    // NITI learning rate for offsets
    IntInputType_t  input_type;   // INT_INPUT_INT8 or INT_INPUT_UINT8
} IntModelCtx_t;

grad_buf[2]: two int8 buffers for ping-pong use during backward pass. Sized to BATCH_SIZE * max(max_out_size_across_all_layers, layers[0].in_size).

The two-buffer ping-pong works as follows:

  1. Before INTODT_Backward: user writes dy (loss gradient) into grad_buf[0]

  2. Backward processes the last layer: reads from grad_buf[0], writes propagated delta to grad_buf[1]

  3. Backward processes second-to-last layer: reads from grad_buf[1], writes to grad_buf[0]

  4. Alternates until the first trainable layer is processed

During INTODT_Infer, grad_buf[0/1] are used as temporary layer activation storage (since act_buf is not written during inference). The ping-pong buffers are reused across forward and inference, safe because they are never used simultaneously.


8.12.3.15.6. 5. integer_model_config.c: Buffer Layout and Sizing

8.12.3.15.6.1. 5.1 Activation Buffers

Each layer has its own activation buffer, sized at compile time:

// RELU layer → uint8_t (output range [0, 255])
static uint8_t  layer0_act_buf[BATCH_SIZE * output_size];  

// Non-RELU layer → int8_t (output range [-128, 127])
static int8_t   layer2_act_buf[BATCH_SIZE * output_size];

During INTODT_Forward, each sample’s output is written to layer->act_buf + sample_idx * out_size.

During INTODT_Backward, each layer reads its input from layers[layer_idx-1].act_buf

8.12.3.15.6.2. 5.2 ReLU Mask Buffers

RELU layers need a bitmask per output element per sample:

static uint8_t layer0_relu_mask[BATCH_SIZE * ceil(out_size / 8)];

8.12.3.15.6.3. 5.3 Grad Buffers

Two ping-pong grad buffers shared across all layers:

static int8_t grad_buf_0[BATCH_SIZE * MAX_BUF];
static int8_t grad_buf_1[BATCH_SIZE * MAX_BUF];

Where MAX_BUF = max(max_out_size_across_all_layers, layers[0].in_size):

8.12.3.15.6.4. 5.4 Weight and Parameter Arrays

Weight array naming convention: layer{i}_weights, layer{i}_offset, layer{i}_mult, layer{i}_k:

//layer weights — int8_t, mutable (updated by backward)
static int8_t layer0_weights[] = {
    -12,   8,  23, -41,  17, -33,  52, -28,  11, -19,  44, -37,  29, -8,  15, -22,
     33, -14,  -7,  41, -26,  18,  -9,  37, -45,  22,  13, -31,   8, 42, -17,  25,
    ...
};

//layer offsets — int32_t, mutable
static int32_t layer0_offset[] = { 142, -88, 213 };

// OSS multiply
static const int8_t layer0_mult[] = { 1, 1, 1 };

// OSS right-shift amounts 
static const int8_t layer0_k[] = { 9, 8, 9 };

What gets modified during ODT: Only weights and offset arrays. The mult and k arrays are const and remain unchanged for the lifetime of the model.