2.7. Environment Variables
ModelMaker finds the TI compiler tools through environment variables. They are needed only to compile a model for a device; training and quantization work without them.
Warning
Set the variable for your target device before running an example, otherwise the compilation step fails.
2.7.1. How the Paths Are Resolved
Each variable below has a default under TOOLS_PATH. If a variable is unset,
ModelMaker uses <TOOLS_PATH>/<default folder name>.
Variable |
Default |
Purpose |
|---|---|---|
|
|
Parent folder searched for the compilers below |
|
|
TI C2000 CGT ( |
|
|
TI C29 Clang ( |
|
|
TI Arm Clang ( |
|
|
Arm Clang for the xWRL6432 radar device (radar tasks only) |
The defaults are in the constants.py of the ModelMaker modules
(tinyml_modelmaker/ai_modules/timeseries, audio, radar). If you install a
compiler in the default folder name under ~/ti you do not need to set anything.
The compiler versions above are the ones 1.5.0 is built against.
2.7.2. Which Variable for Which Device
Target devices |
Variable |
|---|---|
F28P55, F28P65, F2837, F28004, F28003, other C2000 F28x |
|
F29H85, F29P58, F29P32 |
|
MSPM0G3507, MSPM0G3519, MSPM0G5187, MSPM33C32/34, AM13E2, AM263, AM263P, AM261, CC2755, CC2745, CC1312, CC1314, CC1352, CC1354, CC35X1 |
|
xWRL6432 |
|
See Supported Devices for the full device list.
2.7.3. Setting Variables
Per session, or add to ~/.bashrc / ~/.zshrc for permanence:
export TOOLS_PATH=$HOME/ti
export C2000_CG_ROOT=$HOME/ti/ti-cgt-c2000_25.11.1.LTS
export CG_TOOL_ROOT=$HOME/ti/ti-cgt-c29_2.2.1.LTS
export ARM_LLVM_CGT_PATH=$HOME/ti/ti-cgt-armllvm_5.1.1.LTS
$env:C2000_CG_ROOT = "C:\ti\ti-cgt-c2000_25.11.1.LTS"
# Permanent for the current user:
[Environment]::SetEnvironmentVariable("C2000_CG_ROOT", "C:\ti\ti-cgt-c2000_25.11.1.LTS", "User")
set C2000_CG_ROOT=C:\ti\ti-cgt-c2000_25.11.1.LTS
2.7.4. Installing the Compilers
C2000 CGT: https://www.ti.com/tool/C2000-CGT (version 25.11.1.LTS)
TI Arm Clang: https://www.ti.com/tool/ARM-CGT (version 5.1.1.LTS)
TI C29 Clang: from TI’s compiler download page (version 2.2.1.LTS)
Code Composer Studio also installs compilers under
<CCS_INSTALL>/tools/compiler/; point the variables there.
Install them with the vendor installer to any folder, then either set the variable or
install into ~/ti.
2.7.5. Verifying
$C2000_CG_ROOT/bin/cl2000 --version
$ARM_LLVM_CGT_PATH/bin/tiarmclang --version
2.7.6. Troubleshooting
- Compiler not found during compilation
Check the variable points at the folder that contains
bin/(ls $C2000_CG_ROOT/bin).- Works in a terminal but not from an IDE
The IDE may not inherit your shell variables; set them in its run configuration.
- Other versions
The defaults name specific versions. Other versions may work but are not what 1.5.0 was validated with.
Also, ModelMaker sets PYTORCH_ENABLE_MPS_FALLBACK=1 itself on startup (relevant to macOS; see macOS Setup).