7.10.11. Grid Stability
Predict the small-signal stability of a power grid from node-level parameters.
Example folder: examples/grid_stability
(GitHub)
7.10.11.1. Overview
The dataset comes from the UCI Machine Learning Repository. It is simulation-derived and describes a 4-node “star” network with one central generation node and three peripheral consumer nodes. For each node there are three parameters:
tau1totau4: reaction time of the node (larger values mean slower dynamics)p1top4: active power of the node (generation or consumption)g1tog4: price elasticity coefficient (sensitivity to price or control signals)
The label is stable or unstable.
Application: smart grid, power system operation, renewable energy integration
Task: classification (
generic_timeseries_classification)Device: F28P55 (
config.yaml)Model:
CLS_ResCat_3k
Four-node star network used for the grid stability dataset
7.10.11.2. Preparing the Dataset
The config downloads https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/grid_stability_dataset.zip
automatically. To regenerate the zip from the UCI source, run the helper script and point
dataset.input_data_path at the output (examples/grid_stability/grid_stability_dataset.zip):
cd examples/grid_stability
python grid_stability.py
Because the data is simulated, make sure train and validation splits cover the range of operating conditions and avoid overfitting to narrow parameter ranges.
7.10.11.3. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the
tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/grid_stability/config.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\grid_stability\config.yaml
7.10.11.4. Configuration
common:
task_type: generic_timeseries_classification
target_device: F28P55
dataset:
dataset_name: grid_stability
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/grid_stability_dataset.zip
data_processing_feature_extraction:
data_proc_transforms: ['SimpleWindow']
frame_size: 256
stride_size: 0.01
variables: 6
feature_extraction_name: Custom_Default
training:
model_name: CLS_ResCat_3k
num_gpus: 0
early_stopping: true
early_stopping_patience: 5
testing: {}
compilation: {}
7.10.11.5. Understanding the Outputs
The training/base folder holds the float model and feature data; training/quantization holds the INT8
model and its analysis. The PCA plots show whether the classes separate well in feature space. See
Understanding the Run Output for all generated files.
7.10.11.6. Results from the 1.5.0 Test Run
In the automated 1.5.0 config test run, config.yaml reached a test accuracy of 100.00% with an AUC ROC of
1.000 (CLS_ResCat_3k, 1,018 parameters). The example readme does not publish accuracy numbers.
7.10.11.7. See Also
Electrical Fault: transmission line fault classification