7.10.10. Electrical Fault
Detect and classify transmission line faults from three-phase voltage and current measurements, with a focus on solving the multicollinearity problem of raw voltage and current channels through frequency domain feature extraction.
Example folder: examples/electrical_fault
(GitHub)
7.10.10.1. Overview
The dataset is a multivariate time series obtained by simulating a three-phase transmission line in MATLAB Simulink. The six variables are the phase voltages (Va, Vb, Vc) and phase currents (Ia, Ib, Ic).
Application: power grid protection, substation automation, fault localization
Task: time series classification (
generic_timeseries_classification)Variants: 2-class fault detection (fault / no fault) and 6-class fault type classification
Simulink model used to generate the electrical fault data
7.10.10.2. Dataset Variants
The raw data is available as https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/electrical_fault_raw.zip.
Two helper scripts in the example folder convert it to ModelZoo datasets.
Script |
Output dataset |
Classes |
Use case |
|---|---|---|---|
|
|
2 (fault / no fault) |
Binary fault detection |
|
|
6 (from the G, C, B, A target flags) |
Fault type classification |
The shipped configs already point to pre-built copies of these zip files on the TI download server, so running the scripts is only needed if you want to regenerate the datasets locally:
cd examples/electrical_fault
python electrical_fault.py # creates electrical_fault_dataset.zip
python electrical_fault_6class.py # creates electrical_fault_6class_dataset.zip
Then set dataset.input_data_path to the generated zip, for example
examples/electrical_fault/electrical_fault_dataset.zip.
In the 6-class data the target flags [G, C, B, A] encode the fault type, for example [0, 0, 0, 0] is no fault, [0, 1, 1, 0] is a line-to-line fault between nodes B and C, [1, 0, 0, 1] is a line-to-ground fault at node A, and [1, 1, 1, 1] is a fault involving all nodes and ground.
7.10.10.3. Available Configurations
Config file |
Device |
Model |
Notes |
|---|---|---|---|
|
F28P55 |
|
2-class dataset |
|
MSPM0G5187 |
|
6-class dataset, 3 variables, 128-sample frames, Q15 FFT features (32 per frame, 8 frames), 25 epochs |
7.10.10.4. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the
tinyml-modelzoo folder:
# 2-class fault detection on F28P55
./run_tinyml_modelzoo.sh examples/electrical_fault/config.yaml
# 6-class fault type classification on MSPM0G5187
./run_tinyml_modelzoo.sh examples/electrical_fault/config_MSPM0.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\electrical_fault\config.yaml
run_tinyml_modelzoo.bat examples\electrical_fault\config_MSPM0.yaml
7.10.10.5. Configuration (config.yaml)
common:
task_type: generic_timeseries_classification
target_device: F28P55
dataset:
dataset_name: electrical_fault_2class
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/electrical_fault_dataset.zip
data_processing_feature_extraction:
data_proc_transforms: ['SimpleWindow']
stride_size: 0.01
variables: 6
feature_extraction_name: Custom_Default
feat_ext_transform: ['FFT_FE', 'FFT_POS_HALF', 'DC_REMOVE', 'ABS', 'LOG_DB', 'CONCAT']
frame_size: 256
feature_size_per_frame: 128
num_frame_concat: 1
training:
model_name: CLS_ResCat_3k
num_gpus: 0
early_stopping: true
early_stopping_patience: 5
testing: {}
compilation: {}
7.10.10.6. Multicollinearity and Feature Extraction
Raw phase voltages and currents are strongly correlated (the example readme shows correlation
coefficients of about -0.94 to -0.95 between pairs such as Ia and Vc, or Ib and Va). Training directly on such
channels can fail to find good hyperparameters. Two remedies are to remove highly correlated features, or to
extract features that reduce dimensionality. This example uses the second one: an FFT of each frame
(FFT_FE, FFT_POS_HALF, DC_REMOVE, ABS), an optional BINNING step, LOG_DB and
CONCAT. Spectral features decorrelate the channels because they describe how energy is distributed over
frequencies. The example readme.md walks through the transform options step by step. You can try disabling
the features to see the effect:
data_processing_feature_extraction:
feature_extraction_name: Custom_Default
feat_ext_transform: []
7.10.10.7. Results from the 1.5.0 Test Run
The example readme does not publish accuracy numbers. From the automated 1.5.0 config test run:
Config |
Test accuracy |
AUC ROC |
|---|---|---|
|
99.44% |
1.000 |
|
88.89% |
0.981 |
7.10.10.8. See Also
Grid Stability: power grid stability prediction
Using your own data: Classification Dataset Format