7.10.1. Generic Time Series Classification
This example is the “Hello World” of Tiny ML ModelZoo time series classification. It classifies synthetic sine, square and sawtooth waveforms and shows the complete flow (data, feature extraction, training, quantization, compilation) with the smallest possible configuration.
Example folder: examples/generic_timeseries_classification
(GitHub)
7.10.1.1. Overview
Task:
generic_timeseries_classification(3 classes)Dataset: synthetic waveforms (sine, square, sawtooth), 1 variable
Model:
CLS_1k_NPU(about 1,000 parameters)Default device: F28P55 (NPU)
Training: 20 epochs, batch size 256, early stopping enabled (patience 5)
7.10.1.2. Available Configurations
One configuration file is provided per device family.
Config file |
Target device |
Model |
Feature extraction preset |
|---|---|---|---|
|
F28P55 |
|
|
|
MSPM0G5187 |
|
|
|
CC1352 |
|
|
|
CC1354 |
|
|
|
CC2755 |
|
|
|
CC35X1 |
|
|
The non-C2000 configs use the dataset name hello_world_example_dsg with the input data path
https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/generic_timeseries_classification.zip.
7.10.1.3. Running the Example
Install Tiny ML ModelZoo first (see Installation and Quickstart),
then run from the tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/generic_timeseries_classification/config.yaml
See Running Examples for the .bat and .ps1 launchers, for example:
run_tinyml_modelzoo.bat examples\generic_timeseries_classification\config.yaml
To target another device, pass its config file, for example
examples/generic_timeseries_classification/config_MSPM0.yaml.
7.10.1.4. Dataset Format
For classification tasks, Tiny ML ModelZoo expects the dataset in this structure:
{dataset_name}.zip/
|
|-- classes/
|-- class_1/
| |-- file1.csv
| |-- file2.csv
|
|-- class_N/
|-- ...
Note
The folder names under classes/ become the class labels. No annotation files are required.
See Classification Dataset Format for details.
7.10.1.5. Configuration (config.yaml)
common:
task_type: generic_timeseries_classification
target_device: F28P55
dataset:
dataset_name: generic_timeseries_classification
data_processing_feature_extraction:
feature_extraction_name: Generic_1024Input_FFTBIN_64Feature_8Frame
variables: 1
training:
model_name: CLS_1k_NPU
batch_size: 256
training_epochs: 20
early_stopping: true
early_stopping_patience: 5
num_gpus: 0
testing: {}
compilation: {}
The Generic_1024Input_FFTBIN_64Feature_8Frame preset uses frames of 1024 samples, computes the
FFT, bins it into 64 features per frame and concatenates 8 frames (64 x 8 = 512 features). The config
file also lists, as comments, the other generic presets (..._FFT_..., ..._RAW_...) you can try.
For all keys see How to Create a ModelZoo Config YAML.
7.10.1.6. Output Location
Results are written to ./data/projects/generic_timeseries_classification/run/<date-time>/CLS_1k_NPU/
(relative to where you ran the script; configurable with common.projects_path). The most
important artifacts are the trained model under training/, the quantized ONNX model, and the
compiled artifacts under compilation/artifacts. See Understanding the Run Output.
7.10.1.7. Expected Results
The example readme.md does not publish accuracy numbers. The waveforms are well separated, so
training converges quickly; check the printed test accuracy and confusion matrix at the end of your
own run.
7.10.1.8. Variations to Try
Raw time-domain input:
feature_extraction_name: Generic_512Input_RAW_512Feature_1FrameOther model sizes:
CLS_100_NPU(smaller) orCLS_4k_NPU(larger)Another device: use one of the per-device configs above
7.10.1.9. Next Steps
Try DC Arc Fault Detection for a real-world arc fault detection example.
Use your own data: Classification Dataset Format.
Learn all configuration options: How to Create a ModelZoo Config YAML.