7.10.21. Wi-Fi CSI Presence Detection

Detect human presence from Wi-Fi Channel State Information (CSI) on the CC35X1 Wi-Fi microcontroller. This example is new in 1.5.0.

Example folder: examples/wifi_csi_presence_detection (GitHub)

7.10.21.1. Overview

The model classifies 2-second windows of CSI data into no presence (class 0) and presence (class 1), enabling device-free occupancy sensing without body-worn sensors. PIR sensors need line of sight and miss stationary occupants, whereas Wi-Fi CSI is pervasive, passive and sensitive to the small environmental changes caused by a person even at rest. Threshold based CSI detectors are brittle across rooms and furniture arrangements; a trained model on the Wi-Fi SoC gives always-on, privacy-preserving sensing without extra hardware.

  • Task: binary classification (generic_timeseries_classification)

  • Device: CC35X1 (CC3551E); the model is compiled for the M33 CDE

  • Model: WiFiPresDet_4.7k_CDE (about 4.7K parameters)

  • Data: CSI magnitudes of 52 usable subcarriers at 128 Hz

7.10.21.2. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/wifi_csi_presence_detection/config.yaml

7.10.21.3. Configuration

common:
  task_type: generic_timeseries_classification
  target_device: CC35X1
  run_name: '{date-time}/{model_name}'
dataset:
  dataset_name: wifi_csi_occupancy_detection
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/wifi_presence_detection_dsi.zip
data_processing_feature_extraction:
  feature_extraction_name: WiFiCSI_128Input_L2Norm2DFFT_64x26Feature_1Frame_52Subcarriers
  stride_size: 0.7
training:
  model_name: WiFiPresDet_4.7k_CDE
  batch_size: 32
  training_epochs: 50
  early_stopping: true
  early_stopping_patience: 5
  num_gpus: 0
  learning_rate: 0.00005
  quantization: 2
  auto_quantization: false
  output_int: false
testing: {}
compilation: {}

7.10.21.4. Datasets

All datasets contain CSI recordings at 128 Hz across 52 usable subcarriers (hardware indices 0 to 25 and 27 to 52; index 26 is the DC subcarrier and is excluded). Labels are binary.

Dataset

Description

wifi_presence_detection_dsi.zip

Compact in-house dataset and the default of config.yaml; already preprocessed. Recorded in an indoor conference room below 300 sq ft with a CC35X1 LP receiver and a TP-Link Archer C6 router as transmitter. 400 windows of 2 s per class (800 total); the presence class covers sitting, standing, walking and waving.

wifi_presence_detection_dsd.zip

Larger and more diverse dataset (2 GB+ compressed, over 6.4 million data points, 8 recording days, 13 activity conditions collapsed to binary). Requires preprocess_dsd.py before training.

wifi_presence_detection_dsd_2000.zip

Uniformly sampled subset of the DSD data with 2000 samples balanced between both classes; already preprocessed.

wifi_presence_detection_dsd_4400.zip

Same, with 4400 samples; already preprocessed.

To use the DSD dataset, edit IN_ROOT and OUT_ROOT in examples/wifi_csi_presence_detection/preprocess_dsd.py, run it, and set dataset.input_data_path to the output directory. preprocess_dsd.py skips the first 10 s of each recording, extracts 256-sample (2 s) windows with 30% overlap, resamples them, and assigns the train, validation and test splits by recording date. preprocess.py does the equivalent for raw DSI-style CSV folders (drops metadata columns, resamples each session to 128 Hz).

7.10.21.5. Feature Extraction

The preset WiFiCSI_128Input_L2Norm2DFFT_64x26Feature_1Frame_52Subcarriers converts the 52-subcarrier CSI magnitude windows into a 2-D time-frequency feature map:

Step

Operation

Output shape

1

Downsample 128 Hz to 64 Hz

64 x 52

2

Sliding window (2 s at 64 Hz, stride 0.7)

128 x 52

3

L2 normalize each time step across subcarriers (L2_NORM_ROW)

128 x 52

4

Real FFT along the time axis (FFT_FE)

65 x 52

5

Keep the positive half, drop Nyquist (FFT_POS_HALF)

64 x 52

6

Magnitude (ABS)

64 x 52

7

Log magnitude, log10(1 + abs(F)) (LOG_DB)

64 x 52

8

Real FFT across the subcarrier axis, positive half (FFT_COL)

64 x 26

The final model input per window has shape (1, 26, 1, 64).

7.10.21.6. Results

The example readme reports these results for the DSI dataset (float model 99.17% accuracy, 8-bit weight and 8-bit activation QAT model 99.17%, test set 98.75%, AUC ROC 0.985 on the test set) and, on the test set, 98.85% (DSD), 99.00% (DSD 2000) and 99.50% (DSD 4400). In the automated 1.5.0 config test run, config.yaml reached a test accuracy of 98.75% with an AUC ROC of 0.988.

7.10.21.7. Training and Deployment

Running the config performs feature extraction, training, 8-bit quantization (quantization: 2) and compilation with the TI Neural Network Compiler for the M33 CDE of the CC35X1, producing model.a and tvmgen_default.h for firmware integration. See Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check).

7.10.21.8. See Also