8.1. Feature Extraction

Feature extraction transforms raw sensor data into a representation that helps the neural network learn patterns more effectively. The same transforms run on the PC during training and on the MCU during inference, so training and deployment see identical features.

  • Reduced input size: compress long time series.

  • Better patterns: move to a domain (for example frequency) where patterns are clearer.

  • Faster inference: smaller inputs mean smaller and faster models.

  • Domain knowledge: reuse signal processing expertise.

8.1.1. Pipeline

Raw data flows through two stages, data processing and then feature extraction:

Raw signal --> Data processing --> Feature extraction --> Model input
               (data_proc_transforms)  (feat_ext_transform)
               e.g. SimpleWindow,      e.g. FFT_FE, BINNING,
                    Downsample              ABS, LOG_DB, CONCAT

Important

data_proc_transforms run only on the training side (on the PC). feat_ext_transform runs on the PC during training and on the device during inference.

There are two ways to configure it: pick a preset with feature_extraction_name, or define a custom pipeline with a Custom_* name and your own feat_ext_transform list. The section of the config YAML is data_processing_feature_extraction.

8.1.2. Configuration parameters

Core parameters (time series)

Option

Description

feature_extraction_name

Preset name (for example Generic_1024Input_FFTBIN_64Feature_8Frame) or a custom name that starts with Custom_ (for example Custom_Default). With a Custom_* name you must give feat_ext_transform.

data_proc_transforms

Data processing steps run before feature extraction: SimpleWindow, Downsample, in any order, or [].

feat_ext_transform

Ordered list of feature extraction transforms (see the tables below).

variables

Input channels. An integer (first N columns), a list of column indices ([0, 2, 4]) or a list of column names (['accel_x', 'accel_y']).

frame_size

Samples per frame.

feature_size_per_frame

Output features per frame after the transform.

num_frame_concat

Frames concatenated into one model input. Total features = feature_size_per_frame x num_frame_concat.

stride_size

Window stride as a fraction of frame_size (used with SimpleWindow).

sampling_rate and new_sr

Original and target sampling rate for Downsample.

scale

Scaling factor applied to the input data.

offset

Frame overlap control (see Frame offset).

frame_skip

Number of frames skipped between selected frames.

stacking

'2D1' (default) or '1D' (see Stacking modes).

normalize_bin, min_bin

Bin normalization and the first frequency bin to include.

analysis_bandwidth

Fraction of the signal bandwidth to analyse (1 = full).

log_mul, log_base, log_threshold

Parameters of LOG_DB (for example 20, 10, 1e-100).

q15_scale_factor

Bit-shift scale for the Q15 transforms.

gain_variations

Per-class gain augmentation (see Gain variation augmentation).

gof_test

Run the Goodness of Fit test on the extracted features; see Goodness of Fit.

store_feat_ext_data

Store the extracted features to disk.

dont_train_just_feat_ext

Stop after data processing and feature extraction (see Feature extraction only mode).

nn_for_feature_extraction

Use a neural network for feature extraction.

forecast_horizon, target_variables

Forecasting only: number of future steps and the columns to forecast.

8.1.3. Presets

Presets in 1.5.0 are defined in ModelMaker (tinyml_modelmaker/ai_modules/timeseries/constants.py). Use a preset by name and set variables:

data_processing_feature_extraction:
  feature_extraction_name: 'Generic_1024Input_FFTBIN_64Feature_8Frame'
  variables: 1

The generic presets follow the pattern Generic_<InputSize>Input_<Transform>_<Features>Feature_<Frames>Frame. For example, Generic_1024Input_FFTBIN_64Feature_8Frame takes 1024 samples, applies an FFT with binning to 64 features per frame, and concatenates 8 frames (512 features to the model).

Generic presets

Preset

Transform

Generic_1024Input_FFTBIN_64Feature_8Frame, Generic_512Input_FFTBIN_32Feature_8Frame, Generic_256Input_FFTBIN_16Feature_8Frame, Generic_32Input_FFTBIN_4Feature_8Frame

FFT with binning, 8 frames

Generic_1024Input_FFT_512Feature_1Frame, Generic_512Input_FFT_256Feature_1Frame, Generic_256Input_FFT_128Feature_1Frame

FFT, single frame

Generic_512Input_RAW_512Feature_1Frame, Generic_256Input_RAW_256Feature_1Frame, Generic_128Input_RAW_128Feature_1Frame

Raw time-domain samples

Generic_8Input_ABS_8Feature_1Frame

Absolute value of 8 samples

Application presets

Preset

Application

FFT1024Input_256Feature_1Frame_Full_Bandwidth, FFT1024Input_256Feature_1Frame_Half_Bandwidth, FFT1024Input_64Feature_4Frame_Half_Bandwidth, FFT1024Input_32Feature_8Frame_Quarter_Bandwidth, FFT256Input_FE_RFFT_16Feature_8Frame_removeDC_Full_Bandwidth

FFT with full, half or quarter bandwidth

ArcFault_1024Input_256Feature_1Frame_Full_Bandwidth (also _Half_Bandwidth, ArcFault_1024Input_64Feature_4Frame_Half_Bandwidth, ArcFault_1024Input_32Feature_8Frame_Quarter_Bandwidth, ArcFault_1024Input_FE_RFFT_128Feature_8Frame_1InputChannel_removeDC_Full_Bandwidth, ArcFault_512Input_FE_RFFT_32Feature_8Frame_1InputChannel_removeDC_Full_Bandwidth)

Arc fault

Input256_FFTBIN_16Feature_8Frame_3InputChannel_removeDC_1D and _2D1, Input256_FFT_128Feature_1Frame_3InputChannel_removeDC_2D1, Input128_RAW_128Feature_1Frame_3InputChannel_removeDC_2D1, MotorFault_256Input_FE_RFFT_16Feature_8Frame_3InputChannel_removeDC_1D and _2D1, MotorFault_128Input_RAW_128Feature_1Frame_3InputChannel_removeDC_2D1

Motor fault, 3-axis vibration

PIRDetection_125Input_25Feature_25Frame_1InputChannel_2D, PIRDetection_125Input_25Feature_25Frame_1InputChannel_2D_FixedPoint

PIR detection

FallDetection_256Input_FE_RFFT_8Feature_8Frame_3InputChannel_removeDC_2D1

Fall detection

WiFiCSI_128Input_L2Norm2DFFT_64x26Feature_1Frame_52Subcarriers

WiFi CSI presence detection

ECG2500Input_Roundoff_1Frame

ECG classification

Custom_ArcFault, Custom_ArcFault_MSPM0,``Custom_MotorFault``, Custom_MotorFault_MSPM0, Custom_Default, Custom_Default_MSPM0

Starting points for custom pipelines (_MSPM0 variants use the Q15 fixed-point transforms)

The preset list is the one in the source; other presets exist per task type (audio presets are described below). To see the preset an example uses, open its config in examples/<name>/.

8.1.4. Data processing transforms

SimpleWindow segments continuous data into fixed-size windows:

data_processing_feature_extraction:
  data_proc_transforms: ['SimpleWindow']
  frame_size: 256
  stride_size: 0.01
  variables: 1

Downsample reduces the sampling rate (sampling_rate to new_sr). Transforms run in the order given:

data_processing_feature_extraction:
  data_proc_transforms: ['Downsample', 'SimpleWindow']
  sampling_rate: 313000
  new_sr: 3130
  frame_size: 256
  stride_size: 0.01
  variables: 1

8.1.5. Feature extraction transforms

feat_ext_transform is an ordered list. Each step processes the output of the previous one.

Transform

Description

FFT_FE

FFT of each frame.

FFT_POS_HALF

Keep the positive-frequency half of the FFT.

WINDOWING

Apply a window function.

BINNING

Group frequency bins to reduce the feature count.

NORMALIZE, RANGE_NORMALIZE

Normalize features (RANGE_NORMALIZE uses the value range).

ABS

Absolute value.

LOG_DB

Logarithmic (dB) scale.

DC_REMOVE

Remove the DC component.

CONCAT

Concatenate frames into the final feature vector.

RAW_FE

Mean of the wave in each frame; removes DC if dc_remove is true.

ROUND_OFF

Round the values (used by the ECG2500Input_Roundoff_1Frame ECG preset).

FFT_COL

Column-wise real FFT across the variables axis, per window.

L2_NORM_ROW

L2 norm across rows.

KURT_FE, ENT_FE, ZCR_FE, DOM_FE, SLOPE_FE

Statistical features per frame: kurtosis, spectral entropy, zero-crossing rate, dominant frequency, slope changes.

PIR_FE, PIR_FE_Q15

PIR sensor features (float and fixed-point).

Q15 fixed-point transforms mirror the float pipeline with 16-bit fixed-point math, so the same operations run on MCUs without a floating-point unit. Q15 maps [-1, +1] to [-32768, +32767].

Transform

Description

TO_Q15

Convert float to Q15 with saturation.

FFT_Q15

Fixed-point real FFT (equivalent of FFT_FE).

Q15_SCALE

Bit-shift scaling by q15_scale_factor (positive amplifies, negative attenuates).

Q15_MAG

Magnitude of the complex Q15 FFT output (equivalent of ABS).

BIN_Q15

Average per bin, optionally normalized by normalize_bin, clipped to 16 bits (equivalent of BINNING).

Example: FFT with binning

data_processing_feature_extraction:
  feat_ext_transform: ['FFT_FE', 'FFT_POS_HALF', 'DC_REMOVE', 'ABS', 'BINNING', 'LOG_DB', 'CONCAT']
  frame_size: 1024
  feature_size_per_frame: 64
  num_frame_concat: 4
  variables: 1

Example: Q15 pipeline for MCUs

data_processing_feature_extraction:
  feat_ext_transform: ['FFT_Q15', 'Q15_SCALE', 'Q15_MAG', 'DC_REMOVE', 'BIN_Q15', 'CONCAT']
  frame_size: 256
  feature_size_per_frame: 16
  num_frame_concat: 8
  q15_scale_factor: 5
  normalize_bin: True
  variables: 1

8.1.6. Custom feature extraction

Use a Custom_* name and define the pipeline yourself:

data_processing_feature_extraction:
  data_proc_transforms: ['SimpleWindow']
  feature_extraction_name: 'Custom_Default'
  feat_ext_transform: ['FFT_FE', 'FFT_POS_HALF', 'WINDOWING', 'BINNING', 'NORMALIZE', 'ABS', 'LOG_DB', 'CONCAT']
  frame_size: 32
  feature_size_per_frame: 8
  num_frame_concat: 8
  variables: 5

Add the fine-grained keys (normalize_bin, stacking, offset, scale, frame_skip, log_mul, log_base, log_threshold) when you need them.

8.1.7. Windowing and framing

8.1.7.1. Frame offset

offset controls the overlap between consecutive frames. offset: 0 means no overlap. With offset: n the step is 1/n of a frame: offset: 2 gives 50% overlap and offset: 4 gives 75%. More overlap produces more training samples from the same data.

data_processing_feature_extraction:
  offset: 2
  frame_size: 256
  variables: 3

8.1.7.2. Stacking modes

stacking controls how multi-channel features are arranged for the model.

  • '1D': features of all channels are concatenated into one flat sequence ([a1, a2, a3, b1, b2, b3, ...]). Good for fully connected models.

  • '2D1' (default): a 2D matrix with one row per channel. Good for convolutional models.

8.1.7.3. Analysis bandwidth

analysis_bandwidth: 1 analyses the full spectrum; 0.5 only the lower half. Use it when only part of the spectrum matters.

8.1.7.4. Gain variation augmentation

gain_variations multiplies the raw data of each class by a random gain drawn from U(min, max), which makes the model robust to amplitude changes. It is applied before feature extraction, with Downsample or SimpleWindow.

data_processing_feature_extraction:
  data_proc_transforms: [Downsample, SimpleWindow]
  gain_variations:
    arc: [0.9, 1.1]
    normal: [0.8, 1.2]
  sampling_rate: 313000
  new_sr: 3130
  frame_size: 256
  stride_size: 0.01
  variables: 1

8.1.7.5. Forecasting

Forecasting needs SimpleWindow plus the forecasting keys:

data_processing_feature_extraction:
  data_proc_transforms: [SimpleWindow]
  frame_size: 32
  stride_size: 0.1
  forecast_horizon: 2
  variables: 1
  target_variables: [0]

8.1.8. Audio front-ends

Audio classification (target_module: audio) selects the front end with audio_feature and a preset. The audio parameters and their defaults are:

Option

Description

audio_feature

MFCC (default), LPC, FFT, FB (learned filterbank) or RAW.

sampling_rate, audio_duration_ms

Audio sampling rate (default 16000) and clip length (default 1000 ms).

frame_length_ms, frame_step_ms

Analysis frame length and step (defaults 30 and 20 ms).

n_mfcc, n_mels

MFCC settings (defaults 10 and 40).

nlpc, lpc_order

LPC settings (defaults 70 and 10).

fb_conv_kernel, fb_output_channel, fb_conv_stride, fb_context_ms, fb_bitwidth, input_bit_depth

Learned filterbank settings (defaults 64, 64, 4, 20, 8 and 16).

frame_size, feature_size_per_frame, num_frame_concat, q15_scale_factor, min_bin

FFT front-end settings (defaults 512, 32, 1, 8 and 1).

normalize_audio, mono

Normalize the waveform (default true) and mix to mono (default true).

Audio presets:

Preset

Front end

GoogleSpeechCommands_MFCC_Default

MFCC (10 coefficients, 40 mel bands).

MSPM0_LPC_8k, MSPM0_LPC_8820

LPC front end that matches the MSPM0G5187 firmware pipeline (8000 Hz, and 8820 Hz from the I2S path), used by cough detection.

WakeWordDetection_Filterbank_Default

Learned filterbank: a Conv1D filter bank that is trained jointly with the model (fb_* keys), used with TCDS_ResNet_FB_NPU.

GlassBreakDetection_512FFT_Default

Q15 FFT, binning and concatenation (512 point FFT, 32 features per frame), used with DSCNN_GB_NPU.

See Audio Classification, Wake Word Detection and Glass Break Detection.

8.1.9. Radar and image inputs

Radar classification does use the data_proc_transforms mechanism, but with its own radar stages instead of the time series transforms above. The stages run in this order, and a preset or your YAML selects the ones it needs:

data_proc_transforms entry

What it does

Radar Range Data

Selects FFT range bins (bin* columns), optionally limited with radar_range_bins_bounds. Used for surface classification.

Radar Point Cloud Data

Selects and filters point-cloud fields (radar_point_cloud_data_selector, coordinate system, spatial and non-spatial filter bounds).

Radar Track Data

Selects and filters tracker fields (radar_track_data_selector, velocity, acceleration and spatial bounds).

Simple Window

Stacks frame_size radar frames into one sample (stride_size sets the overlap) and applies the frame quality checks (radar_frames_quality_index, radar_min_points_per_window) and feature ordering (radar_feature_ordering).

Scaling

Scales values such as track velocity (radar_data_scaling_track_velocity).

The radar presets are Generic_248Input_Posture_and_Fall_Detection, Generic_130Input_Radar_SurfaceClassification, Generic_392Input_PointCloudWithTrack_SimpleWindow and Generic_Radar_SimpleWindowOnly. See Radar Classification and the full parameter reference in Radar Data Pre-Processing Pipeline — Complete Reference Guide.

Image classification is the one that uses image-style parameters: its presets (for example Mnist_Default) set image_height, image_width, image_num_channel, image_mean and image_scale. See Image Classification.

8.1.10. Evaluating feature extraction quality

Before training, ModelMaker writes PCA plots of the extracted features for classification tasks (pca_on_feature_extracted_train_data.png and ..._validation_data.png in the training/base folder of the run). Clusters that are visibly separable are easier for the model to learn.

PCA on training data

PCA of the extracted features on training data

PCA on validation data

PCA of the extracted features on validation data

  • Tight, well-separated clusters: the features represent the classes well.

  • Overlapping clusters: try a different feature extraction.

  • Scattered points: high variance, possibly noisy data.

No single feature extraction is best for every dataset. Frequency-domain presets (FFT with binning) usually do better on periodic signals like vibration, and raw presets on waveform-shape problems. Compare several presets.

8.1.10.1. Feature extraction only mode

Set dont_train_just_feat_ext: True to run only data processing and feature extraction. Combine with store_feat_ext_data: True to export the features. This is a fast way to compare presets by their PCA plots:

data_processing_feature_extraction:
  dont_train_just_feat_ext: True
  store_feat_ext_data: True
  feature_extraction_name: 'Input256_FFTBIN_16Feature_8Frame_3InputChannel_removeDC_2D1'
  variables: 3

8.1.11. Memory cost on the device

Feature extraction runs on the MCU before inference and needs its own RAM and Flash. Since 1.5.0 you can see this cost before training: the compile step reports a Feature Extraction Library memory block next to the model, and the standalone estimate_memory tool prints it in seconds. See Memory Estimation.

8.1.12. Best practices

  1. Match the transform to the signal: FFT for periodic signals, raw for transient ones.

  2. Start from a standard preset and customize only if needed.

  3. Mind the device: fewer features give smaller models and faster inference.

  4. Compare several options with dont_train_just_feat_ext and the PCA plots.

8.1.13. Next steps