7.10.2. Generic Timeseries Regression
A “Hello World” introduction to timeseries regression with Tiny ML ModelZoo. It shows how any generic timeseries regression task is set up, trained, quantized and compiled.
Example folder: examples/generic_timeseries_regression
(GitHub)
7.10.2.1. Overview
Task: timeseries regression (
generic_timeseries_regression), continuous value predictionDataset: synthetic,
y = 1.2 sin(x) + 3.2 cos(x)withxdrawn randomly from [0, 3]Device: F28P55 (
config.yaml)Model:
REGR_2k(a small CNN regressor)
7.10.2.2. The Dataset
Column |
Description |
|---|---|
|
Randomly generated in the range [0, 3] |
|
Target, |
The split is 7 training files, 2 validation files and 1 test file, with 5000 data points per file. The
config downloads the dataset automatically from
https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/generic_timeseries_regression.zip.
7.10.2.3. Dataset Format
For regression ModelMaker always requires annotation files, which assign each file to the train, validation
or test set. The data folder is named files for regression and forecasting tasks.
{dataset_name}.zip/
|
|-- files/
| |-- {file1}
| |-- {file2}
| |-- {fileN}
|
|-- annotations/
|-- file_list.txt
|-- instances_train_list.txt
|-- instances_val_list.txt
|-- instances_test_list.txt
To use your own data, see Regression Dataset Format.
7.10.2.4. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from
the tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/generic_timeseries_regression/config.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\generic_timeseries_regression\config.yaml
7.10.2.5. Configuration
common:
task_type: generic_timeseries_regression
target_device: F28P55
dataset:
dataset_name: generic_timeseries_regression
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/generic_timeseries_regression.zip
data_processing_feature_extraction:
stride_size: 1
data_proc_transforms:
- SimpleWindow
frame_size: 10
variables: 1
training:
optimizer: adam
lr_scheduler: cosineannealinglr
model_name: REGR_2k
batch_size: 256
training_epochs: 45
early_stopping: true
early_stopping_patience: 5
lambda_reg: 0.01
num_gpus: 0
quantization: 2 # 0 = float model, 2 = 8-bit quantized model
auto_quantization: True
testing: {}
compilation: {}
variables is the number of input columns (after the time columns) that are used to predict the target.
num_gpus: 0 runs on CPU; set it to 1 if a GPU is available. The quantization and
auto_quantization keys select the float, partially quantized or fully quantized flow (see below). For
the meaning of every key see How to Create a ModelZoo Config YAML.
7.10.2.6. Evaluation Metrics
RMSE (root mean square error): the square root of the mean squared error. Range 0 to infinity, ideal value 0 (lower is better).
R2 score (coefficient of determination): the fraction of the variance in the data that the model explains. Range (-infinity, 1], ideal value 1 (higher is better).
The best epoch is the one with the lowest validation MSE; the checkpoint is updated whenever a lower value is seen.
7.10.2.7. Results
The example readme reports these test-set results for the three quantization settings:
Model |
RMSE |
R2 score |
|---|---|---|
Float ( |
0.15 |
0.95 |
Partially quantized ( |
0.11 |
0.98 |
Fully quantized ( |
0.11 |
0.97 |
These numbers come from the example readme. The automated 1.5.0 config test run (short, early stopped) reached a quantized test RMSE of 0.33 and R2 of 0.78, so expect results to vary with the training length and early stopping.
7.10.2.8. Output Location
Results are written to ./data/projects/generic_timeseries_regression/run/<date-time>/REGR_2k/.
training/quantization/post_training_analysis/: predicted-versus-actual plot, error histogram andresults_on_test_set.csv(columnsground_truthandpredicted)training/quantization/golden_vectors/:user_input_config.handtest_vector.ccompilation/artifacts/:mod.aandtvmgen_default.h
See Understanding the Run Output for details.
7.10.2.9. Running on Device
Follow Deploying Regression Models from ModelMaker to Device to integrate the compiled artifacts into a device project.
7.10.2.10. Next Steps
Torque Measurement Regression: real-world motor torque prediction
Regression Dataset Format: use your own regression data
Understanding Config: all config options