1.1. What is Tiny ML ModelZoo?
Tiny ML ModelZoo is Texas Instruments’ central repository of AI models, example applications and configurations for microcontroller (MCU) applications. Together with the toolchain it installs, it takes you from raw data to a compiled model running on a TI MCU.
Note
Up to release 1.4.0 this toolchain was distributed as Tiny ML Tensorlab
(tinyml-tensorlab), a set of repositories you cloned together. From 1.5.0,
tinyml-modelzoo is the entry point and everything else comes in as prebuilt wheels
(Installation). tinyml-tensorlab is deprecated and its source is private.
1.1.1. Overview
The toolchain handles:
Data preparation: format and preprocess datasets for training
Feature extraction: transform raw signals into meaningful features
Model training: train neural networks designed for embedded deployment
Model optimization: quantize models for efficient inference
Compilation: generate device-specific code with TI’s Neural Network Compiler
Analysis: evaluate model performance before deployment
1.1.2. Target Applications
- Predictive maintenance
Motor bearing, gearbox and fan blade fault detection, equipment anomaly monitoring, vibration analysis.
- Power systems
DC and AC arc fault detection, grid fault and stability, electrical fault classification.
- Control systems
Torque estimation, motor speed prediction, temperature forecasting, battery state-of-charge estimation.
- Sensor processing and sensing
Activity and fall detection, PIR and Wi-Fi CSI presence detection, gas classification, radar point cloud and surface classification.
- Audio and vision
Keyword and wake word detection, cough and glass break detection, image classification.
1.1.3. Key Capabilities
Supported ML tasks
Time Series Classification |
Categorize sensor signals into discrete classes |
Time Series Regression |
Predict continuous values from sensor inputs |
Time Series Forecasting |
Predict future values from historical patterns |
Time Series Anomaly Detection |
Identify abnormal patterns using autoencoders |
Audio Classification |
Classify audio from MFCC features |
Image Classification |
Categorize images into classes |
Radar Classification |
Classify point-cloud frames or FFT range profiles from radar sensors |
Device support
33 MCU and wireless devices (as listed in the README of the 1.5.0 release) across these families. See Supported Devices for details.
C2000 (C28 DSP): F28P55 (with NPU), F28P65, F2837, F2838x, F28003, F28004 and others
C2000 (C29 DSP): F29H85, F29P58, F29P32
MSPM0: MSPM0G3507, MSPM0G3519, MSPM0G5187 (with NPU)
MSPM33C: MSPM33C32, MSPM33C34
AM13: AM13E2 (with NPU)
AM26x: AM263, AM263P, AM261
Connectivity: CC2755, CC2745, CC1312, CC1314, CC1352, CC1354, CC35X1
Radar: xWRL6432
Example applications and models
The examples/ folder ships ready-to-run applications (the generic ones for each task
plus dedicated applications such as arc fault, motor bearing fault, ECG, wake word and
Wi-Fi presence detection), and the model zoo contains 85 models. See
Examples & Applications and Model Zoo Reference.
Model optimization
Quantization-aware training (QAT) and post-training quantization (PTQ)
Hessian-aware (HAWQ) automatic mixed-precision quantization
Residual connection support for NPU quantization
NPU acceleration
Select devices (F28P55, MSPM0G5187, AM13E2) include TI’s TinyEngine NPU for hardware-accelerated inference with faster execution and lower power. See NPU Configuration Guidelines for TI Neural Network Compiler.
1.1.4. What’s New in 1.6.0
Radar surface classification example (
radar_surface_classification) and two new radar models,RF_MLP_3L_11KandRF_DualStream_PointCloud_19Kradar_pose_and_fall_detectionrenamed toradar_posture_and_fall_detection, with a new radar processing pipeline guide85 models (was 83)
1.1.5. What’s New in 1.5.0
Standalone pip install of
tinyml-modelzoo; one repository to clone for model workNew tasks and devices: audio classification, radar point cloud classification, AM13E2 vision
Early stopping on by default, NaN-loss detection, memory estimation before training
macOS Apple Silicon (MPS) support, Python 3.14 / PyTorch 2.11 compatibility for training
Integer on-device training, learned filterbank front end, new example applications
See the release history in the README and the changelog in the appendix.
1.1.6. Repository Structure
tinyml-modelzoo/
├── examples/ # ready-to-run example configurations
├── tinyml_modelzoo/
│ ├── models/ # neural network model definitions
│ └── model_descriptions/ # model metadata (names used in configs)
├── docs/ # guides
├── run_tinyml_modelzoo.sh / .bat / .ps1
└── ADDING_NEW_MODELS.md
The other parts of the toolchain are installed as packages, not cloned:
tinyml_modelmakerOrchestrates the workflow: reads the config, runs training, testing and compilation.
tinyml_tinyverseCore training infrastructure: datasets, training scripts, feature extraction transforms.
tinyml_torchmodeloptQuantization toolkit (TINPU and generic wrappers, QAT/PTQ).
1.1.7. Workflow Summary
Install: Installation
Prepare data and a config: Bring Your Own Data, How to Create a ModelZoo Config YAML
Run:
./run_tinyml_modelzoo.sh examples/generic_timeseries_classification/config.yamlReview results: Understanding the Run Output
Deploy to a device: Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check)