8.12.3.1. On-Device Training Documentation

8.12.3.1.1. Table of Contents


8.12.3.1.2. Introduction

On-device training enables deep learning models to continue training directly on TI microcontrollers after deployment. Instead of the traditional “train on PC → deploy frozen model” workflow, models can adapt to new environments, personalize to specific installations, and maintain accuracy as conditions change — all without sending data back to a PC.

The on-device training framework supports both partial model training (freeze early layers, train last k layers) and full model training (train all layers on-device). The core ODT libraries are device-agnostic and designed to work across TI MCU families. It currently supports the anomaly detection task with autoencoder models.

Traditional:   Train on PC → Compile → Deploy → Inference only (fixed model)

On-Device:     Train on PC → Split model → Deploy frozen + trainable parts → Continue training on MCU → Adapt to real environment → Inference

8.12.3.1.3. What You Need

Requirement

Details

Hardware

A supported TI MCU LaunchPad. Currently, examples are available for the F29H85x (C29x family).

SDK

The corresponding device SDK and Code generation tools (e.g., F29H85x SDK for C29x)

IDE

Code Composer Studio (CCS)

ModelZoo

tinyml-modelzoo installed and working (pip install -e . from the tinyml-modelzoo folder, see the repository README)

Baseline working

The standard (non-ODT) anomaly detection example for your device should build and run successfully before attempting on-device training. This verifies your SDK, CCS, and hardware setup are correct. See the fan blade example readme.


8.12.3.1.4. Key Concepts

This section summarizes the core architectural ideas. For full details, see Overview.

8.12.3.1.4.1. Frozen + Trainable Split

The model is split into two parts before deployment:

Raw Input → [Feature Extraction] → [Frozen Model] → [Trainable Model] → Output
                                     ─────┬─────      ──────┬──────
                                          │                 │
                                  Compiled via TVM     Exported as C arrays
                                  Stored as mod.a      Weights updated on-device
                                  Cannot be changed    
  • The frozen part (earlier layers) is compiled into an optimized static library (mod.a) via TVM. It extracts general-purpose features (e.g., frequency patterns from FFT) that transfer well across environments. It runs fast but cannot be updated on-device.

  • The trainable part (last k layers) is exported as float C arrays with full forward and backward pass support. These layers perform task-specific computation that is most affected by environmental changes. They are retrained on-device to adapt to the deployment environment.

  • The split point is controlled by trainable_layers_from_last in the YAML config. Setting it to 1 trains only the last main layer. Setting it equal to the total number of main layers trains the entire model on-device.

8.12.3.1.4.2. PC-Side Pipeline → Device-Side Training

The workflow has two phases:

PC side (run once):

  1. Train the model using ModelZoo (or export with 0 epochs for fully on-device training)

  2. Split the ONNX model → compile frozen part (mod.a) + export trainable part (trainable_model_config.h/.c)

  3. Export a small number of training/validation/test samples as C arrays (ondevice_training_data.h/.c)

  4. Copy all artifacts to the CCS project

Device side (runs on MCU):

  1. Initialize the model (frozen + trainable parts)

  2. Train the trainable layers using the embedded data (or live sensor data)

  3. Perform task-specific post-training calibration (e.g., threshold recalculation for anomaly detection)

  4. Run inference with the updated model

8.12.3.1.4.3. On-Device Training Loop

The device-side training is a standard neural network training loop adapted for MCU constraints:

  • Forward pass: Input flows through frozen model → trainable model → output

  • Loss computation: Loss is computed between model output and target

  • Backward pass: Gradients propagate through trainable layers only; weights are updated via SGD

  • Validation: After each epoch, validation loss is computed

  • Early stopping: Training stops automatically when validation loss stops improving (EMA-smoothed, with configurable patience)

  • Best weight checkpointing: The best-performing weights are saved during training and restored at the end

For batch_size=1 (the default), weight updates happen immediately during the backward pass — no gradient accumulation buffer needed, saving both memory and compute.

8.12.3.1.4.4. Task-Specific Libraries

The core ODT library (ondevice_training_lib) is task-agnostic — it provides forward pass, backward pass, weight updates, and loss computation. Task-specific behavior is implemented in separate libraries built on top:

Task Library

Status

Key Features

anomaly_detection_odt

Available

State machine (train/threshold/inference modes), EMA-smoothed early stopping, percentile and Gaussian threshold calculation, majority voting inference

classification_odt

Planned

Cross-entropy loss, accuracy tracking

8.12.3.1.4.5. Supported Configurations

Category

Currently Supported

Layer types

Linear (fully connected), ReLU

Tasks

Anomaly detection (autoencoder)

Loss functions

MSE (Mean Squared Error)

Optimizers

SGD

Data format

Float32

Training modes

Partial model (last k layers) or full model (all layers)

Example devices

Works across all devices like C28, C29 etc.


8.12.3.1.5. Quickstart

This walkthrough uses the fan blade anomaly detection on device learning example. By the end, you will have a model that got trained on device.

8.12.3.1.5.1. Step 1: Configure YAML

Start with the fan blade ODT YAML or add these ODT-specific fields to your existing anomaly detection YAML:

training:
    model_name: 'Ondevice_Trainable_AD_Linear'   # Model that supports split training
    quantization: 0                                # Must be 0 (float for trainable path)
    ondevice_training: True                        # Enable ODT export pipeline
    trainable_layers_from_last: 1                  # Train last 1 main layer on-device
    export_samples_per_class: [10, 10, 10]         # [train, val, test] samples to embed

The complete YAML is at:

tinyml-modelzoo/examples/fan_blade_fault_classification/fan_blade_anomaly_detection_ondevice_training.yaml

For full details on each field, see Running ModelZoo for ODT.

8.12.3.1.5.2. Step 2: Run ModelZoo

./run_tinyml_modelzoo.sh examples/fan_blade_fault_classification/fan_blade_anomaly_detection_ondevice_training.yaml

This runs the standard training pipeline, then additionally:

  • Splits the ONNX model at the configured layer

  • Compiles the frozen part via TVM → mod.a

  • Exports the trainable part → trainable_model_config.h/.c

  • Exports embedded training data → ondevice_training_data.h/.c

  • Generates golden vectors and feature extraction config

8.12.3.1.5.3. Step 3: Import CCS Project and Copy Artifacts

First, import the on-device training example project from your device SDK into CCS:

  1. In CCS: File → Import → CCS Projects

  2. Browse to the on-device training example in your device SDK (for F29H85x: the fan_blade_anomalydetection_ondevice_learning example)

  3. Import the project

Then copy these generated files from the ModelMaker output into the imported project’s artifacts/ directory:

File

What it is

mod.a

Compiled frozen model

tvmgen_default.h

Frozen model API

trainable_model_config.h/.c

Trainable layer architecture + weights

ondevice_training_data.h/.c

Embedded train/val/test datasets

user_input_config.h

Feature extraction config + initial threshold

test_vector.c

Golden vectors for validation

These files replace the default artifacts that ship with the example project. For exact source paths in the ModelMaker output, see Running ModelZoo — Copying Artifacts.

8.12.3.1.5.4. Step 4: Build, Flash, and Run

  1. Select the Flash build configuration

  2. Build the project

  3. Connect your LaunchPad and flash the device

  4. Open the CCS console — you should see initialization logs:

========================================
ANOMALY DETECTION MODEL INITIALIZATION
========================================
Learning rate(multiplied by 10^5): 10
Batches per epoch: 10, total samples per epoch 10
...

========================================
ODT INITIALIZATION
========================================
  Layer 0: Linear(48→24)
  Layer 1: ReLU(24)
  ...
  Layer 10: Linear(24→48)

The application then runs golden vector validation and pre-training inference automatically, then waits for you to trigger training.

8.12.3.1.5.5. Step 5: Trigger Training

In CCS, open the Variables view, add the variable start_training, and change its value from 0 to 1. Training begins immediately.

The console shows per-epoch training and validation loss. Training runs until early stopping triggers . After training, the threshold is automatically recalculated and post-training inference runs.

8.12.3.1.5.6. What to Expect

Stage

What Happens

Golden vector validation

All 48 outputs match → artifacts loaded correctly

Pre-training inference

Untrained model, produces random results, all predictions are random

Training

Loss drops from ~5500 to ~10 over ~120 epochs, early stopping triggers

Threshold recalculation

New threshold: ~25 (down from ~6430)

Post-training inference

12/12 correct with normal errors ~10 and anomaly errors ~130–1000 — genuine separation

For the complete walkthrough with real console output, see Application Example — Fan Blade.


8.12.3.1.6. Documentation Map

Read in order for a complete understanding, or jump to the section relevant to you.

8.12.3.1.6.1. 1. Overview

The starting point for understanding on-device training. Covers what ODT is and why it is needed (data drift, privacy, personalization). Explains the frozen+trainable split architecture in detail, what trainable_layers_from_last controls, partial vs full model training, the complete end-to-end workflow, feature tables for core framework and anomaly detection task library, supported configurations, memory considerations, and current limitations.

8.12.3.1.6.2. 2. Running ModelZoo for ODT

Step-by-step guide to generating all artifacts using the ModelZoo pipeline. Covers the ODT-specific YAML fields with detailed explanations, a complete YAML example, the exact command to run, real console log output at each stage, how the pipeline works under the hood (ONNX splitting, weight flattening, buffer offset computation), the output directory structure, and a file-by-file mapping of what to copy to the CCS project.

8.12.3.1.6.3. 3. Generated Artifacts Overview

A bird’s-eye view of all generated files and how they connect. Shows which files are shared with the standard (non-ODT) pipeline and which are new for ODT. Explains the role of each artifact and how data flows between them at runtime on the device.

8.12.3.1.6.4. 4. Trainable Model Configuration

Deep dive into trainable_model_config.h and .c. Covers every #define, every data structure (LayerType_t, LayerParams_t, LAYER_PARAMS_INIT), the flat weight array with offset-based access, intermediate and gradient buffer allocation, memory section attributes for MCU RAM placement, batch size configuration, and the USE_GRADIENT_ACCUMULATION compile-time optimization.

8.12.3.1.6.5. 5. On-Device Training Data

Deep dive into ondevice_training_data.h and .c. Explains how raw sensor data is exported as 2D C arrays, the data layout (samples x raw input size), label encoding, sample counts per split, RAW_INPUT_SIZE computation from the feature extraction config, and how the application iterates through these arrays during training.

8.12.3.1.6.6. 6. On-Device Training Library

Complete API reference for the core training engine (ondevice_training_lib.h/.c). Covers ModelContext_t and its flat-array memory architecture with detailed diagrams, initialization and validation, forward and backward pass, MSE loss and gradient computation, weight checkpointing, the batch_size=1 optimization, Linear and ReLU layer implementations, the logging system, a complete custom training loop example, and how to add new layer types.

8.12.3.1.6.7. 7. Anomaly Detection ODT Library

Complete API reference for the anomaly detection task library (anomaly_detection_odt.h/.c). Covers the three-mode state machine (inference, training, threshold calculation), all configuration parameters, training orchestration with automatic epoch and phase management, EMA-smoothed early stopping, percentile and Gaussian threshold calculation, majority voting inference, rolling statistics, all API functions with detailed behavior, and usage examples showing the complete workflow.

8.12.3.1.6.8. 8. Application Example — Fan Blade

A complete working example walkthrough. Walks through all six stages: initialization, golden vector validation, pre-training inference, on-device training with real epoch-by-epoch console output, threshold recalculation, and post-training inference. Includes before-vs-after comparison, key code patterns, hyperparameter reference, and instructions for adapting the example to your own dataset.

8.12.3.1.6.9. 9. FAQ & Troubleshooting

Common issues and their solutions. Covers training problems (loss not decreasing, exploding loss, early stopping too early/late), deployment issues (golden vector mismatch, build failures, RAM overflow), threshold and inference problems, YAML configuration mistakes, and general questions about learning rate tuning, live sensor data, retraining, and persistence.


8.12.3.1.7. Reading Paths

New to on-device training? → Overview → Running ModelZoo → Application Example

Developer integrating ODT into a project? → Application Example → Anomaly Detection ODT Library → Generated Artifacts Overview

Understanding the generated files? → Generated Artifacts Overview → Trainable Model Configuration → On-Device Training Data

Writing a custom training loop? → On-Device Training Library (Section 12: Writing a Custom Training Loop)

Extending the framework (new layers, new tasks)? → On-Device Training Library (Section 13: How to Add a New Layer Type) → Overview (Section 7: Supported Task Libraries)

Something not working? → FAQ & Troubleshooting