7.10.17. PIR Detection
Edge AI solution for PIR (passive infrared) sensor based motion classification on the MSPM0G5187 with NPU acceleration, also available for the SimpleLink CC13xx/CC27xx/CC35X1 wireless MCUs.
Example folder: examples/pir_detection
(GitHub)
7.10.17.1. Overview
Traditional PIR sensors only detect presence or absence of motion and cannot tell its source. Pets and environmental factors cause false alarms, and manual threshold tuning is unreliable across environments. This example classifies PIR sensor signals into motion categories, which reduces false positives while keeping detection sensitivity.
Application: security systems, smart home automation, occupancy sensing
Task: classification (
task_type: pir_detection), 3 classesPrimary device: MSPM0G5187
Model:
PIRDetection_model_1_tTargets of the reference solution: real-time classification, more than 90% accuracy, low power
7.10.17.2. System Components
Hardware: MSPM0G5187 with integrated NPU, and the EdgeAI Sensor Boosterpack (TIDA-010997) with a PIR sensor
Software: Code Composer Studio 12.x or later, MSPM0 SDK 2.08.00 or later
7.10.17.3. Available Configurations
Config file |
Device |
Feature extraction preset / epochs |
|---|---|---|
|
MSPM0G5187 |
|
|
CC1312 |
|
|
CC1314 |
same as CC1312 |
|
CC1352 |
same as CC1312 |
|
CC1354 |
same as CC1312 |
|
CC2755 |
same as CC1312 |
|
CC35X1 |
same as CC1312 |
The MSPM0 config uses the fixed-point feature extraction that matches the integer pipeline on the device; the other configs use the floating point version.
7.10.17.4. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the
tinyml-modelzoo folder:
# MSPM0G5187 (primary)
./run_tinyml_modelzoo.sh examples/pir_detection/config_MSPM0.yaml
# other devices
./run_tinyml_modelzoo.sh examples/pir_detection/config_CC1352.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\pir_detection\config_MSPM0.yaml
7.10.17.5. Dataset
pir_detection_classification (https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/pir_detection_classification_dsk.zip)
contains PIR recordings captured with the EdgeAI Sensor Boosterpack from a range of 6 to 8 meters:
Class |
Description |
|---|---|
Human motion |
Movement patterns characteristic of humans |
Background motion |
Environmental disturbances and noise |
Dog motion |
Movement patterns characteristic of dogs |
7.10.17.6. Feature Extraction Pipeline
The PIRDetection_125Input_25Feature_25Frame_1InputChannel_2D presets process the raw signal as follows:
ADC sampling
DC offset removal
Windowed processing
Symmetric mirroring
FFT computation
Magnitude calculation
Average pooling
Additional features: zero crossing rate (ZCR), slope changes, dominant frequency
Concatenation of all features into the model input
7.10.17.7. Configuration (config_MSPM0.yaml)
common:
task_type: pir_detection
target_device: MSPM0G5187
dataset:
dataset_name: pir_detection_classification
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/pir_detection_classification_dsk.zip
data_processing_feature_extraction:
data_proc_transforms: []
feature_extraction_name: PIRDetection_125Input_25Feature_25Frame_1InputChannel_2D_FixedPoint
variables: 1
training:
model_name: PIRDetection_model_1_t
batch_size: 64
training_epochs: 100
PIRDetection_model_1_t is a compact CNN with about 53K or more parameters, NPU compatible and optimized for
multivariate input signals. The MSPM0 config trains with batch size 64, learning rate 0.00001, weight decay 1e-20 and
100 epochs; the CC13xx/CC27xx/CC35X1 configs use batch size 64, learning rate 0.001 and 50 epochs. The optimizer
is the default SGD. Compilation uses the TI Neural Network Compiler and generates
model.a and tvmgen_default.h.
7.10.17.8. Results
The example readme.md reports about 98% accuracy for CC1352 with floating point feature extraction and
about 92.46% for MSPM0 with fixed point feature extraction (earlier release). In the automated 1.5.0 config test
run:
Config |
Test accuracy |
AUC ROC |
|---|---|---|
|
94.81% |
0.826 |
|
65.40% |
0.795 |
Note
The MSPM0 test-run accuracy (65.40%) is far below the 92.46% the example readme quotes from an earlier release. The reasons were not investigated here; check the printed confusion matrix of your own run and consider tuning epochs and learning rate for the fixed-point configuration.