11.1.3. Compilation Only
If you already have a trained model in ONNX format, for example exported from PyTorch or another framework, you can compile it for a TI device with ModelMaker and skip the dataset and training stages.
The flow is:
Train (and, for NPU devices, quantize) the model outside ModelZoo.
Export it to ONNX.
Run ModelMaker with only the compilation stage enabled and
compilation.model_pathpointing at the ONNX file.Deploy the compiled artifacts to the device (see Deployment).
Use it when you have a model from another framework or training environment, or an architecture you do not want to add to the ModelZoo. If you want ModelZoo to train and quantize your model, use Bring Your Own Model (BYOM) instead.
11.1.3.1. Configuration
Disable the dataset and training stages and give the path of the ONNX file under compilation:
common:
target_module: 'timeseries'
task_type: 'generic_timeseries_classification'
target_device: 'F28P55'
run_name: '{date-time}/{model_name}'
dataset:
enable: False # no dataset needed
dataset_name: my_model # only used to name the output folders
training:
enable: False # no training
model_name: 'my_model' # only used to name the output folders
compilation:
enable: True
model_path: '/path/to/your/model.onnx'
When compilation.model_path points to an existing file, ModelMaker compiles that file. Otherwise it looks for the
model.onnx that a training stage of the same run produced.
11.1.3.1.1. Quantized models and NPU devices
For an NPU device the compiler needs a model quantized for the NPU. The compile target keeps the hard NPU mode only
when training.quantization is 2 (TINPU); for any other value the target is switched to the software NPU. If your
ONNX file is already an NPU-quantized model, set the level so that the NPU target is kept:
training:
enable: False
model_name: 'my_model'
quantization: 2
A float model compiles for the software path and is not accelerated by the NPU. Quantize it first, for example with the wrappers described in Quantization.
11.1.3.2. Running the compilation
Run the config like any other, from the tinyml-modelzoo folder (see Running Examples):
./run_tinyml_modelzoo.sh byom_config.yaml
run_tinyml_modelzoo.bat byom_config.yaml
./run_tinyml_modelzoo.ps1 byom_config.yaml
The compiled artifacts are written to the compilation folder of the run
(./data/projects/<project_name>/run/<date-time>/<model_name>/compilation/). It contains the compiled library
mod.a and the header tvmgen_default.h in artifacts/, and a zip package of the compilation output.
Note
The compile-only flow needs the compiler tools to be installed (see Installation). The golden vectors used by the deployment guides come from a training run, and a compile-only run does not create them. See Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check). This page describes what the 1.5.0 ModelMaker code supports; the flow was not re-run end to end for this guide.
11.1.3.3. Example: external PyTorch model
Export the trained model to ONNX with a batch size of 1:
import torch
model.eval()
dummy_input = torch.randn(1, 1, 512, 1) # (batch, variables, features, 1)
torch.onnx.export(model, dummy_input, 'my_model.onnx',
input_names=['input'], output_names=['output'],
opset_version=18)
The ModelZoo training scripts export with ONNX opset 18 by default, so using the same opset avoids surprises. Then use the
configuration above with model_path: 'my_model.onnx'. A TensorFlow model can be converted to ONNX first (for
example with tf2onnx) and compiled the same way.
11.1.3.4. NPU constraints
For NPU devices the ONNX model must follow the NPU rules (channel counts that are multiples of 4, limits on kernel and pooling sizes). See NPU Configuration Guidelines for TI Neural Network Compiler. If the model does not meet them you can modify and retrain it, target a device without NPU, or accept that those layers run on the CPU.
11.1.3.5. Troubleshooting
Unsupported operator: replace it with a supported operation or simplify the model.
Input shape mismatch: check the input shape of the ONNX model against what the application feeds it.
Model not accelerated on an NPU device: the model is not NPU-quantized, or
training.quantizationis not2.
11.1.3.6. Best practices
Test the ONNX model with ONNX Runtime before compiling.
Start by compiling for a device without NPU to debug the model.
Compare the outputs of the compiled model with the original.