7.10.22. Torque Measurement Regression

Estimate the electromagnetic torque of a permanent magnet synchronous motor (PMSM) from electrical and thermal measurements, as a virtual (sensorless) torque sensor.

Example folder: examples/torque_measurement_regression (GitHub)

7.10.22.1. Overview

  • Task: timeseries regression (generic_timeseries_regression)

  • Application: motor control, sensorless torque estimation

  • Device: F28P55 (config.yaml)

  • Model: REGR_10k

  • Target: torque

7.10.22.2. The Dataset

The data are measurements from a PMSM prototype on a test bench (German OEM motor, recorded by the LEA department at Paderborn University), sampled at 2 Hz. It is the Electric Motor Temperature dataset on Kaggle.

Column

Description

i_d, i_q

Current d- and q-components

u_d, u_q

Voltage d- and q-components

motor_speed

Motor speed

ambient, coolant

Ambient and coolant temperature

pm

Permanent magnet surface temperature

stator_winding, stator_tooth, stator_yoke

Stator temperatures

torque

Torque induced by current (the target)

The example uses the first 10 columns (i_d to stator_tooth) as inputs (variables: 10) and predicts torque. The config downloads https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/torque_measurement_dataset.zip. The dataset follows the regression layout described in Regression Dataset Format.

7.10.22.3. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/torque_measurement_regression/config.yaml

7.10.22.4. Configuration

common:
  task_type: generic_timeseries_regression
  target_device: F28P55
dataset:
  dataset_name: torque_measurement
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/torque_measurement_dataset.zip
data_processing_feature_extraction:
  data_proc_transforms:
  - SimpleWindow
  variables: 10
  frame_size: 128
  stride_size: 0.25
training:
  model_name: REGR_10k
  batch_size: 512
  training_epochs: 50
  early_stopping: true
  early_stopping_patience: 5
  num_gpus: 1
  learning_rate: 0.001
  output_int: false
  auto_quantization: true
testing: {}
compilation: {}

num_gpus: 1 expects a GPU; set it to 0 to train on CPU. Try other frame_size and stride_size values to see how they affect training. In the readme experiment the smaller frame (128) gave the better R2 score.

7.10.22.5. Results

The example readme reports these results for two frame sizes (stride size 0.25):

Frame size

Float R2 (MSE)

Quantized R2 (MSE)

Cycles

128

0.994 (12.98)

0.963 (83.59)

114102

256

0.983 (36.82)

0.948 (113.36)

187445

For frame size 128 the readme also reports a test-set RMSE of 9.40, MSE of 88.36 and R2 of 0.98. The cycle counts are taken from the readme and were measured on the device for the quantized model.

7.10.22.6. Output Location

Results are written to ./data/projects/torque_measurement/run/<date-time>/REGR_10k/. The four files needed on the device are compilation/artifacts/mod.a, compilation/artifacts/tvmgen_default.h, training/quantization/golden_vectors/test_vector.c and training/quantization/golden_vectors/user_input_config.h. See Understanding the Run Output.

7.10.22.7. Running on Device

The C2000Ware (or tinyml-sdk) example f28p55x_generic_timeseries_regression takes these four files. Follow Deploying Regression Models from ModelMaker to Device and Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check). Check the test_result variable for the cases in test_vector.c.

7.10.22.8. See Also