8.12.3.3. Running ModelZoo for On-Device Training
8.12.3.3.1. Table of Contents
8.12.3.3.2. 1. Overview
This guide explains how to use TI’s ModelZoo pipeline to generate all the artifacts needed for on-device training on microcontrollers. By the end of this page, you will have a set of files ready to copy into a CCS project for on-device training.
Prerequisites:
tinyml-modelzooinstalled and working (pip install -e .from thetinyml-modelzoofolder, see the repository README)A YAML configuration file with on-device training enabled
For conceptual background on what on-device training is and why it uses a frozen+trainable split, see Overview.
8.12.3.3.3. 2. ODT-Specific YAML Configuration
On-device training builds on the standard YAML configuration used to run the training pipeline in ModelZoo. Most fields (dataset, feature extraction, compilation) are identical to a regular run. Only a few fields are specific to on-device training.
8.12.3.3.3.1. ODT-specific fields
Field |
Example Value |
Description |
|---|---|---|
|
|
Enables the on-device training export pipeline. When set, ModelMaker will split the ONNX model, custom export the trainable portion, and generate training data files. |
|
|
Number of main layers (Linear etc) from the end of the model to keep trainable. The ONNX graph is traversed backward from the output; |
|
|
Number of samples to embed for on-device use, as [train, validation, test]. These samples are exported as C arrays in |
|
|
Must be 0 for on-device training. The trainable portion operates in float32 — quantization is not compatible with on-device weight updates. The frozen portion could theoretically be quantized separately, but the current pipeline exports it as float. |
|
|
Model architecture that supports the frozen+trainable split. The model must produce a linear (sequential) ONNX graph — no branches, skip connections, or cycles. Only supported layer types are allowed in the trainable portion: Gemm (Linear), ReLU, Reshape, and Flatten. Graph-structured models with skip connections etc are not supported for on-device training. |
8.12.3.3.3.2. Fields that are unchanged from standard anomaly detection
All other fields work exactly as documented in the standard anomaly detection pipeline:
dataset— Dataset source, split type, split ratiosdata_processing_feature_extraction— Feature extraction preset, variables, frame concatenationtraining.batch_size,training.training_epochs— PC-side training configuration. Note:training_epochscan be set to0if you want to train entirely on-device.training.learning_rate— PC-side learning rate (the on-device learning rate is configured separately in the C application code)compilation— TVM compilation settings for the frozen model
8.12.3.3.3.3. Complete YAML example
Below is the fan blade on-device training YAML with ODT-specific fields highlighted:
common:
target_module: 'timeseries'
task_type: 'generic_timeseries_anomalydetection'
target_device: 'F28P55'
run_name: '{date-time}/{model_name}'
dataset:
enable: True
dataset_name: fan_blade_ondevice
input_data_path: 'https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/fan_blade_ad_dataset.zip'
split_type: 'amongst_files'
split_factor: [0.6, 0.1, 0.3]
data_processing_feature_extraction:
data_proc_transforms: []
feature_extraction_name: Input256_FFTBIN_16Feature_8Frame_3InputChannel_removeDC_2D1
variables: 3
num_frame_concat: 1
stride_size: 1
training:
enable: True
model_name: 'Ondevice_Trainable_AD_Linear' # ← ODT: model architecture
model_config: ''
batch_size: 64
training_epochs: 200
num_gpus: 0
learning_rate: 0.001
quantization: 0 # ← ODT: must be 0
output_int: False
ondevice_training: True # ← ODT: enables split/export
trainable_layers_from_last: 1 # ← ODT: split point
export_samples_per_class: [10, 10, 10] # ← ODT: [train, val, test]
testing:
enable: True
compilation:
enable: True
compile_preset_name: 'forced_soft_npu_preset'
8.12.3.3.4. 3. Running the Command
Execute ModelZoo with the on-device training YAML:
./run_tinyml_modelzoo.sh examples/fan_blade_fault_classification/fan_blade_anomaly_detection_ondevice_training.yaml
8.12.3.3.4.1. What to expect in the logs
The pipeline runs through the standard anomaly detection flow with additional ODT-specific steps. Here are the key log sections from an actual run (paths abbreviated):
Dataset loading and feature extraction
Loading training data 100%|████████████████████████████| 60/60 [00:08<00:00, 7.42it/s] Loading validation data 100%|████████████████████████████| 10/10 [00:01<00:00, 8.07it/s]
Model creation and summary
Creating model Variables: 3, Input_features: 16 =============================================================================================== AD_3_LAYER_DEEP_ONDEVICE_TRAINABLE_MODEL_TS [1, 3, 16, 1] -- ├─Sequential: 1-1 [1, 24] -- │ └─Flatten: 3-1 [1, 48] -- │ └─Linear: 3-2 [1, 24] 1,176 │ └─ReLU: 3-3 [1, 24] -- │ ... ... ... ├─Linear: 1-2 [1, 48] 1,200 =============================================================================================== Total params: 3,150
Model training (PC-side)
Start training Best Epoch: None MSE inf Exporting model after training.
Note: With
training_epochs: 0, no actual training occurs — the model exports with randomly initialized weights.Best Epoch: NoneandMSE infconfirm this. For non-zero epochs, you will see per-epoch loss values and a valid best epoch.On-device training export (ODT-specific)
Trainable layers from end (k): 6 Searching for split point (k=6 trainable layers from end) Split point found: /frozen_model/encoder/encoder.0/Flatten_output_0 Creating frozen subgraph (input -> /frozen_model/encoder/encoder.0/Flatten_output_0) Extracting trainable layers (from .../Flatten_output_0 -> output) Layer 0: Linear (48->24) Layer 1: ReLU (24->24) Layer 2: Linear (24->12) ... Layer 10: Linear (24->48) Extracted total 11 layers including both main and intermediate layers Flattening weights for 11 layers Total parameters: 3150 Offsets: [0, 1152, 1176, 1464, ..., 3102, 3150] Computing buffer offsets for 11 layers Frozen output size: 48 Generated trainable model config header file at .../trainable_model_config.h Generated trainable model config source file at .../trainable_model_config.c
Golden vector and threshold generation
Creating Golden data for reference at .../golden_vectors Creating test_vector.c at: .../golden_vectors/test_vector.c Creating user_input_config.h at: .../golden_vectors/user_input_config.h
Testing and threshold analysis
Reconstruction Error Statistics: Normal training data - Mean: 5705.585449, Std: 241.798920 Anomaly test data - Mean: 8546.039062, Std: 1576.968628 Threshold for K = 1.5 : 6068.283691 Anomaly detection rate (recall): 99.52% Accuracy: 99.49%
TVM compilation (of frozen model)
TI Model Library Memory Usage (mod.a) ============================================================ Code: 42 bytes ( 0.04 KB) RO Data: 0 bytes ( 0.00 KB) RW Data: 0 bytes ( 0.00 KB) Total: 42 bytes ( 0.04 KB)
Note: The frozen model is only 42 bytes because in this full-model-training configuration (
trainable_layers_from_last: 6), the frozen part contains only a Flatten operation. For partial training configurations, the frozen model will be significantly larger.
8.12.3.3.5. 4. How It Works Under the Hood
When ondevice_training: True is set, the training script adds an extra step after the standard ONNX model export which performs the following:
Load the trained ONNX model
Find split point — traverse the ONNX graph backward from the output, counting main layers. Stop at the k-th one. The input tensor to this layer becomes the split point.
Extract frozen subgraph — copy the graph from input to split point, save as
frozen_model/model.onnxfor TVM compilationExtract trainable layers — traverse forward from split point to output, parsing each layer
Flatten weights — all trainable weights and biases are concatenated into a single contiguous float array with offset tracking
Compute buffer offsets — calculate memory layout for intermediate activations and gradient buffers
Generate C files — write
trainable_model_config.h(architecture, types, layer table) andtrainable_model_config.c(weight data, buffer definitions)
The frozen model ONNX is then compiled by TVM into mod.a through the standard compilation pipeline.
8.12.3.3.6. 5. Output Directory Structure
After a successful run, the ModelMaker output directory contains:
./data/projects/<project_name>/run/<date-time>/<model_name>/ (relative to where you ran the script)
├── training/base/
│ ├── model.onnx # Full trained ONNX model
│ ├── checkpoint.pth # PyTorch checkpoint
│ ├── frozen_model/
│ │ └── model.onnx # Frozen subgraph (for TVM)
│ ├── trainable_model/
│ │ ├── trainable_model_config.h # ★ Trainable architecture + types
│ │ ├── trainable_model_config.c # ★ Trainable weights + buffers
| | ├── ondevice_training_data.h # ★ Dataset dimensions + declarations
| | └── ondevice_training_data.c # ★ Embedded train/val/test data
│ └── golden_vectors/
│ ├── test_vector.c # ★ Golden test vectors
│ └── user_input_config.h # ★ Feature extraction config
│
├── compilation/
│ └── artifacts/
│ ├── mod.a # ★ Compiled frozen model
│ └── tvmgen_default.h # ★ Frozen model API header
(★ = files to copy to CCS project)
8.12.3.3.7. 6. Copying Artifacts to the CCS Project
The following files need to be copied from the ModelMaker output to the CCS project’s artifacts/ directory:
File |
Source (ModelMaker) |
Destination (CCS Project) |
|---|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Compared to a standard (non-ODT) anomaly detection project, the extra files are:
trainable_model_config.h— model architecture for trainable layerstrainable_model_config.c— trainable weight data and buffersondevice_training_data.h— dataset dimensionsondevice_training_data.c— embedded training/validation/test data
8.12.3.3.8. 7. Next Steps
Understand what was generated → Generated Artifacts Overview
Deploy and run on device → Application Example — Fan Blade
Understand the on-device training concepts → Overview