7.10.6. AC Arc Fault

AC arc fault detection is an Edge AI solution for the MSPM0G5187 microcontroller with an on-chip NPU. It detects series arc faults in residential and commercial electrical systems, a leading cause of electrical fires, using ML inference on data captured through the TIDA-010971 analog front end with a PCB Rogowski coil. The goal is Arc Fault Circuit Interrupter (AFCI) products that comply with NEC requirements.

Example folder: examples/ac_arc_fault (GitHub). For DC arc faults, see DC Arc Fault Detection.

7.10.6.1. Overview

  • Task: binary classification (task_type: arc_fault)

  • Device: MSPM0G5187 (Arm Cortex-M0+ with NPU), config config_MSPM0.yaml

  • Dataset: ac_arc_fault_log300_example_dsk

  • Model: CLS_1k_NPU

7.10.6.2. Why AC Arc Fault Detection?

Arc faults cause more than 30,000 home fires each year in the United States, and traditional circuit breakers are not designed to detect low-level arcs. Edge AI enables complex pattern recognition, multi-feature analysis and adaptive detection across load types. The targets of the reference solution are:

Metric

Target

Response time

less than 10 ms

Detection accuracy

more than 95%

Compliance

UL 1699

7.10.6.3. System Components

  • Hardware: MSPM0G5187 and the TIDA-010971 analog front end (PCB Rogowski coil)

  • Software: Code Composer Studio 12.x or later, MSPM0 SDK 2.08.00 or later

7.10.6.4. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/ac_arc_fault/config_MSPM0.yaml

7.10.6.5. Configuration

common:
  task_type: arc_fault
  target_device: MSPM0G5187
dataset:
  dataset_name: ac_arc_fault_log300_example_dsk
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/ac_arc_fault_log300.zip
data_processing_feature_extraction:
  feature_extraction_name: ArcFault_512Input_FE_RFFT_32Feature_8Frame_1InputChannel_removeDC_Full_Bandwidth
  store_feat_ext_data: false
training:
  model_name: CLS_1k_NPU
  batch_size: 30
  training_epochs: 30
  num_gpus: 0
  quantization: 2
  learning_rate: 0.001
  weight_decay: 0.00001
testing: {}
compilation: {}

quantization: 2 enables quantization-aware training (INT8), which is required for the MSPM0G5187 NPU.

7.10.6.6. Dataset

ac_arc_fault_log300.zip contains 100+ captures per load type:

  • Normal operation: inductive loads, LED lighting, switched-mode power supplies, mixed loads

  • Arc faults: series and parallel arc faults

  • Masking loads: dimmer, SMPS, drill, compressor, resistive loads, vacuum cleaner

To prepare and label your own AC arc fault captures use examples/ac_arc_fault/AFCI_LabellingScript.py; instructions are in examples/ac_arc_fault/readme_labelling.md.

7.10.6.7. Feature Extraction

The preset ArcFault_512Input_FE_RFFT_32Feature_8Frame_1InputChannel_removeDC_Full_Bandwidth mirrors the on-device pipeline:

  1. ADC capture: 512 samples at 107 kSps (about 4.76 ms per frame)

  2. 512-point real FFT (ARM CMSIS-DSP on device)

  3. Complex magnitude

  4. DC removal

  5. Binning of 8 adjacent bins, giving 32 features per frame

  6. Normalization to the INT8 range

  7. Concatenation of 8 frames, giving 256 features per input

7.10.6.8. Models

Any enabled classification model can be used. In 1.5.0 the arc fault specific models are enabled in the ModelZoo and can be selected with training.model_name, next to the generic NPU models.

Model

Approx. parameters

Comment

ArcFault_model_200_t

200

Smallest and fastest

ArcFault_model_300_t

300

ArcFault_model_700_t

800

Balance of speed and memory

ArcFault_model_1400_t

1,600

Most accurate

CLS_500_NPU / CLS_1k_NPU / CLS_2k_NPU / CLS_4k_NPU

500 to 4,000

Generic NPU models (CLS_1k_NPU is the default in the config)

7.10.6.9. Results

The example readme.md reports these figures for the reference solution on MSPM0G5187 with NPU (recommended model, 8-frame voting):

Metric

Value

End-to-end latency

less than 150 ms

Detection accuracy

more than 99%

False positive rate

0.01%

Precision / Recall / F1

99.97% / 99.72% / 99.84%

In the 1.5.0 config test run, config_MSPM0.yaml with CLS_1k_NPU reached a test accuracy of 99.64% with an AUC ROC of 1.000.

7.10.6.10. Training and Deployment Flow

Running the config performs feature extraction, training, INT8 quantization and compilation with the TI Neural Network Compiler, producing the model library and interface headers for the MSPM0 SDK. See Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check) and NPU Device Deployment.

7.10.6.11. References

See also DC Arc Fault Detection and Classification Dataset Format.