7.10.14. Human Activity Recognition

Classify human activities from smartphone accelerometer data (WISDM dataset). The example also shows support for residual connections and how to change model parameters with model_config.

Example folder: examples/human_activity_recognition (GitHub). This folder was named branched_model_parameters in the 1.4.0 documentation.

7.10.14.1. Overview

The WISDM (WIreless Sensor Data Mining) dataset is a public dataset of smartphone sensor recordings used for activity recognition. See the WISDM site for the activity list.

  • Application: wearables, fitness trackers, smart home, elderly care

  • Task: classification (generic_timeseries_classification)

  • Data: 3 variables (accelerometer X, Y, Z), 128-sample windows

  • Dataset: wisdm_example from https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/wisdm_dataset.zip

  • Device: F28P55

  • Model: CLS_ResCat_3k (residual/concatenation architecture)

7.10.14.2. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/human_activity_recognition/config.yaml

7.10.14.3. Configuration

common:
  task_type: generic_timeseries_classification
  target_device: F28P55
dataset:
  dataset_name: wisdm_example
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/wisdm_dataset.zip
data_processing_feature_extraction:
  data_proc_transforms:
  - SimpleWindow
  frame_size: 128
  stride_size: 0.01
  variables: 3
training:
  model_name: CLS_ResCat_3k
  model_config: examples/human_activity_recognition/residual_network_config.yaml
  batch_size: 32
  training_epochs: 10
  early_stopping: true
  early_stopping_patience: 5
  num_gpus: 0
testing: {}
compilation: {}

7.10.14.4. Preparing the WISDM Dataset

The config downloads the prepared zip automatically. To rebuild it yourself, run python wisdm.py in the example folder (requires requests and pandas): it downloads the raw WISDM data, cleans it, splits each class into NUM_SPLITS files and zips the result in the format expected by ModelZoo.

7.10.14.5. The CLS_ResCat_3k Model

CLS_ResCat_3k ONNX graph

CLS_ResCat_3k with residual connections

The model has an input batch normalization followed by two branches. The first branch has three convolution layers, the second a single convolution. The branch outputs are concatenated, pooled, flattened and fed to a fully connected layer.

The channel counts are configurable through training.model_config, which points to residual_network_config.yaml:

out_channel_layer1: 8
out_channel_layer2: 16
out_channel_layer3: 32

7.10.14.6. Comparison of Models

The example readme.md compares three models on this dataset (results measured with an earlier release):

Model

Parameters

Accuracy

AUC ROC

CLS_1k_NPU

1,316

94.92%

0.995

CLS_ResCat_3k

3,132

93.84%

0.965

CLS_13k_NPU

14,124

94.45%

0.987

The purpose of the example is to demonstrate residual connections, not to show that CLS_ResCat_3k is better than the other models.

In the automated 1.5.0 config test run, config.yaml reached a test accuracy of 88.87% with an AUC ROC of 0.931 (900 parameters reported in that log). The shipped config uses only 10 epochs, so expect results to vary between runs.

7.10.14.7. See Also