8.12.3.11. Integer On-Device Training Documentation

8.12.3.11.1. Table of Contents


8.12.3.11.2. Introduction

Integer on-device training (integer ODT) enables deep learning models to continue training directly on TI microcontrollers using pure integer arithmetic. Unlike the float ODT framework which uses 32-bit floating point throughout the training pass, integer ODT works entirely in INT8 weights, INT32 accumulators, and integer-only gradient updates.

Float ODT:    Train on PC (float) → Deploy → Train on device with float32 math
Integer ODT:  Train on PC (QAT)   → Deploy → Train on device with INT8/INT32 math

Why integer? The Cortex-M33 and similar MCUs can execute integer MAC operations significantly faster than float. INT8 weights take one quarter the RAM of float weights, freeing memory for larger models or larger training batches. And if needed, we can later extend the inference to happen on NPU if available.

The current example targets the arc fault classification application on the AM13E230X LaunchPad (M33 core), but the C library is device-agnostic and works on any MCU.


8.12.3.11.3. How This Differs from Float ODT

If you are already familiar with the float ODT framework, here is what changes:

Aspect

Float ODT

Integer ODT

YAML quantization

0 (float)

2 (QAT, required)

Weight representation

float32

INT8

Gradient arithmetic

float32

INT32 accumulate, INT8 store

Learning rate method

Fixed SGD step

NITI dynamic shifts (mu_weight, mu_offset)

Activation buffers

float32

8 bit integer activations

Training C library

ondevice_training_lib.h/.c

integer_odl.h/.c

Config file name

trainable_model_config.h/.c

integer_model_config.h/.c

Training data file

ondevice_training_data.h/.c

train_data.h/.c

Supported layers

Linear, Conv2d, ReLU

Conv2D, Linear, ReLU

For background on what on-device training is and why the frozen+trainable split architecture is used, see the float ODT Overview. Those concepts apply equally here.


8.12.3.11.4. What You Need

Requirement

Details

Hardware

AM13E230X LaunchPad

SDK

AM13E230X SDK with TI ARM Clang toolchain

IDE

Code Composer Studio (CCS)

ModelMaker

tinyml-modelzoo installed and working (it pulls in ModelMaker; see the repository README)

Baseline working

The standard (non-ODT) arc fault classification example should build and run before attempting integer ODT. This verifies your SDK, CCS, and hardware setup are correct.


8.12.3.11.5. Key Concepts

8.12.3.11.5.1. Integer Arithmetic

Standard backpropagation in float computes gradients like:

weight_new = weight - lr * gradient

Integer ODT does the same computation in integer form using the NITI algorithm. The key insight is that gradient magnitudes vary widely during training, rather than using a fixed shift to fit gradients into INT8 range, NITI measures the actual gradient magnitude each batch and computes the minimum shift needed:

shift = max(0, ceil(log2(max_gradient)) - target_bits)
quantized_gradient = round(gradient >> shift)
weight_new = sat_int8(weight - quantized_gradient)

This adaptive scaling keeps gradients in INT8 range without overflow while preserving as much precision as possible. The effective learning rate is controlled by two parameters in IntModelCtx_t:

  • mu_weight: learning rate for weight updates (default: 1)

  • mu_offset: learning rate for bias/offset updates (default: 1)

Higher mu → smaller effective shift → larger learning rate. See Integer ODL Library for the full math.

8.12.3.11.5.2. No PREQUANT Layer in the C Library

The float-to-INT8 quantization step (the PREQUANT block in the ONNX graph) does not appear in INT_LAYERS[]. Instead it is compiled into the TVM frozen model and handled by the NPU. The C library receives INT8 data directly from TVM’s output, with no float-to-int conversion needed at runtime.

For full model ODT (all compute layers trainable): TVM compiles only the PREQUANT block. Its output is INT8 and feeds directly into INTODT_Forward.

For partial model ODT (last k layers trainable): TVM compiles the PREQUANT block plus the frozen compute layers. Its output is UINT8 (the RELU output of the last frozen layer) and feeds directly into INTODT_Forward.

8.12.3.11.5.3. Activation Buffer Types

Because the model computes in integer arithmetic, intermediate activations have different types depending on whether the layer has ReLU:

  • RELU layers (INT_LAYER_CONV2D_RELU, INT_LAYER_LINEAR_RELU): outputs are in [0, 255], stored as uint8_t

  • Non-RELU layers (INT_LAYER_CONV2D, INT_LAYER_LINEAR): outputs are in [-128, 127], stored as int8_t

The C library handles this automatically. You do not need to cast or convert between the two.

8.12.3.11.5.4. Supported Layer Types

Type

Training support

Conv2D (no ReLU)

Yes

Conv2D + ReLU

Yes

Linear / MatMul (no ReLU)

Yes

Linear / MatMul + ReLU

Yes


8.12.3.11.6. Quickstart

This walkthrough uses the arc fault classification example. By the end, you will have a model that was fine-tuned on-device using integer arithmetic.

8.12.3.11.6.1. Step 1: Configure YAML

Add these fields to your arc fault classification YAML, or use the example YAML directly:

training:
    quantization: 2                       # Required: QAT (integer weights)
    ondevice_training: true               # Enable integer ODT export pipeline
    trainable_layers_from_last: 3         # 3 compute layers 
    export_samples_per_class: '[10,5,5]'  # [train, val, test] samples per class

Critical: quantization: 2 is mandatory. The integer ODT pipeline requires QAT, the weights must already be quantized to INT8 before export. Running with quantization: 0 (float) will not generate integer ODT artifacts.

For full YAML details see Running ModelMaker for Integer ODT.

8.12.3.11.6.2. Step 2: Run ModelMaker

./run_tinyml_modelzoo.sh examples/dc_arc_fault/config_dsi_ondevice_learning.yaml

This runs QAT training, then additionally:

  • Parses the QAT ONNX graph (identifies Conv, Linear, PREQUANT blocks)

  • Analyzes output distribution → derives TARGET_MAG_CORRECT/WRONG per class

  • Exports integer_model_config.h/.c with INT8 weights and layer descriptors

  • Exports train_data.h/.c with float training samples and INT8 labels

  • Saves frozen_model/model.onnx at the correct split point for TVM

  • TVM compiles frozen_model/model.onnx → mod.a + tvmgen_default.h

8.12.3.11.6.3. Step 3: Copy Artifacts to CCS Project

Import the arc_fault_odl example from the SDK into CCS:

  1. File → Import → CCS Projects

  2. Browse to tinyml-sdk/am13/ai/examples/arc_fault_odl/

  3. Import

Then copy these files from the ModelMaker output into artifacts/ in the imported project:

File

ModelMaker output path

mod.a

<run_dir>/compilation/artifacts/mod.a

tvmgen_default.h

<run_dir>/compilation/artifacts/tvmgen_default.h

integer_model_config.h

<run_dir>/training/quantization/integer_model_config/integer_model_config.h

integer_model_config.c

<run_dir>/training/quantization/integer_model_config/integer_model_config.c

train_data.h

<run_dir>/training/quantization/integer_model_config/train_data.h

train_data.c

<run_dir>/training/quantization/integer_model_config/train_data.c

test_vector.c

<run_dir>/training/quantization/golden_vectors/test_vector.c

user_input_config.h

<run_dir>/training/quantization/golden_vectors/user_input_config.h

For exact file-by-file instructions see Running ModelMaker: Copying Artifacts.

8.12.3.11.6.4. Step 4: Build, Flash, and Run

  1. Select the Flash build configuration in CCS

  2. Build the project

  3. Connect your AM13E230X LaunchPad and flash

  4. Open the CCS console, you should see something like below output:

============================================================
  INPUT_SIZE=128  N_CLASSES=2  BATCH_SIZE=8  EPOCHS=30  N_SAMPLES=20
============================================================

Accuracy BEFORE ODL: 7 / 20  (35.0%)

The application evaluates accuracy with the freshly-deployed (barely trained) model, then runs the training loop, then re-evaluates:

Epoch [1/30]   Loss: 183204.0000
Epoch [2/30]   Loss: 112847.0000
...
Epoch [30/30]  Loss: 1243.5000

Accuracy AFTER  ODL: 20 / 20  (100.0%)
Done.

8.12.3.11.7. Documentation Map

8.12.3.11.7.1. 1. Overview

What integer ODT is, why integer arithmetic, how NITI works, the frozen+trainable split for integer models, full vs partial model modes, memory layout, supported configurations, and current limitations. Start here if you want to understand the architecture before using it.

8.12.3.11.7.2. 2. Running ModelMaker for Integer ODT

Step-by-step guide to generating artifacts. Covers every ODT-specific YAML field with explanation, a complete working YAML, the exact command to run, console log walkthrough, output directory structure, and file-by-file copy guide for the CCS project.

8.12.3.11.7.3. 3. Generated Artifacts Overview

A map of all generated files, what each contains, and how they connect at runtime. Read this if you want to understand what ModelMaker produces before diving into individual files.

8.12.3.11.7.4. 4. Integer Model Configuration

Deep dive into integer_model_config.h and integer_model_config.c. Covers every #define, the IntLayerDesc_t structure field by field, IntModelCtx_t, weight/k/offset arrays, activation buffer layout, ReLU mask memory, and grad_buf sizing.

8.12.3.11.7.5. 5. Training Data

Deep dive into train_data.h and train_data.c. Covers data layout, label encoding, why inputs are float (and the partial model limitation), and how the training loop iterates through these arrays.

8.12.3.11.7.6. 6. Integer ODL Library: API Reference

Complete API reference for integer_odl.h/.c. Covers all three public functions (INTODT_Infer, INTODT_Forward, INTODT_Backward), the NITI shift calculation with worked examples, conv/linear forward and backward math, the user loss function pattern, and a complete custom training loop.


8.12.3.11.8. Reading Paths

New to on-device training entirely? → Read the float ODT Overview first for concepts, then come back here.

Familiar with float ODT, switching to integer? → How This Differs from Float ODT → Overview → Running ModelMaker

Just want to get it working quickly? → Quickstart → Running ModelMaker

Understanding the generated files? → Generated Artifacts Overview → Integer Model Configuration → Training Data

Writing your own training loop / adapting main.c? → Integer ODL Library (Section: Writing a Complete Training Loop)