7.10.20. Dynamic Hand Gesture Recognition
Real-time dynamic hand gesture classification from 3-axis accelerometer data on the MSPM0G5187 with integrated NPU.
Example folder: examples/dynamic_hand_gesture_recognition
(GitHub)
7.10.20.1. Overview
Buttons and touchscreens are impractical in hands-free or hygienic environments, rule-based gesture logic is brittle against natural variation, and cloud recognition adds latency and privacy concerns. This example classifies gestures directly on the MCU.
Task: multi-class classification (4 classes),
generic_timeseries_classificationApplication: gesture-based human-machine interface
Sensor: 3-axis accelerometer of the TI Sensor BoosterPack
Device: MSPM0G5187 (
config_MSPM0.yaml, the only config)Model:
CLS_55k_NPU(about 55K parameters)
7.10.20.2. Gesture Classes
Circle: clockwise or counter-clockwise circular motion
Wave: side-to-side waving motion
Tap: short impact gesture
Others: non-gesture or unrecognized motion
7.10.20.3. System Components
Hardware: MSPM0G5187 with integrated NPU, TI Sensor BoosterPack
Software: Code Composer Studio 12.x or later, MSPM0 SDK 2.10.04 or later
7.10.20.4. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the
tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/dynamic_hand_gesture_recognition/config_MSPM0.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\dynamic_hand_gesture_recognition\config_MSPM0.yaml
7.10.20.5. Configuration
common:
task_type: generic_timeseries_classification
target_device: MSPM0G5187
dataset:
dataset_name: hand_gesture_dataset
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/hand_gesture_dataset.zip
split_type: within_files
gof_test: true
data_processing_feature_extraction:
feature_extraction_name: HandGesture256Input_RangeNormalize_1Frame
training:
model_name: CLS_55k_NPU
batch_size: 30
learning_rate: 0.001
training_epochs: 40
num_gpus: 0
gof_test: true
auto_quantization: false
testing:
enable: true
compilation:
enable: true
7.10.20.6. Feature Extraction
The preset HandGesture256Input_RangeNormalize_1Frame uses raw time-domain data (no FFT):
Raw 3-axis (X, Y, Z) accelerometer data
Windowing: 256 samples per frame
Stride 0.25 (frames overlap with a step of 64 samples)
Range normalization per frame, which captures the gesture amplitude and shape
A single frame is passed to the model
gof_test: true additionally runs the Goodness of Fit analysis of class separability.
7.10.20.7. Training and Deployment
The example uses batch size 30, learning rate 0.001, the default SGD optimizer and 40 epochs. The model is quantized to INT8 and compiled with the TI Neural Network Compiler for the NPU. See Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check) and NPU Device Deployment.
7.10.20.8. Results
The example readme reports an accuracy of about 94.46% on the test data. In the automated 1.5.0 config test run,
config_MSPM0.yaml reached a test accuracy of 94.08% with an AUC ROC of 0.993 (52,434 parameters).
7.10.20.9. See Also
Human Fall Detection and Human Activity Recognition: other accelerometer examples