5.2. Regression Dataset Format

This guide explains how to format datasets for time series regression tasks.

5.2.1. Directory Structure

Regression datasets use a flat files/ folder structure (not class folders):

my_dataset/
├── files/                          # MUST be named "files"
│   ├── datafile1.csv
│   ├── datafile2.csv
│   └── datafileN.csv
└── annotations/                    # Optional - auto-generated if missing
    ├── instances_train_list.txt
    └── instances_val_list.txt

Important

The data directory must be named files/, not classes/ or anything else.

5.2.2. Data File Format

Critical: The target value must be in the last column.

feature1,feature2,feature3,...,target
0.5,18.2,45.5,...,0.187
0.6,18.5,45.6,...,0.245
...

Example: Motor Torque Prediction

current_d,current_q,voltage_d,voltage_q,motor_speed,pm_temp,target_torque
-0.450,0.032,18.805,1.499,0.002,24.55,0.187
-0.325,0.045,18.818,1.542,0.003,24.54,0.245
-0.440,0.028,18.876,1.456,0.002,24.54,0.176
  • Columns 1-6: Input features

  • Column 7 (last): Target value to predict

5.2.3. Time Column Handling

Any column containing “time” is automatically dropped:

Time,feature1,feature2,target
0.001,0.5,18.2,0.187
0.002,0.6,18.5,0.245

The “Time” column will be removed automatically.

5.2.4. Annotation Files (Optional)

Annotation files list the files that belong to each split, one name per line (relative to files/). Providing them is recommended for regression so that the train/val/test split is reproducible:

instances_train_list.txt:

datafile1.csv
datafile3.csv
datafile5.csv

instances_val_list.txt:

datafile2.csv
datafile4.csv

instances_test_list.txt (optional):

datafile6.csv

If you don’t provide annotations, ModelMaker auto-generates them using split_type and split_factor (see Data Splitting).

5.2.5. Configuration

dataset:
  enable: True
  dataset_name: 'my_regression_data'
  input_data_path: '/path/to/my_dataset'
  data_dir: 'files'
  annotation_dir: 'annotations'

data_processing_feature_extraction:
  data_proc_transforms: ['SimpleWindow']  # Required!
  frame_size: 128
  stride_size: 0.25
  variables: 6                            # Input columns (excluding target)

Important

SimpleWindow transform is required for regression tasks.

5.2.6. Target Processing

The target value (last column) is processed as follows:

  1. Each window of frame_size rows is extracted

  2. The target value is averaged across the window

  3. This averaged value becomes the label for that window

Example with frame_size=4:

Window 1: rows 0-3, targets [0.18, 0.24, 0.17, 0.19] → avg = 0.195
Window 2: rows 2-5, targets [0.17, 0.19, 0.22, 0.20] → avg = 0.195

5.2.7. Complete Example

Dataset structure:

torque_measurement/
├── files/
│   ├── experiment_001.csv
│   ├── experiment_002.csv
│   ├── experiment_003.csv
│   └── experiment_004.csv
└── annotations/
    ├── instances_train_list.txt    # experiment_001.csv, experiment_002.csv
    └── instances_val_list.txt      # experiment_003.csv, experiment_004.csv

experiment_001.csv:

i_d,i_q,u_d,u_q,speed,temp,torque
-0.45,0.03,18.80,1.49,0.002,24.5,0.187
-0.32,0.04,18.81,1.54,0.003,24.5,0.245
...

config.yaml (excerpt; see examples/generic_timeseries_regression/config.yaml for a tested config):

common:
  task_type: 'generic_timeseries_regression'
  target_device: 'F28P55'

dataset:
  dataset_name: 'torque_measurement'
  input_data_path: '/data/torque_measurement'

data_processing_feature_extraction:
  data_proc_transforms: ['SimpleWindow']
  frame_size: 128
  stride_size: 0.25
  variables: 6

training:
  model_name: 'REGR_2k_NPU'
  training_epochs: 100      # early stopping (on by default) may end training sooner

5.2.8. Troubleshooting

“Target column not found” error

The target variable must be in the last column of every CSV file. If your target is not the last column, either reorder the columns or specify target_variables explicitly in the configuration. Double-check that no extra trailing delimiter is creating a phantom empty column after your intended target.

“Insufficient sequence length” error

Each data file must contain enough rows to produce at least one window. The minimum row count per file is:

frame_size + (stride as absolute rows)

For example, with frame_size=128 and stride_size=0.25 (which translates to a stride of 32 rows), you need at least 128 rows per file. If files are shorter, either increase their length or reduce frame_size.

Incomplete annotation files

If some but not all of the split lists (train, val, test) exist in annotations/, ModelMaker regenerates all of them. Provide either the complete set of lists or none; with none, splits are generated automatically.

“Data dimension mismatch” error

All CSV files in the files/ directory must have the same number of columns. Verify that:

  • No files have extra or missing columns

  • The variables parameter in the config matches the actual number of input feature columns (i.e., total columns minus the target column, minus any auto-dropped time column)

  • Delimiters are consistent across all files

“Time column” gotcha

Warning

Do not name any feature column with the word “time” (case-insensitive). Any column whose header contains “time” (e.g., Time, Timestamp, TIME (microsec)) is automatically dropped during data loading. If you need a temporal feature, use a name like elapsed_sec or sample_index instead.

5.2.9. Best Practices

  • Use consistent column ordering across all files in the dataset. Every CSV should have the same columns in the same order.

  • Avoid naming columns “time”. Use timestamp, elapsed_sec, or sample_index if you need a temporal reference column, since any column with “time” in its name is silently dropped.

  • Ensure numerical-only data. All values (except the optional header row) must be numeric (integers or floats). String values, NaN entries, or missing fields will cause errors during data loading.

  • Include enough variety in the target range for the model to generalize. If all target values cluster in a narrow range, the model may fail to learn meaningful regression. Aim for training data that covers the full expected operating range of the target variable.

  • Remove outliers and NaN values before preparing the dataset. Extreme outliers can disproportionately affect MSE-based training.

  • Use descriptive filenames (e.g., motor_test_001.csv) to make annotation files easier to manage.

  • Test with a small subset first to validate the dataset format before launching a full training run.

5.2.10. Common Issues

“Target not found” error

Ensure the target is in the last column of your CSV.

“No windows generated” error

Check that files have at least frame_size rows.

Poor regression performance

  • Try different frame_size values

  • Ensure input features are relevant to target

  • Normalize extreme values in your data

5.2.11. See Also