5.4. Anomaly Detection Dataset Format
This page describes how to format your dataset for anomaly detection tasks
(generic_timeseries_anomalydetection).
5.4.1. Folder Structure
For anomaly detection tasks, ModelMaker expects the dataset to be organized with separate folders for Normal and Anomaly data:
dataset_name/
|
+-- classes/
| +-- Normal/
| | +-- file1.csv
| | +-- file2.csv
| | +-- ...
| +-- Anomaly/
| +-- file1.csv
| +-- file2.csv
| +-- ...
|
+-- annotations/ # Optional
+-- file_list.txt # List of all files
+-- instances_train_list.txt # Training files (Normal only)
+-- instances_val_list.txt # Validation files (Normal only)
+-- instances_test_list.txt # Test files (Normal + Anomaly)
Warning
Training uses ONLY normal data. The Anomaly/ folder is excluded
from training entirely. Anomaly data is used only for testing to
evaluate detection performance.
Key points:
Normal/ folder: Contains all samples representing normal operating conditions. All training and validation data comes from this folder.
Anomaly/ folder: Contains samples representing anomalous behavior (faults, failures, defects). Used ONLY for testing, never for training.
annotations/ folder: Optional. If not provided, ModelMaker automatically generates the annotation files based on your
split_typeandsplit_factorsettings.Multiple anomaly types (e.g., imbalance, damage, bearing wear) all go in the same
Anomaly/folder. The model treats them all as “not normal” and does not distinguish between different anomaly types.
5.4.2. Concrete Example
fan_blade_ad_dataset.zip/
|
+-- classes/
| +-- Normal/
| | +-- normal_001.csv
| | +-- normal_002.csv
| | +-- ...
| | +-- normal_100.csv # 100 normal samples
| |
| +-- Anomaly/
| +-- imbalance_001.csv
| +-- imbalance_002.csv
| +-- damage_001.csv
| +-- obstruction_001.csv
| +-- ...
| +-- obstruction_005.csv # 20 anomaly samples (mixed types)
|
+-- annotations/ # Optional - auto-generated if missing
+-- file_list.txt
+-- instances_train_list.txt
+-- instances_val_list.txt
+-- instances_test_list.txt
5.4.3. Data Splitting Strategy
Normal data is split into train, validation, and test sets. Anomaly data is used only in the test set.
Split |
Normal Data |
Anomaly Data |
Purpose |
|---|---|---|---|
Training |
60% of Normal files |
None |
Learn what “normal” looks like |
Validation |
10% of Normal files |
None |
Monitor overfitting on normal patterns |
Test |
30% of Normal files |
All Anomaly files |
Evaluate detection performance |
Configure splitting in your YAML:
dataset:
split_type: 'amongst_files' # or 'within_files'
split_factor: [0.6, 0.1, 0.3] # [train, val, test]; the default is [0.6, 0.3, 0.1]
Two split methods are available:
amongst_files (default): Files are divided into train, validation, and test sets. For example, with 100 normal files and
split_factor: [0.6, 0.1, 0.3], you get 60 files for training, 10 for validation, and 30 for testing.within_files: Each file is split internally. All files appear in all splits with different portions. For example, each file contributes its first 60% of samples to training, next 10% to validation, and last 30% to testing.
Note
If you do not provide an annotations/ folder, ModelMaker automatically
generates annotation files. For amongst_files, it randomly splits
normal files according to the split factor and adds all anomaly files to
the test list. For within_files, it creates new files for each split
portion.
5.4.4. What If You Don’t Have Anomaly Data?
It is common, especially early in a project, to have collected normal operating data but no examples of anomalies.
What You CAN Do Without Anomaly Data:
Train the model: Training only requires normal data.
Set a conservative threshold: ModelMaker computes
mean + 3 * stdof the reconstruction error on the normal training data and writes it asRECONSTRUCTION_ERROR_THRESHOLDinto the generateduser_input_config.h. Use it as a starting point.Deploy and monitor: Deploy the model and monitor reconstruction error in real time. Samples exceeding the threshold can be flagged for review.
What You CANNOT Do Without Anomaly Data:
Measure anomaly detection performance: Without anomaly samples, you cannot calculate recall, precision, or F1 score.
Validate detection capability: You can only verify the model does not produce false alarms on normal data.
Note
Once deployed, you can collect anomaly samples as they naturally occur.
These can then be added to the Anomaly/ folder and used to re-run the
testing step to get proper metrics and judge whether the default threshold suits your data.
5.4.5. Datafile Format (CSV)
ModelMaker supports .csv, .txt, .npy, and .pkl file formats.
Within CSV files, two layouts are accepted:
Headerless format (no header row, no index column):
2078
2136
2117
2077
2029
Headered format (with column names, optionally with a time/index column):
Time,Vibration_X,Vibration_Y,Vibration_Z
0.0000,-2753,-558,64376
0.0001,-2551,-468,63910
0.0002,-424,-427,64032
Warning
Any column with the text time in its header (case-insensitive) is
automatically dropped by ModelMaker. If you have a useful column that
contains “time” in its name, rename it before using the dataset.
For multi-channel data (e.g., 3-axis accelerometer), specify the number of variables in your configuration:
data_processing_feature_extraction:
variables: 3 # X, Y, Z axes
5.4.6. See Also
Anomaly Detection - Anomaly detection task type overview
Classification Dataset Format - Classification dataset format
Data Splitting - Data splitting strategies
Generic Timeseries Anomaly Detection - Complete example
Early Stopping - Early stopping (default on in 1.5.0; monitors the validation reconstruction MSE)