6.6. Connectivity, AM26x, MSPM33 and Radar Devices
This page covers the device families that do not have a page of their own: the SimpleLink connectivity MCUs (CC27xx, CC13xx, CC35xx), the AM26x Arm Cortex-R5F family, the MSPM33C family, and the xWRL6432 radar sensor. For the per-device task matrix, SDK example and memory-estimation support see Device Overview. AM13E2 is listed in Device Overview as well; it has a hardware NPU (see NPU Guidelines).
Note
The tinyml-sdk repository ships on-device AI examples for C2000 (c28, c29), AM13
and AM26 only. There are no Tiny ML ModelZoo SDK examples for the CC,
MSPM33 or xWRL6432 devices. For those devices ModelMaker produces the compiled model
library and golden vectors, and you integrate them into your own SimpleLink / MSPM33 /
mmWave project. The hardware numbers for the CC devices in the 1.4.0 guide
(flash, RAM, energy per inference, recommended model sizes) could not be verified against
1.5.0 sources and are not repeated here; use the device data sheets.
6.6.1. Connectivity Devices (CC)
No CC device has a hardware NPU (only F28P55, MSPM0G5187, AM13E2 and MSPM33C34 do). They use
one of two compilation styles, set in tinyml-modelmaker (timeseries/constants.py).
|
Compiler core flags |
Compilation style |
|---|---|---|
CC2755, CC2745 |
Cortex-M33, |
Default preset uses the Arm Custom Datapath Extension (CDE), |
CC35X1 |
Cortex-M33, |
Same as CC2755: CDE preset by default, soft preset available. |
CC1354, CC1314 |
Cortex-M33, |
Software (soft) preset only. |
CC1352, CC1312 |
Cortex-M4F, |
Software (soft) preset only. |
Note
The 1.4.0 guide listed CC2755, CC1352, CC1354 and CC35X1 (as a Cortex-M4 Wi-Fi part). In 1.5.0 the device list also contains CC2745, CC1312 and CC1314, and the compiler flags for CC35X1 are those of a Cortex-M33 with CDE. The CC devices are listed by classification, motor fault and PIR detection models (see Device Overview); regression, forecasting and anomaly-detection models do not list them.
Example configuration:
common:
task_type: 'generic_timeseries_classification'
target_device: 'CC2755'
compilation:
enable: True
Choose a model that lists your device; ModelMaker rejects a model that does not.
6.6.2. AM26x (AM263, AM263P, AM261)
Arm Cortex-R5F devices (VFPv3-D16 floating point), compiled without an NPU. AM263 supports
classification, arc fault, motor fault, blower imbalance, regression, forecasting and anomaly
detection models; AM263P and AM261 support classification, regression, forecasting and anomaly
detection (see Device Overview). The tinyml-sdk folder am26/ai/examples
contains the same twelve example projects as the AM13 folder (arc_fault, blower_imbalance,
fan_blade_anomalydetection, forecasting_pmsm_rotor_temp, generic_timeseries_*,
hvac_indoor_temp_forecast, motor_fault, torque_measurement, washing_machine_load_weighing).
Deployment follows Non-NPU Deployment.
6.6.3. MSPM33C (MSPM33C32, MSPM33C34)
Arm Cortex-M33 devices. MSPM33C32 is a CPU-only target (MSPM33 SDK mspm33c321a).
MSPM33C34 has an NPU compilation profile and is accepted on the command line, but no
1.5.0 model lists it, so every task is rejected for it. Use MSPM33C32 for MSPM33 projects.
6.6.4. xWRL6432 (Radar)
The xWRL6432 mmWave radar sensor (Arm Cortex-M4F, no NPU) is the target of the radar tasks (point cloud and surface classification) and the only device they list.
6.6.5. Where to Go Next
Device Overview for the complete device matrix
Non-NPU Deployment for CPU-only deployment
Deployment for the deployment guides