8.12.3.7. On-Device Training Library

8.12.3.7.1. Table of Contents


8.12.3.7.2. 1. Overview

The ondevice_training_lib is the core neural network training engine for on-device training on TI microcontrollers. It provides the fundamental building blocks — forward pass, backward pass, weight updates, loss computation — that any task-specific library can use to implement on-device training.

Key design principles:

  • Task-agnostic: This library knows nothing about classification, anomaly detection etc. It only knows about layers, weights, gradients, and loss.

  • Zero dynamic allocation: All memory is statically allocated via trainable_model_config.c. The library only uses pointers into these pre-allocated arrays.

  • Flat array architecture: All weights, buffers, and gradients live in single contiguous arrays accessed via offsets.

  • Compile-time optimization: Batch size = 1 eliminates gradient accumulation code entirely via #if USE_GRADIENT_ACCUMULATION.

8.12.3.7.2.1. Where it fits

┌─────────────────────────────────────────┐
│         Application Code                │
│    (application_main.c)                 │
├─────────────────────────────────────────┤
│      Task Library                       │
│    (anomaly_detection_odt)              │  ← Orchestrates training workflow
├─────────────────────────────────────────┤
│      Core Training Library              │
│    (ondevice_training_lib)              │  ← THIS LIBRARY: forward, backward, SGD
├─────────────────────────────────────────┤
│      Model Configuration                │
│    (trainable_model_config.h/.c)        │  ← Layer definitions, weights, buffers
└─────────────────────────────────────────┘

8.12.3.7.2.2. Source files

File

Location

Purpose

ondevice_training_lib.h

tinyml-sdk/c29/ai/common/ondevice_training/

API declarations, ModelContext_t structure, logging macros

ondevice_training_lib.c

tinyml-sdk/c29/ai/common/ondevice_training/

All function implementations


8.12.3.7.3. 2. Data Structures

8.12.3.7.3.1. 2.1 ModelContext_t — The Central Training State

Every function in this library takes a ModelContext_t* as its first argument. This structure holds the complete state of the trainable model.

Fields:

Field

Type

Description

layers[]

LayerParams_t[NUM_TRAINABLE_LAYERS]

Layer descriptors copied from LAYER_PARAMS_INIT during init

num_layers

uint16_t

Number of layers in trainable model

intermediate_buffers[]

float*[NUM_TRAINABLE_LAYERS + 1]

Pointers into INTERMEDIATE_BUFFERS. Index 0 = frozen model output (input to first layer). Index i = output of layer i-1

gradient_buffers[]

float*[NUM_TRAINABLE_LAYERS + 1]

Pointers into GRADIENT_BUFFERS. Index i+1 = gradient flowing backward into layer i (input to layer i’s backward pass). Index i = gradient flowing backward out of layer i (output of layer i’s backward pass). Last index is gradient of loss function w.r.t outputs. Index 0 is gradient w.r.t. inputs of trainable model

current_weights

float*

Points to ALL_WEIGHTS — the active model parameters being updated during training

best_weights

float*

Points to ALL_BEST_WEIGHTS — checkpoint storage for the best-performing weights

weight_gradients

float*

Points to ALL_WEIGHT_GRADS — accumulated gradients for batch training. Only exists when USE_GRADIENT_ACCUMULATION is 1

batch_sample_count

uint16_t

Number of samples processed in the current batch

is_training_mode

TrainingPhase_t

Current phase: PHASE_TRAINING or PHASE_INFERENCE

learning_rate

float

SGD learning rate for weight updates

How memory is organized:

All three flat arrays follow the same indexing pattern, illustrated here with a simple 3-layer example: Linear(4→3), ReLU(3), Linear(3→2) and a loss function(FROZEN_OUTPUT_SIZE=4, FINAL_OUTPUT_SIZE=2, NUM_TRAINABLE_LAYERS=3).

ALL_WEIGHTS — all trainable parameters packed sequentially:

ALL_WEIGHTS[TOTAL_PARAMS]   (TOTAL_PARAMS = 4×3 + 3 + 3×2 + 2 = 23)
┌──────────────────┬─────────────┬──────────────────┬─────────────┐
│ Layer 0 weights  │ Layer 0     │ Layer 2 weights  │ Layer 2     │
│ W[3×4] = 12      │ biases = 3  │ W[2×3] = 6       │ biases = 2  │
└──────────────────┴─────────────┴──────────────────┴─────────────┘
 offset=0           offset=12    offset=15          offset=21

(Layer 1 is ReLU — no weights, so it occupies no space in ALL_WEIGHTS)

INTERMEDIATE_BUFFERS — forward pass activations, one slot per layer boundary:

INTERMEDIATE_BUFFERS[TOTAL_INTERMEDIATE_BUFFER_SIZE]   (= 4 + 3 + 3 + 2 = 12)
┌─────────────┬────────────────┬────────────────┬────────────────┐
│  buffer[0]  │   buffer[1]    │   buffer[2]    │   buffer[3]    │
│  4 floats   │   3 floats     │   3 floats     │   2 floats     │
│  (input to  │   (output of   │   (output of   │   (output of   │
│   layer 0)  │    layer 0)    │    layer 1)    │    layer 2)    │
└─────────────┴────────────────┴────────────────┴────────────────┘
 offset=0      offset=4        offset=7         offset=10

GRADIENT_BUFFERS — backward pass gradients, same layout as intermediate:

GRADIENT_BUFFERS[TOTAL_GRADIENT_BUFFER_SIZE]   (same size = 12)
┌─────────────┬────────────────┬────────────────┬────────────────┐
│  grad[0]    │   grad[1]      │   grad[2]      │   grad[3]      │
│  4 floats   │   3 floats     │   3 floats     │   2 floats     │
│  grad w.r.t │   grad flowing │   grad flowing │   loss gradient│
│  input      │   into         │   into         │   (dL/d_output)│
│             │   layer 0      │   layer 1      │   placed here  │
└─────────────┴────────────────┴────────────────┴────────────────┘
 offset=0      offset=4        offset=7         offset=10

Backward flow:  grad[3] => Layer 2 => grad[2] => Layer 1 => grad[1] => Layer 0 => grad[0]

Each layer reads from intermediate_buffers[i] and writes to intermediate_buffers[i+1] during the forward pass. During the backward pass, layer i reads the incoming gradient from gradient_buffers[i+1] (gradient flowing backward from the layer above) and writes the outgoing gradient to gradient_buffers[i] (gradient flowing backward to the layer below). The loss gradient is placed in gradient_buffers[num_layers] to start the backward pass. gradient_buffers[0] receives the gradient w.r.t. the trainable model input, which is computed but not used.

8.12.3.7.3.2. 2.2 TrainingPhase_t

typedef enum {
    PHASE_TRAINING,   // Model is in training mode
    PHASE_INFERENCE   // Model is in inference mode
} TrainingPhase_t;

This enum is stored in ModelContext_t.is_training_mode


8.12.3.7.4. 3. Initialization

8.12.3.7.4.1. ODT_Init

Signature:

int ODT_Init(ModelContext_t* ctx, float learning_rate);

Parameters:

Parameter

Type

Description

ctx

ModelContext_t*

Model context to initialize

learning_rate

float

Learning rate for SGD (e.g., 0.0001). Must be > 0

Returns: 0 on success, -1 on error.

Prepares the model context for use. This is a one-time setup that must be called before any other function in the library. It reads the auto-generated model configuration (LAYER_PARAMS_INIT, ALL_WEIGHTS, BUFFER_OFFSETS, etc.), sets up all internal pointers, and validates that the model architecture is consistent (layer dimensions chain correctly, offsets are within bounds, first layer matches FROZEN_OUTPUT_SIZE, last layer matches FINAL_OUTPUT_SIZE).

After this call, the model context is ready for forward passes, backward passes, and weight updates. The model starts in PHASE_INFERENCE mode.

Example:

ModelContext_t model_ctx;
int status = ODT_Init(&model_ctx, 0.0001f);
if (status != 0) {
    // Handle initialization error
}

Console output (DEBUG build):

========================================
ODT INITIALIZATION
========================================
  Layer 0: Linear(48→24)
  Layer 1: ReLU(24)
  Layer 2: Linear(24→12)
  Layer 3: ReLU(12)
  Layer 4: Linear(12→6)
  Layer 5: ReLU(6)
  Layer 6: Linear(6→12)
  Layer 7: ReLU(12)
  Layer 8: Linear(12→24)
  Layer 9: ReLU(24)
  Layer 10: Linear(24→48)

Common errors (returns -1 ):

  • NULL context or non-positive learning rate

  • Layer dimension mismatch (e.g., layer 2 expects 12 inputs but layer 1 outputs 24)

  • Weight offsets out of bounds (usually means trainable_model_config files are corrupted or mismatched)

  • First/last layer size doesn’t match FROZEN_OUTPUT_SIZE / FINAL_OUTPUT_SIZE


8.12.3.7.5. 4. Core API — Forward Pass

8.12.3.7.5.1. ODT_Forward

Signature:

int ODT_Forward(ModelContext_t* ctx, float* input, float* output);

Parameters:

Parameter

Type

Size

Description

ctx

ModelContext_t*

—

Initialized model context

input

float*

FROZEN_OUTPUT_SIZE

Input from frozen model (or raw input for full model training)

output

float*

FINAL_OUTPUT_SIZE

Buffer to receive model output

Returns: 0 on success, -1 on error.

Runs the input through all trainable layers in sequence and writes the final result to output. Intermediate activations are saved in internal buffers — these are needed if you call ODT_Backward afterward.

Data flow diagram (using the same 3-layer example: Linear(4→3), ReLU(3), Linear(3→2)):

input (4 floats) ──copy──► intermediate_buffers[0] (4 floats)
                                   │
                                   ▼
                            Layer 0: Linear(4→3)
                                   │
                                   ▼
                           intermediate_buffers[1] (3 floats)
                                   │
                                   ▼
                            Layer 1: ReLU(3)
                                   │
                           intermediate_buffers[2] (3 floats)
                                   │
                                   ▼
                            Layer 2: Linear(3→2)
                                   │
                                   ▼
                           intermediate_buffers[3] (2 floats) ──copy──► output (2 floats)

Each intermediate_buffers[i] is a pointer to a region of the flat INTERMEDIATE_BUFFERS array. The number in parentheses is the number of floats at that position. Layer i reads from intermediate_buffers[i] and writes its result to intermediate_buffers[i+1].

Important: The intermediate buffers are preserved after the forward pass. They are needed by the backward pass to compute gradients. Do not modify them between a forward and backward call during training.

Example:

float model_input[input_size];  
float model_output[output_size];

ODT_Forward(&model_ctx, model_input, model_output);
// model_output now contains the trainable model's output

8.12.3.7.6. 5. Core API — Backward Pass

8.12.3.7.6.1. ODT_Backward

Signature:

int ODT_Backward(ModelContext_t* ctx, float* loss_gradient);

Parameters:

Parameter

Type

Size

Description

ctx

ModelContext_t*

—

Model context (must have valid intermediate buffers from a prior forward pass)

loss_gradient

float*

FINAL_OUTPUT_SIZE

Gradient of the loss with respect to the model output. Computed by ODT_MSEGradient or similar

Returns: 0 on success, -1 on error.

Propagates gradients backward through all layers in reverse order, using the saved activations from the most recent forward pass. For each layer, it computes the gradient flowing to the previous layer.

For Linear layers, the backward pass also handles weight updates:

  • Batch size = 1: Weights are updated immediately during the backward pass (no separate update step needed)

  • Batch size > 1: Gradients are accumulated into a buffer; call ODT_UpdateWeights after the batch is complete

Data flow diagram (using the same 3-layer example, in reverse):

loss_gradient (2 floats) ──copy──► gradient_buffers[3] (2 floats)
                                   │
                                   ▼
                            Layer 2: Linear(3→2) backward
                                   │
                                   ▼
                           gradient_buffers[2] (3 floats)
                                   │
                                   ▼
                            Layer 1: ReLU(3) backward
                                   │
                                   ▼
                           gradient_buffers[1] (3 floats)
                                   │
                                   ▼
                            Layer 0: Linear(4→3) backward
                                   │
                                   ▼
                           gradient_buffers[0] (4 floats)  

Each layer’s backward pass does two things:

  1. Reads the incoming gradient from gradient_buffers[i+1] and the saved activation from intermediate_buffers[i]

  2. Writes the outgoing gradient to gradient_buffers[i]

For model layers, the backward pass additionally computes weight gradients and either updates weights immediately (batch_size=1) or accumulates gradients for later update (batch_size>1).

Important: ODT_Backward must be called after ODT_Forward on the same sample. The intermediate buffers from the forward pass contain saved activations needed for gradient computation.

Example (complete training step for batch_size=1):

// 1. Forward pass
ODT_Forward(&model_ctx, model_input, model_output);

// 2. Compute loss
float loss;
ODT_MSELoss(model_output, target, output_size, &loss);

// 3. Compute loss gradient
float loss_grad[output_size];
ODT_MSEGradient(model_output, target, loss_grad, output_size);

// 4. Backward pass (weights updated immediately when batch_size=1)
ODT_Backward(&model_ctx, loss_grad);

// Done! For batch_size=1, gradients are calculated and applied immediately.
// For batch_size>1, gradients are accumulated in the gradient buffer for later update.

8.12.3.7.7. 6. Core API — Weight Update and Gradient Management

8.12.3.7.7.1. ODT_UpdateWeights

Signature:

int ODT_UpdateWeights(ModelContext_t* ctx, uint16_t batch_size);

Parameters:

Parameter

Type

Description

ctx

ModelContext_t*

Model context

batch_size

uint16_t

Number of samples accumulated in the batch (for averaging)

Returns: 0 on success, -1 on error.

Behavior:

  • When USE_GRADIENT_ACCUMULATION is 0 (batch_size=1): This function is a no-op. Weights were already updated immediately during ODT_Backward.

  • When USE_GRADIENT_ACCUMULATION is 1 (batch_size>1): Applies accumulated gradients to all weights:

    for each parameter i:
        current_weights[i] -= (learning_rate / batch_size) * weight_gradients[i]
    

    The division by batch_size averages the gradients across all samples in the batch.

8.12.3.7.7.2. ODT_ZeroGradients

Signature:

int ODT_ZeroGradients(ModelContext_t* ctx);

Behavior:

  • When USE_GRADIENT_ACCUMULATION is 0 (batch_size=1): No-op. No gradient accumulators exist.

  • When USE_GRADIENT_ACCUMULATION is 1 (batch_size>1): Zeros the entire weight_gradients array via memset. Must be called at the start of each new batch.

Example (complete training step for batch_size>1):

// Start of batch
ODT_ZeroGradients(&model_ctx);

// Accumulate gradients over batch
for (int s = 0; s < batch_size; s++) {
    ODT_Forward(&model_ctx, inputs[s], output);
    ODT_MSELoss(output, targets[s], output_size, &loss);
    ODT_MSEGradient(output, targets[s], loss_grad, output_size);
    ODT_Backward(&model_ctx, loss_grad);
    // Gradients accumulated but NOT applied yet
}

// Apply averaged gradients
ODT_UpdateWeights(&model_ctx, batch_size);

8.12.3.7.8. 7. Core API — Weight Checkpointing

8.12.3.7.8.1. ODT_SaveBestWeights

Signature:

int ODT_SaveBestWeights(ModelContext_t* ctx);

Saves a snapshot of all current model weights as the “best” checkpoint.

When to call: After a validation epoch shows a new best loss. Call it to store the current model and load back the weights when training is over.

8.12.3.7.8.2. ODT_LoadBestWeights

Signature:

int ODT_LoadBestWeights(ModelContext_t* ctx);

Restores the previously saved “best” weights as the active model weights.

When to call: When training ends. This ensures the final model uses the best-performing checkpoint rather than the last epoch’s weights, which may have overfit.

Example:

// During training, after each validation epoch:
if (val_loss < best_val_loss) {
    best_val_loss = val_loss;
    ODT_SaveBestWeights(&model_ctx);
}

// When training ends:
ODT_LoadBestWeights(&model_ctx);
// model now uses the best weights, not the last epoch's weights

8.12.3.7.9. 8. Loss Functions

8.12.3.7.9.1. ODT_MSELoss

Signature:

int ODT_MSELoss(float* prediction, float* target, uint16_t size, float* loss);

Calculates the mean squared error from prediction and target and return the average loss.

Parameters:

Parameter

Type

Description

prediction

float*

Model output

target

float*

Ground truth / expected output

size

uint16_t

Number of elements

loss

float*

Pointer to store the computed loss value

Formula:

MSE = (1/N) × Σ(prediction[i] - target[i])²

8.12.3.7.9.2. ODT_MSEGradient

Signature:

int ODT_MSEGradient(float* prediction, float* target, float* grad_output, uint16_t size);

Computes the gradient of the MSE loss with respect to each element of the prediction. This gradient vector is passed to ODT_Backward to initiate backpropagation through the network.

Parameters:

Parameter

Type

Description

prediction

float*

Model output

target

float*

Ground truth

grad_output

float*

Output buffer for the gradient

size

uint16_t

Number of elements

Formula:

grad_output[i] = (2/N) × (prediction[i] - target[i])

Example (computing loss and gradient together):

float loss;
float loss_grad[output_size];

ODT_MSELoss(model_output, target, output_size, &loss);
ODT_MSEGradient(model_output, target, loss_grad, output_size);

printf("MSE Loss: %f\n", loss);
// loss_grad is ready to pass to ODT_Backward

8.12.3.7.10. 9. Layer Operations

These are internal functions called by ODT_Forward and ODT_Backward — users do not call them directly. They are documented here for understanding and for extending the library with new layer types.

8.12.3.7.10.1. 9.1 Linear Layer

A linear (fully connected) layer performs the standard matrix-vector operation: output = W × input + bias.

8.12.3.7.10.1.1. ODT_LinearForward

void ODT_LinearForward(float* input, float* output, LayerParams_t* layer);

Computes the weighted sum of inputs plus bias for each output neuron. The weight matrix is stored in row-major format [output_size × input_size] in the flat ALL_WEIGHTS array, starting at layer->weight_offset.

8.12.3.7.10.1.2. ODT_LinearBackward

void ODT_LinearBackward(ModelContext_t* ctx, float* grad_output, float* grad_input, float* input, LayerParams_t* layer);

Performs three operations during the backward pass:

  1. Input gradient: Computes grad_input = W^T × grad_output — the gradient flowing to the previous layer. This is always computed regardless of batch size.

  2. Weight/bias update (behavior depends on batch size):

    • Batch size = 1 (USE_GRADIENT_ACCUMULATION = 0): Computes weight gradients and applies them immediately using SGD (W -= lr × gradient). No gradient storage buffer needed.

    • Batch size > 1 (USE_GRADIENT_ACCUMULATION = 1): Accumulates weight gradients into a separate buffer. The actual weight update happens later when ODT_UpdateWeights is called.

The two paths are selected at compile time via #if USE_GRADIENT_ACCUMULATION, so the unused path is completely eliminated from the binary. The batch_size=1 path saves both memory (no ALL_WEIGHT_GRADS array) and compute (no separate accumulation or update pass).

8.12.3.7.10.2. 9.2 ReLU Layer

ReLU (Rectified Linear Unit) applies an element-wise non-linearity. It has no trainable parameters.

8.12.3.7.10.2.1. ODT_ReLUForward

void ODT_ReLUForward(float* input, float* output, uint16_t size);

Applies output[i] = max(0, input[i]) for each element. Negative values are zeroed out, positive values pass through unchanged.

8.12.3.7.10.2.2. ODT_ReLUBackward

void ODT_ReLUBackward(float* grad_output, float* grad_input, float* forward_output, uint16_t size);

Masks the gradient using the saved forward output: where the forward output was positive, the gradient passes through unchanged; where it was zero (input was negative), the gradient is blocked. No weight updates occur since ReLU has no parameters.


8.12.3.7.11. 10. Batch Size Optimization — Detailed Explanation

The batch size optimization is one of the memory optimization and here is how it works:

8.12.3.7.11.1. Batch size = 1

Compile-time configuration:

#define TRAIN_BATCH_SIZE 1
// Results in: USE_GRADIENT_ACCUMULATION = 0

What happens:

  • ALL_WEIGHT_GRADS is not allocated (compile-time elimination)

  • weight_grad and bias_grad fields do not exist in LayerParams_t

  • ODT_LinearBackward computes gradient AND updates weight in a single fused loop

  • ODT_UpdateWeights is a no-op

  • ODT_ZeroGradients is a no-op

Training loop (simplified):

for each sample:
    ODT_Forward(ctx, input, output)
    ODT_MSELoss(output, target, size, &loss)
    ODT_MSEGradient(output, target, loss_grad, size)
    ODT_Backward(ctx, loss_grad)          // ← weights updated HERE
    // No ODT_UpdateWeights needed
    // No ODT_ZeroGradients needed

Memory savings: For a model with P total parameters, this saves P × 4 bytes of RAM. For example, a model with 3,150 parameters saves 3,150 × 4 = 12,600 bytes.

8.12.3.7.11.2. Batch size > 1

Compile-time configuration:

#define TRAIN_BATCH_SIZE 4
// Results in: USE_GRADIENT_ACCUMULATION = 1

What happens:

  • ALL_WEIGHT_GRADS[TOTAL_PARAMS] is allocated

  • ODT_LinearBackward accumulates gradients without updating weights

  • ODT_UpdateWeights applies the averaged accumulated gradients

  • ODT_ZeroGradients must be called before each batch

Training loop (simplified):

for each batch:
    ODT_ZeroGradients(ctx)                // ← Reset accumulators
    for each sample in batch:
        ODT_Forward(ctx, input, output)
        ODT_MSELoss(output, target, size, &loss)
        ODT_MSEGradient(output, target, loss_grad, size)
        ODT_Backward(ctx, loss_grad)      // ← gradients accumulated, NOT applied
    ODT_UpdateWeights(ctx, batch_size)    // ← Apply averaged gradients

8.12.3.7.12. 11. Logging System

The library uses compile-time controlled logging via the ODT_LOG macro:

DEBUG build (-DDEBUG):

#define ODT_LOG(...) printf(__VA_ARGS__)

All log statements compile to printf calls, producing detailed console output.

DEBUG build with interrupt safety (-DDEBUG -DUSE_INTERRUPT_SAFE_LOGGING):

#define ODT_LOG(...) do { DINT; printf(__VA_ARGS__); EINT; } while(0)

Same as above, but disables interrupts during printing to prevent garbled output when logging from interrupt context.

Release build (no -DDEBUG):

#define ODT_LOG(...) ((void)0)

All log statements compile to nothing — zero code size, zero runtime overhead.


8.12.3.7.13. 12. Writing a Custom Training Loop

This section shows how to use the library directly to implement your own training loop. This is useful if you want full control over the training process.

8.12.3.7.13.1. Understanding the data flow

Before writing the training loop, it helps to understand how data flows from raw input to trainable model output:

Raw sensor data (e.g., accelerometer samples)
        │
        ▼
Feature Extraction (FE)  ← User must implement if they need additional ones that are not offered by Tiny ML ModelZoo
        │
        ▼
feature_input [FE_NN_OUT_SIZE]  (extracted features)
        │
        ▼
Frozen Model (tvmgen_default_run)  ← Compiled model from mod.a
        │
        ▼
frozen_output [FROZEN_OUTPUT_SIZE]  (input to trainable model)
        │
        ▼
Trainable Model (ODT_Forward)  
        │
        ▼
trainable_output [FINAL_OUTPUT_SIZE]  (model prediction)

The feature extraction and frozen model inference steps are application-specific — you must implement them based on your sensor data and model architecture. For the fan blade example, this involves FFT-based feature extraction followed by tvmgen_default_run(). See application_main.c in the SDK example for a complete implementation.

The ODT library only handles the trainable model portion — everything from frozen_output onward.

8.12.3.7.13.2. Complete training loop example

This example assumes batch_size=1 (the default and recommended setting for on-device training).

#include "ondevice_training_lib.h"
#include "trainable_model_config.h"
#include "ondevice_training_data.h"
#include "tvmgen_default.h"

// ---------------------------------------------------------------
// Buffers
// ---------------------------------------------------------------
// frozen_output: the frozen model's output, which becomes the trainable model's input. Size = FROZEN_OUTPUT_SIZE.
float frozen_output[FROZEN_OUTPUT_SIZE];

// trainable_output: the trainable model's prediction. Size = FINAL_OUTPUT_SIZE.
float trainable_output[FINAL_OUTPUT_SIZE];

// loss_gradient: gradient of the loss w.r.t. trainable_output. Passed to ODT_Backward to start backpropagation.
float loss_gradient[FINAL_OUTPUT_SIZE];

// target: the ground truth for loss computation.
// The application is responsible for providing the correct target for each sample.
float target[FINAL_OUTPUT_SIZE];

// ---------------------------------------------------------------
// Application-specific: prepare frozen_output and target from one raw sample
// ---------------------------------------------------------------
// You MUST implement this function for your application.
// It should:
//   1. Run feature extraction on the raw sample data (e.g., FFT, mel spectrogram — depends on your pipeline)
//   2. Run the frozen model on the extracted features (tvmgen_default_run from the compiled mod.a)
//   3. Write the frozen model's output into frozen_out[]
//   4. Write the appropriate target into target[]
//
// Pseudocode:
//   void prepare_sample(const float* raw_sample, float* frozen_out, float* target) {
//       float features[FEATURE_SIZE];
//       run_feature_extraction(raw_sample, features);
//       // Set target based on your task (application-specific)
//       set_target(target, ...);
//       struct tvmgen_default_inputs  in  = { features };
//       struct tvmgen_default_outputs out = { frozen_out };
//       tvmgen_default_run(&in, &out);
//   }
void prepare_sample(const float* raw_sample, float* frozen_out, float* target);

void train_model(void) {

    // =========================================================
    // Step 1: Initialize the trainable model
    // =========================================================
    // ODT_Init reads the auto-generated model config, sets up all weight/buffer pointers, and validates the architecture.
    ModelContext_t ctx;
    ODT_Init(&ctx, 0.0001f);  // learning rate = 1e-4

    float best_val_loss = 1e30f;
    int epochs_without_improvement = 0;
    int max_epochs = 200;
    int patience = 10;

    for (int epoch = 0; epoch < max_epochs; epoch++) {

        // =========================================================
        // Step 2: Training phase — learn from training samples
        // =========================================================
        float epoch_train_loss = 0.0f;

        for (int s = 0; s < NUM_TRAIN_SAMPLES; s++) {

            // (a) Prepare input: raw data → FE → frozen model → frozen_output + target
            prepare_sample(TRAIN_INPUTS[s], frozen_output, target);

            // (b) Forward pass: frozen_output → trainable layers → trainable_output
            ODT_Forward(&ctx, frozen_output, trainable_output);

            // (c) Compute loss: how different is the prediction from the target?
            float sample_loss;
            ODT_MSELoss(trainable_output, target, FINAL_OUTPUT_SIZE, &sample_loss);
            epoch_train_loss += sample_loss;

            // (d) Compute loss gradient: dLoss/d(trainable_output)
            ODT_MSEGradient(trainable_output, target, loss_gradient, FINAL_OUTPUT_SIZE);

            // (e) Backward pass: propagate gradient through all layers and update weights immediately (batch_size=1)
            ODT_Backward(&ctx, loss_gradient);

            // Note: For batch_size=1, weights are already updated inside ODT_Backward.
            // For batch_size>1, you would call ODT_UpdateWeights(&ctx, batch_size) after accumulating gradients over all samples in the batch.
        }

        // =========================================================
        // Step 3: Validation phase — evaluate without learning
        // =========================================================
        // Same forward + loss as training, but NO backward pass. We only measure loss to decide if the model is improving.
        float epoch_val_loss = 0.0f;

        for (int s = 0; s < NUM_VALIDATION_SAMPLES; s++) {

            prepare_sample(VALIDATION_INPUTS[s], frozen_output, target);

            ODT_Forward(&ctx, frozen_output, trainable_output);

            float sample_loss;
            ODT_MSELoss(trainable_output, target, FINAL_OUTPUT_SIZE, &sample_loss);
            epoch_val_loss += sample_loss;
        }
        float avg_val_loss = epoch_val_loss / NUM_VALIDATION_SAMPLES;

        // =========================================================
        // Step 4: Checkpointing and early stopping
        // =========================================================
        if (avg_val_loss < best_val_loss - 0.5f) {
            best_val_loss = avg_val_loss;
            epochs_without_improvement = 0;
            ODT_SaveBestWeights(&ctx);  // Snapshot current weights
        } else {
            epochs_without_improvement++;
            if (epochs_without_improvement >= patience) {
                break;  // Stop — model is no longer improving
            }
        }
    }

    // =========================================================
    // Step 5: Restore best weights
    // =========================================================
    // The last epoch may have overfit. Load the checkpoint from the epoch with the lowest validation loss.
    ODT_LoadBestWeights(&ctx);

    // Model is now ready for inference with best-performing weights.
}

8.12.3.7.13.3. How this example works

Where the data comes from: TRAIN_INPUTS, VALIDATION_INPUTS, and their corresponding labels are defined in ondevice_training_data.h/.c — auto-generated arrays containing a small number of samples exported from the PC-side training pipeline. Each sample is a flat float array of RAW_INPUT_SIZE elements representing raw sensor data.

Data flow for one training sample:

  1. prepare_sample() — Your application-specific function takes one raw sample, runs feature extraction (FFT, binning, etc.), runs the frozen model via tvmgen_default_run(), and sets the target appropriate for your task. The frozen model output is written to frozen_output[], a FROZEN_OUTPUT_SIZE-element float array. This is the only part you need to implement yourself. See application_main.c in the SDK example for a complete implementation.

  2. ODT_Forward() — Takes frozen_output as input, passes it through all trainable layers (Linear, ReLU, etc.), and writes the prediction to trainable_output[]. Intermediate activations are saved internally for the backward pass.

  3. ODT_MSELoss() — Compares trainable_output to target and computes the loss value.

  4. ODT_MSEGradient() — Computes how each element of trainable_output contributed to the loss. This produces loss_gradient[], which tells the backward pass which direction to adjust the weights.

  5. ODT_Backward() — Propagates loss_gradient backward through all layers in reverse order. With batch_size=1, weights are updated immediately inside this call — no separate update step is needed.

Training vs. validation: Both phases run steps 1–3 (prepare → forward → loss). The critical difference is that training also runs steps 4–5 (gradient → backward) to update weights, while validation does not. Never call ODT_Backward during validation — it would modify the weights and corrupt the model.

Early stopping and checkpointing: After each epoch, the average validation loss is compared against the best seen so far. If it improved, ODT_SaveBestWeights snapshots the current weights. If it hasn’t improved for patience consecutive epochs, training stops early. At the end, ODT_LoadBestWeights restores the best checkpoint — this is important because the last epoch’s weights may have started overfitting.

8.12.3.7.13.4. Key rules

  1. Always call ODT_Init first. It validates the model configuration and sets up all internal pointers.

  2. Forward before backward. The backward pass reads activations saved during the forward pass. Calling backward without a prior forward is undefined behavior.

  3. Never call backward during validation. Validation is read-only — forward + loss computation only.

  4. Save best weights on improvement, load best at end. This ensures the final model is the best-performing one, not the last one.

  5. For batch_size=1: ODT_ZeroGradients and ODT_UpdateWeights are not needed — weights are updated inside ODT_Backward.

  6. For batch_size>1: Call ODT_ZeroGradients before each batch and ODT_UpdateWeights after each batch.


8.12.3.7.14. 13. How to Add a New Layer Type

To extend the library with a new layer type (e.g., Conv1D):

Step 1: Add the new enum value in trainable_model_config.h:

typedef enum {
    LAYER_TYPE_LINEAR,
    LAYER_TYPE_RELU,
    LAYER_TYPE_CONV1D,    // ← New
} LayerType_t;

Step 2: Add shape metadata to the LayerParams_t union (already has a placeholder):

union {
    struct { 
        uint16_t rows;
        uint16_t cols;
    } linear;
    struct { 
        uint16_t out_channels;
        uint16_t in_channels;
        uint16_t kernel_size;
        uint16_t stride;
        uint16_t padding;
     } conv1d;       // add new layer info
} shape;

Step 3: Implement the forward function:

void ODT_Conv1DForward(float* input, float* output, LayerParams_t* layer);

Step 4: Implement the backward function:

void ODT_Conv1DBackward(ModelContext_t* ctx, float* grad_output, float* grad_input, float* input, LayerParams_t* layer);

Step 5: Add cases to ODT_Forward and ODT_Backward switch statements:

case LAYER_TYPE_CONV1D:
    ODT_Conv1DForward(layer_input, layer_output, layer);
    break;

Step 6: Update the Python export pipeline (ondevice_training.py) to parse the new ONNX op type and generate the appropriate LAYER_PARAMS_INIT entries.


8.12.3.7.15. 14. API Quick Reference

Function

Purpose

Returns

ODT_Init(ctx, lr)

Initialize model context, validate config, set up pointers

0 or -1

ODT_Forward(ctx, input, output)

Forward pass through all trainable layers

0 or -1

ODT_Backward(ctx, loss_gradient)

Backward pass, compute gradients, update weights (batch=1)

0 or -1

ODT_UpdateWeights(ctx, batch_size)

Apply accumulated gradients (batch>1 only, no-op for batch=1)

0 or -1

ODT_ZeroGradients(ctx)

Reset gradient accumulators (batch>1 only, no-op for batch=1)

0 or -1

ODT_SaveBestWeights(ctx)

Copy current weights to best weights checkpoint

0 or -1

ODT_LoadBestWeights(ctx)

Restore best weights to current weights

0 or -1

ODT_MSELoss(pred, target, size, loss)

Compute Mean Squared Error loss

0 or -1

ODT_MSEGradient(pred, target, grad, size)

Compute MSE gradient: 2/N × (pred - target)

0 or -1

ODT_LinearForward(in, out, layer)

Linear layer: out = W×in + b

void

ODT_LinearBackward(ctx, grad_out, grad_in, in, layer)

Linear backward: input grad + weight update/accumulate

void

ODT_ReLUForward(in, out, size)

ReLU: out = max(0, in)

void

ODT_ReLUBackward(grad_out, grad_in, fwd_out, size)

ReLU backward: pass grad where fwd > 0

void