7.10.19. Human Fall Detection

Edge AI solution for real-time human fall detection from accelerometer data on the MSPM0G5187 with NPU acceleration. For the radar based variant, see the radar examples.

Example folder: examples/fall_detection_classification (GitHub)

7.10.19.1. Overview

The application classifies human movement as Activities of Daily Living (ADL) or Fall. Falls are a leading cause of injury among elderly people and in industrial environments, and traditional systems rely on cloud connectivity or bulky wearables. Here the classification runs directly on a microcontroller, for example in a belt-mounted safety device.

  • Application: elderly care, worker safety, wearable safety systems

  • Task: binary classification (generic_timeseries_classification): ADL or Fall

  • Data: 3-axis accelerometer (InputChannel_3)

  • Device: MSPM0G5187 (config_MSPM0.yaml, the only config)

  • Model: CLS_6k_NPU

  • Targets: real-time classification, accuracy of at least 97.5%, low memory footprint

7.10.19.2. System Components

  • Hardware: MSPM0G5187 and the EdgeAI Boosterpack TIDA-010997 with a BMI270 accelerometer

  • Software: Code Composer Studio 12.x or later, MSPM0 SDK 2.11.00 or later

7.10.19.3. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/fall_detection_classification/config_MSPM0.yaml

7.10.19.4. Configuration

common:
  task_type: generic_timeseries_classification
  target_device: MSPM0G5187
dataset:
  dataset_name: fall_detection_classification
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/fall_detection_classification.zip
data_processing_feature_extraction:
  feature_extraction_name: FallDetection_256Input_FE_RFFT_8Feature_8Frame_3InputChannel_removeDC_2D1
training:
  model_name: CLS_6k_NPU
  batch_size: 256
  training_epochs: 50
  num_gpus: 0
testing: {}
compilation: {}

7.10.19.5. Dataset

The example uses the SisFall dataset (about 4500 recordings, two classes). Each SisFall file has three sensors: ADXL345 (13-bit accelerometer), ITG3200 (gyroscope) and MMA8451Q (accelerometer). The prepared zip is downloaded automatically. The preparation applied to it was:

  1. Sensor filtering: only the ADXL345 accelerometer columns are kept, to match the single accelerometer (BMI270) of the target hardware.

  2. Bit-depth scaling: the 13-bit ADXL345 values are multiplied by 8 (2^16 / 2^13) so that they match the 16-bit BMI270 data seen by the firmware during inference.

  3. Format conversion: each file is parsed, labeled ADL or Fall and exported in the ModelZoo dataset structure.

7.10.19.6. Feature Extraction

The preset FallDetection_256Input_FE_RFFT_8Feature_8Frame_3InputChannel_removeDC_2D1 mirrors the on-device pipeline:

  1. 3-axis accelerometer input scaled to 16 bit

  2. 256-point real FFT (ARM CMSIS-DSP on device)

  3. Complex magnitude

  4. DC removal

  5. Binning: 16 adjacent bins averaged into 8 features

  6. Concatenation of 8 frames (64 features per axis)

7.10.19.7. Model and Results

The example readme reports for the reference model (CLS_6k, about 6,000 parameters), measured on the LP-MSPM0G5187 LaunchPad with an earlier release: 14 kB flash, 0.7 kB RAM, 0.67 ms NPU inference latency and 97.65% accuracy, with INT8 quantization.

In the automated 1.5.0 config test run, config_MSPM0.yaml (CLS_6k_NPU, 6,696 parameters) reached a test accuracy of 97.15% with an AUC ROC of 0.996.

7.10.19.8. Practical Considerations

  • Mount the accelerometer on the belt or wrist and keep the sensor firmly attached.

  • The BMI270 sampling rate is 100 to 200 Hz.

  • False positives (rapid ADL movements such as jumping) can be reduced by adding such samples to the training data.

  • All inference runs on the device; raw accelerometer data never leaves it.

7.10.19.9. Deployment

See Project Compilation Guide: Timeseries Classification Examples and Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check). To adapt the model to a person after deployment, see On-Device Training — Overview.

7.10.19.10. See Also