2.1. Prerequisites
Check these requirements before installing Tiny ML ModelZoo 1.6.0.
2.1.1. System Requirements
Linux |
Ubuntu 20.04 or later recommended (x86_64) |
Windows |
Windows 10/11, native or WSL2 |
macOS |
Apple Silicon (arm64) with MPS training support. See macOS Setup. |
CPU / RAM / disk |
Multi-core CPU, 8 GB RAM minimum (16 GB recommended), about 10 GB free disk for the install and datasets |
GPU |
Optional. CUDA GPU on Linux/Windows, or MPS on Apple Silicon, to speed up training |
2.1.2. Python
Important
Use Python 3.10 if you want to compile models for a device.
tinyml_modelzoodeclaresrequires-python >=3.10,<3.15and 1.5.0 added Python 3.14 / PyTorch 2.11 compatibility, so training works on Python 3.10 to 3.14.The TI Neural Network Compiler wheel (
ti_mcu_nnc 2.1.2) that ModelMaker uses for compilation is only installed on Python 3.10 (its dependency marker ispython_version < '3.11'). On Python 3.11 or later, pip skips it silently and the compile step is not available.The project README lists “Python 3.10 environment” as the prerequisite.
Pinned dependencies installed by pip (from pyproject.toml): torch==2.11.0,
PyYAML==6.0.3, numpy==2.2.6 (Python 3.10) or numpy==2.5.2 (Python 3.11+).
Do not pre-install other versions of torch or numpy in the same environment.
pyenv is a convenient way to get Python 3.10:
curl https://pyenv.run | bash # macOS: brew install pyenv
pyenv install 3.10.14
pyenv global 3.10.14
python --version
Install Python 3.10 from https://www.python.org/downloads/ or use pyenv-win:
pyenv install 3.10.11
pyenv global 3.10.11
python --version
2.1.3. pip and Git
python -m pip install --upgrade pip setuptools wheel
git --version # only needed for the clone install
Git is only needed for the clone install (Clone Installation). The wheel install (Wheel Installation) needs only Python and pip.
2.1.4. TI Compiler Tools (for compilation)
Required only to compile models for a device. Download from TI and set the matching environment variable (Environment Variables).
C2000 F28x: TI C2000 Code Generation Tools (https://www.ti.com/tool/C2000-CGT)
C2000 F29x: TI C29 Clang compiler
MSPM0, MSPM33C, AM13, AM26x, CC13xx/CC27xx/CC35xx, xWRL6432: TI Arm Clang compiler (https://www.ti.com/tool/ARM-CGT)
To flash and debug on hardware, install Code Composer Studio (https://www.ti.com/tool/CCSTUDIO) and see Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check).
2.1.5. Verification Checklist
python --version # 3.10.x for compilation support
pip --version
git --version # clone install only
Then proceed to Wheel Installation or Clone Installation.