7.10.26. Battery State of Charge (SOC) Estimation
Estimate the state of charge of a lithium-ion cell from voltage, current, temperature and accumulated capacity on the MSPM0G5187 microcontroller with its integrated NPU. New in 1.5.0.
Example folder: examples/bms_soc_estimation
(GitHub)
7.10.26.1. Overview
Task: timeseries regression (
generic_timeseries_regression)Application: battery management systems (BMS), prevention of over-charge and over-discharge, remaining runtime estimation, battery life extension
Device: MSPM0G5187 (
config_MSPM0.yaml, the only config in the folder)Model:
REGR_20k_NPU(about 20,000 parameters, INT8 NPU quantization)Target:
SOC
Traditional coulomb counting and open-circuit-voltage lookup drift over time and are sensitive to sensor noise
and battery aging. A short window of raw voltage, current and temperature is not enough either, because SOC
depends on the charge and discharge history. The model therefore also receives the accumulated charge
(capacity_Ah) as an input.
7.10.26.2. The Dataset
The dataset is the public LG 18650HG2 Li-ion battery data (LG_18650HG2_Liion_Battery_Data), charge and
discharge cycles logged at fixed intervals, split into 4491 files. Each file provides four input variables in
this column order:
voltage_Vcurrent_Atemperature_Ccapacity_Ah
The target is SOC. The config downloads
https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/LG_18650HG2_Liion_Battery_Data.zip. The layout is the
regression layout (files/ plus annotations/), see Regression Dataset Format.
7.10.26.3. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from
the tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/bms_soc_estimation/config_MSPM0.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\bms_soc_estimation\config_MSPM0.yaml
7.10.26.4. Configuration
common:
target_module: timeseries
task_type: generic_timeseries_regression
target_device: MSPM0G5187
run_name: '{date-time}/{model_name}'
dataset:
dataset_name: LG_18650HG2_Liion_Battery_Data
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/LG_18650HG2_Liion_Battery_Data.zip
data_processing_feature_extraction:
data_proc_transforms:
- SimpleWindow
frame_size: 16
stride_size: 0.5
variables: 4
training:
enable: true
model_name: REGR_20k_NPU
quantization: 2
num_gpus: 1
training_epochs: 50
batch_size: 128
learning_rate: 0.001
testing: {}
compilation: {}
quantization: 2 selects INT8 NPU-optimized quantization, and compilation with the TI Neural Network
Compiler generates mod.a and tvmgen_default.h for the MSPM0G5187 NPU. num_gpus: 1 expects a GPU;
use 0 for CPU.
7.10.26.5. Results
The example readme reports the following for REGR_20k_NPU on the full dataset (best run):
Metric |
Value |
|---|---|
Test RMSE |
2.56% SOC (0.0256) |
Test R2 |
0.99 |
Best-epoch R2 during training |
0.987 |
Flash on MSPM0G5187 |
26.39 KB (code 2.43 KB, read-only data 21.52 KB, read-write data 2.45 KB) |
The readme sets a stretch target of RMSE below 2% SOC with R2 above 0.99.
Note
The readme results were measured with an earlier release. In the automated 1.5.0 config test run
config_MSPM0.yaml failed while loading the dataset (the annotation list file was not found, IndexError
in load_list), so these results are unverified in 1.5.0.
7.10.26.6. Output Location
Results are written to ./data/projects/LG_18650HG2_Liion_Battery_Data/run/<date-time>/REGR_20k_NPU/. The
device files are compilation/artifacts/mod.a, compilation/artifacts/tvmgen_default.h and the golden
vectors in training/quantization/golden_vectors/.
7.10.26.7. Running on Device
Use the MSPM0 SDK (2.08.00 or later) with Code Composer Studio and follow Deploying Regression Models from ModelMaker to Device and Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check). For the MSPM0G5187 NPU see Supported Devices.