7.10.34. Cough Detection

Binary audio classification (cough versus other) running fully on the LP-MSPM0G5187 LaunchPad, using LPC spectral envelope features and a TCDS-ResNet on the NPU. New in 1.5.0.

Example folder: examples/cough_detection (GitHub)

7.10.34.1. Overview

  • Task: audio classification (audio_classification, target_module: audio), 2 classes (cough, other)

  • Application: health monitoring in hospital or wearable settings, where a missed cough is worse than a false alarm

  • Device: MSPM0G5187 (Arm Cortex-M0+ at 80 MHz, TinyEngine NPU, 128 KB flash, 32 KB SRAM). The folder has a single config.yaml.

  • Model: TCDS_ResNet_NPU

  • Features: preset MSPM0_LPC_8820 (linear predictive coding, matched to the firmware)

7.10.34.2. Data Collection

Audio was captured with TI EdgeAI Studio connected to the LaunchPad over USB. A PCM1809 MEMS microphone feeds the I2S peripheral at 44.1 kHz; the firmware keeps the left channel, converts samples to 16 bits and decimates 5:1 to 8820 Hz mono. EdgeAI Studio stores the raw FIFO samples as a labeled CSV file per recording. The recording set is about 6 minutes in total: three cough recordings (two male, one female) and three speech recordings (greetings, meeting speech, chatting), about 57 seconds each. Silence and white noise were recorded only as a noise bank for augmentation.

7.10.34.3. Preparing the Dataset

The config downloads the prepared dataset from https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/cough_detection.zip. To prepare your own recordings, use prepare_dataset.py:

cd examples/cough_detection
python prepare_dataset.py --data-dir /path/to/csvs --output-dir /path/to/output

The script mirrors the firmware signal path so that training clips equal what the firmware produces:

  1. Extract int16 samples (shift right by 10, clamp).

  2. Deinterleave and keep the left channel (44.1 kHz).

  3. Decimate by 5 to 8820 Hz with plain integer decimation and no anti-alias filter. This must match the firmware, otherwise training and inference see different aliasing.

  4. Cut into 2-second clips (17,640 samples) with 50% overlap.

  5. Augment the cough class with gain 1.0 (original) and gain 0.15 plus a 10 dB SNR noise mix.

A cough is naturally louder than speech. Without the attenuated copies the model would learn to threshold on loudness. The attenuated copies make both classes span the same RMS range, so the model must discriminate on spectral shape. The v2 dataset in the readme has 330 cough clips (165 original, 165 augmented) and 165 other clips.

7.10.34.4. Feature Extraction: MSPM0_LPC_8820

Every parameter of this preset matches a constant in the firmware (lpc_defs.h, feature_extraction.c). If the training and firmware parameters differ, accuracy collapses.

Parameter

Value

Note

sampling_rate

8820 Hz

44100 / 5

audio_duration_ms

2000 ms

100 frames of 20 ms

audio_feature

LPC

Linear predictive coding

lpc_order

10

Order of the all-pole vocal tract model

nlpc

70

Frequency bins of the envelope

frame_length_ms / frame_step_ms

30 ms / 20 ms

264-sample window, 176-sample step

Per 20 ms frame the preset applies pre-emphasis, a Q15 Hamming window, autocorrelation (lags 0 to 10), a Levinson-Durbin recursion, evaluates the frequency response at 70 log-spaced bins (112 Hz to 3946 Hz), converts it to dB and quantizes it to INT8. The model input is (1, 1, 100, 70) INT8. Cough gives a broadband, flat spectral envelope, speech gives narrow formant peaks between 700 and 3000 Hz, which LPC captures in only 70 numbers.

7.10.34.5. Model

TCDS_ResNet_NPU (Temporal Channel-Decoupled Separable ResNet) is designed for INT8-only execution, a small activation memory and 1D temporal convolutions. The input is permuted from (N, 1, T, F) to (N, F, T, 1) so the 70 LPC bins become channels and every kernel is K x 1.

Stage

Block

In ch.

Out ch.

Stride

Stem

Conv2d 3x1

70

16

1

Blocks 1 and 2

TCDSBasicBlock 9x1

16, 24

24, 24

2, 1

Blocks 3 and 4

TCDSBasicBlock 9x1

24, 32

32, 32

2, 1

Blocks 5 and 6

TCDSBasicBlock 9x1

32, 48

48, 48

2, 1

Head

GAP, Dropout 0.5, FC

48

2 classes

Each block is a depthwise K x 1 convolution plus a pointwise 1x1 convolution with BatchNorm and ReLU. The blocks have no residual connection, which avoids the quantized-add incompatibility with TI QAT. The readme quotes a depthwise-separable factorization saving of about 8 to 10 times in parameters. The audio models enabled in 1.5.0 are DSCNN_NPU, DSCNN_32K_NPU (a compact DSCNN for LPC features), DSCNN_GB_NPU, TCDS_ResNet_NPU and TCDS_ResNet_FB_NPU.

7.10.34.6. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/cough_detection/config.yaml

7.10.34.7. Configuration

common:
  target_module: audio
  task_type: audio_classification
  target_device: MSPM0G5187
dataset:
  dataset_name: cough_detection
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/cough_detection.zip
data_processing_feature_extraction:
  feature_extraction_name: MSPM0_LPC_8820
training:
  model_name: TCDS_ResNet_NPU
  batch_size: 64
  training_epochs: 40
  early_stopping: true
  early_stopping_patience: 5
  num_gpus: 1
  learning_rate: 0.01
  weight_decay: 4e-4
testing: {}
compilation:
  compile_preset_name: default_preset

num_gpus: 1 expects a CUDA GPU; use 0 for CPU. The learning rate is kept low for the small dataset. The compilation step runs the TI Neural Network Compiler and produces model.a and tvmgen_default.h for the MSPM0G5187 NPU. For the audio task type see Audio Classification.

7.10.34.8. Results

The example readme reports these results on its v2 dataset (562 clips, 80/20 train and validation split):

Metric

Value

Best validation accuracy

88.5%

Cough recall

100% (0 false negatives)

Cough precision / F1

about 85% / about 92%

The validation confusion matrix has 99 correct coughs, 0 missed coughs, 17 false positives and 32 correct others. The false positives are speech segments that sound like a cough. The high recall is intentional because missing a cough is the worse error; the firmware debounce (DETECT_THRESH = 8 frames, 160 ms of consecutive cough predictions) filters out isolated false positives.

The automated 1.5.0 config test run (early stopped, test set of 50 clips) reached a test accuracy of 78.00% and an AUC ROC of 0.979, so it is below the readme figures. Expect the result to vary with the data and training length.

7.10.34.9. Memory Footprint

Reported by the TI Neural Network Compiler for MSPM0G5187 in the readme:

Segment

Size

Memory

Code (firmware glue)

4.58 KB

Flash

Read-only data (weights and parameters)

45.04 KB

Flash

Read-write data (activations)

14.45 KB

SRAM

That is 49.62 KB of 128 KB flash (39%) and 14.45 KB of 32 KB SRAM (45%).

7.10.34.10. Output Location

Results are written to ./data/projects/cough_detection/run/<date-time>/TCDS_ResNet_NPU/. See Understanding the Run Output and Project Compilation Guide: Timeseries Classification Examples for deployment.

7.10.34.11. See Also