7.10.16. NILM Appliance Usage Classification
Non-Intrusive Load Monitoring (NILM): identify which appliances are active from a single measurement point (such as a smart meter), without a sensor on every appliance. This page covers both NILM examples in the ModelZoo.
Example folders:
7.10.16.1. Overview
NILM analyzes time series of electrical measurements to detect which appliances are running. Typical uses are energy cost optimization in factories, power distribution tracking in electric vehicles, and appliance usage analysis in households.
Both examples are time series classification (generic_timeseries_classification) on the F28P55 with the
CLS_13k_NPU model, the same feature extraction preset Generic_32Input_FFTBIN_4Feature_8Frame and INT8
quantization (quantization: 2).
|
|
|
|---|---|---|
Dataset name |
|
|
Dataset URL |
|
|
Variables |
5 (active power, voltage, current, reactive power, phase) |
2 (voltage and current at 30 kHz) |
Classes |
4 appliance combinations |
11 appliance types |
Training |
15 epochs, batch size 256 |
30 epochs, batch size 256, learning rate 0.04 |
7.10.16.2. Running the Examples
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the
tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/nilm_appliance_usage_classification/config.yaml
./run_tinyml_modelzoo.sh examples/PLAID_nilm_classification/config.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\nilm_appliance_usage_classification\config.yaml
run_tinyml_modelzoo.bat examples\PLAID_nilm_classification\config.yaml
7.10.16.3. Appliance Usage Classification (ESDA NILM 2021)
The data comes from the Kaggle ESDA NILM Competition 2021
(vw_train.csv). The original file has 28 classes of appliance combinations and 30 columns. Because many
classes have too little data, the example keeps 4 classes and 5 easily measured variables:
Classes:
+fridge,+fridge+tumble_dryer+washer_dryer,+fridge+washer_dryer,+fridge+washing_machine+washer_dryerVariables: active power, voltage, current, reactive power, phase
The prepared zip is downloaded automatically from the URL in the config.
common:
task_type: generic_timeseries_classification
target_device: F28P55
dataset:
dataset_name: esda_nilm_2021_5_variable_4_class_dataset
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/esda_nilm_2021_5_variable_4_class_dataset.zip
data_processing_feature_extraction:
feature_extraction_name: Generic_32Input_FFTBIN_4Feature_8Frame
variables: 5
training:
model_name: CLS_13k_NPU
batch_size: 256
training_epochs: 15
quantization: 2
The preset windows the data into 32-sample frames, applies FFT, bins to 4 features per frame, converts to log scale and concatenates 8 frames. Compilation uses the default NPU preset with full INT8 quantization.
7.10.16.4. PLAID Appliance Identification
The PLAID dataset contains voltage and current measurements sampled at 30 kHz from 11 appliance types: air
conditioner, compact fluorescent lamp, fan, fridge, hairdryer, heater, incandescent light bulb, laptop,
microwave, vacuum and washing machine. The example uses a subset (plaid_nilm_submetered_dataset.zip).
common:
task_type: generic_timeseries_classification
target_device: F28P55
dataset:
dataset_name: plaid_submetered
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/plaid_nilm_submetered_dataset.zip
data_processing_feature_extraction:
feature_extraction_name: Generic_32Input_FFTBIN_4Feature_8Frame
variables: 2
training:
model_name: CLS_13k_NPU
batch_size: 256
training_epochs: 30
early_stopping: true
early_stopping_patience: 5
num_gpus: 0
quantization: 2
learning_rate: 0.04
testing: {}
compilation:
keep_libc_files: true
7.10.16.5. Results
Test-set results documented in the example readmes (measured with an earlier release) and in the automated 1.5.0 config test run:
Example |
Example readme |
1.5.0 test run |
AUC ROC (1.5.0 run) |
|---|---|---|---|
|
95.95% |
96.85% |
0.998 |
|
97.72% |
97.82% |
0.989 |
7.10.16.6. On-Device Results and Performance
Both readmes describe running the compiled model on a LAUNCHXL-F28P55X (C2000Ware 6.00, CCS 20.3.0) and checking that the device output matches the golden vectors. The deployment steps are in Project Compilation Guide: Timeseries Classification Examples and Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check).
Device output matching the golden vectors (appliance usage classification)
Metric (F28P55x, NPU, from the example readmes) |
Appliance usage |
PLAID |
|---|---|---|
AI model cycles |
165,629 |
190,571 |
Inference time |
1104.19 us |
1270.47 us |
Model flash |
11,967 bytes |
13,032 bytes |
Model SRAM |
1,220 bytes |
1,004 bytes |
7.10.16.7. See Also
Classification Dataset Format: use your own classification data