7.10.31. Google Speech Command Recognition
12-class keyword spotting from 1-second audio clips, using MFCC features and a depthwise separable CNN (DSCNN) on the MSPM0G5187 with NPU.
Example folder: examples/google_speech_command
(GitHub)
7.10.31.1. Overview
Task: audio classification (
audio_classification,target_module: audio), 12-class keyword spottingApplication: voice command recognition
Dataset: Google Speech Commands v0.02, 12-class variant
Device: MSPM0G5187 (
config_MSPM0.yaml, the only config in the folder)Model:
DSCNN_NPU
7.10.31.2. Keyword Classes
Type |
Labels |
|---|---|
Known keywords (10) |
|
Unknown |
|
Silence |
|
7.10.31.3. The Dataset
The config downloads the prepared dataset from
https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/google_speech_commands_12class.zip, so you can run the
example directly. To regenerate it from the original data, run the helper script (needs torch,
torchaudio, scipy, pydub, numpy and tqdm) and point dataset.input_data_path at the
result:
cd examples/google_speech_command
python generate_dataset.py
The script downloads Google Speech Commands v0.02 through TorchAudio, copies the 10 keyword classes into their own
folders, maps all other words into _unknown_ (prefixing the original label to avoid file name collisions), and
cuts the background noise files into 1-second windows with 50% overlap for _silence_. The output is
SpeechCommands/classes/<class>/.
7.10.31.4. Features
The config uses the feature extraction preset GoogleSpeechCommands_MFCC_Default:
Parameter |
Value |
|---|---|
Sampling rate |
16000 Hz |
Audio duration |
1000 ms |
Frame length / step |
30 ms / 20 ms |
MFCC coefficients |
10 |
Mel bins |
40 |
The output feature shape is [N, 1, 49, 10]: batch, 1 channel, 49 time frames and 10 MFCC coefficients.
7.10.31.5. Model
DSCNN_NPU is a depthwise separable CNN designed for efficient inference on the NPU: a 10x4 convolution with
stride 2, dropout, four blocks of depthwise 3x3 plus pointwise 1x1 convolution, dropout, adaptive average pooling
and a fully connected layer to 12 classes (64 filters). Splitting a convolution into depthwise (spatial) and
pointwise (channel mixing) parts cuts computation and model size while keeping good keyword spotting accuracy.
Other audio models enabled in 1.5.0 are DSCNN_32K_NPU, DSCNN_GB_NPU, TCDS_ResNet_NPU and
TCDS_ResNet_FB_NPU (see Wake Word Detection).
7.10.31.6. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from
the tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/google_speech_command/config_MSPM0.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\google_speech_command\config_MSPM0.yaml
7.10.31.7. Configuration
common:
target_module: audio
task_type: audio_classification
target_device: MSPM0G5187
dataset:
dataset_name: google_speech_commands_12class
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/google_speech_commands_12class.zip
data_processing_feature_extraction:
feature_extraction_name: GoogleSpeechCommands_MFCC_Default
sampling_rate: 16000
audio_duration_ms: 1000
training:
model_name: DSCNN_NPU
batch_size: 64
training_epochs: 20
num_gpus: 1
quantization: 2
learning_rate: 0.1
weight_decay: 1e-5
testing: {}
compilation: {}
num_gpus: 1 expects a GPU; use 0 for CPU. Training on this dataset is long compared with the other examples.
See Audio Classification for the audio task type.
7.10.31.8. Results
The example readme does not publish accuracy numbers. In the automated 1.5.0 config test run the training reached a best quantized epoch (epoch 7) with a validation accuracy of 91.30%, an F1 score of 0.913 and an AUC ROC of 0.997. That run hit the test harness time limit before it finished, so it is a partial result and not a converged 20-epoch result.
7.10.31.9. Output Location
Results are written to ./data/projects/google_speech_commands_12class/run/<date-time>/DSCNN_NPU/. See
Understanding the Run Output for the generated files and
Project Compilation Guide: Timeseries Classification Examples for device deployment. The MSPM0 SDK
2.10.04 or later was listed for this example in 1.4.0.