7.10.5. DC Arc Fault Detection

DC arc fault detection is one of the main applications of Tiny ML ModelZoo. The example folder examples/dc_arc_fault contains six configurations: two supervised classification variants (DSK and DSI datasets), a bring-your-own-model variant, an on-device learning variant, and two anomaly detection variants.

Example folder: examples/dc_arc_fault (GitHub). For AC arc faults on MSPM0, see AC Arc Fault.

7.10.5.1. Overview

  • Task: binary classification (normal vs. arc), task_type: arc_fault; anomaly detection variants use generic_timeseries_anomalydetection

  • Application: solar inverters, battery systems, DC distribution

  • Datasets: real current waveforms from arc fault experiments (DSK and DSI captures)

  • Default device: F28P55 (NPU)

7.10.5.2. Why Arc Fault Detection?

Electrical arcs are a fire hazard in buildings, damage equipment in industrial settings and are a safety risk in battery systems. Fuses and breakers do not detect low-level arcs reliably, whereas an AI model can learn the arc signature in the current waveform.

7.10.5.3. Available Configurations

Config file

Device

Model

Notes

config_dsk.yaml

F28P55

CLS_1k_NPU

DSK dataset dc_arc_fault_example_dsk, preset FFT1024Input_256Feature_1Frame_Full_Bandwidth, 10 epochs, batch size 32

config_dsi.yaml

F28P55

CLS_13k_NPU

DSI dataset arc_fault_example_dsi (313 kHz), Downsample + SimpleWindow transforms, 10 epochs, batch size 2048

config_dsk_my_model.yaml

F28P55

MY_CLS_2k_NPU

Same as config_dsk.yaml but with a user-defined model; see Bring Your Own Model (BYOM)

config_dsi_ondevice_learning.yaml

AM13E2

CLS_24k_NPU

DSI data with on-device training enabled (ondevice_training: true, last 3 layers trainable); see On-Device Training — Overview

config_anomaly_detection_dsi.yaml

F28P55

AD_17k

Anomaly detection on DSI data (arc_fault_example_dsi_ad), 100 epochs, forced_soft_npu_preset compilation

config_anomaly_detection_dsk.yaml

F28P55

AD_17k

Anomaly detection on DSK data (arc_fault_example_dsk_ad), 250 epochs

Datasets are downloaded automatically from https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/ (for example arc_fault_classification_dsi.zip, arc_fault_dsi_anomaly_detection.zip, arc_fault_dsk_anomaly_detection.zip). The DSK classification dataset is resolved from its dataset name.

7.10.5.4. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/dc_arc_fault/config_dsk.yaml

Replace config_dsk.yaml with any config from the table above.

7.10.5.5. Configuration (config_dsk.yaml)

common:
  task_type: arc_fault
  target_device: F28P55
dataset:
  dataset_name: dc_arc_fault_example_dsk
data_processing_feature_extraction:
  feature_extraction_name: FFT1024Input_256Feature_1Frame_Full_Bandwidth
  variables: 1
training:
  model_name: CLS_1k_NPU
  batch_size: 32
  training_epochs: 10
  num_gpus: 0
  early_stopping: true
  early_stopping_patience: 5
testing: {}
compilation: {}

FFT1024Input_256Feature_1Frame_Full_Bandwidth takes a 1024-sample frame, computes the FFT and keeps 256 frequency features of one frame (no temporal concatenation). This captures the high-frequency signature of arcs.

7.10.5.6. Configuration for the DSI Dataset

The DSI captures are sampled at 313 kHz, so the config downsamples them and windows the signal instead of using a feature extraction preset:

data_processing_feature_extraction:
  data_proc_transforms: [Downsample, SimpleWindow]
  gain_variations:
    arc: [0.9, 1.1]
    normal: [0.8, 1.2]
  sampling_rate: 313000
  new_sr: 3130
  frame_size: 256
  stride_size: 0.01
  variables: 1
training:
  model_name: CLS_13k_NPU
  batch_size: 2048
  training_epochs: 10

7.10.5.7. Available Models

Any enabled classification model can be used. Commonly used choices:

Model

Approx. parameters

Description

CLS_500_NPU

500

Small, NPU-optimized

CLS_1k_NPU

1,000

Baseline NPU model (default for the DSK config)

CLS_2k_NPU

2,000

Medium NPU model

CLS_4k_NPU

4,000

Larger NPU model

CLS_13k_NPU

13,000

Used for the DSI config

ArcFault_model_200_t / _300_t / _700_t / _1400_t

200 to 1,400

Arc fault specific models (also enabled in 1.5.0)

7.10.5.8. Results from the 1.5.0 Test Run

The following values come from the automated 1.5.0 config test logs (runs of each config with default settings, device F28P55 unless noted). They illustrate what to expect; your numbers will vary with the data split and random seed.

Config

Test accuracy

AUC ROC

config_dsk.yaml (CLS_1k_NPU)

100.00%

1.000

config_dsi.yaml (CLS_13k_NPU)

94.98%

0.976

config_dsi_ondevice_learning.yaml (CLS_24k_NPU, 1 epoch)

85.13%

0.960

config_anomaly_detection_dsi.yaml (AD_17k)

F1 score 100.00%

not applicable

Note

In the same test run, config_anomaly_detection_dsk.yaml failed during quantization-aware training (a per-channel fake-quantize error), so no result is reported for it. Treat that config as not yet working.

7.10.5.9. Interpreting Results

After training, check these outputs in the run folder (see Understanding the Run Output). The figures below are examples from the 1.4.0 version of this page and are shown for illustration only.

ROC curve (One_vs_Rest_MultiClass_ROC_test.png): the AUC should be close to 1.0.

ROC curve for arc fault detection

One-vs-rest multi-class ROC curves

Class score histogram (Histogram_Class_Score_differences_test.png): wide separation indicates a robust classifier.

Class score histogram

Distribution of class score differences

FPR/TPR CSV (fpr_tpr_thresholds.csv): use it to choose the operating threshold, balancing arc detection against false alarms.

7.10.5.10. Deployment Considerations

7.10.5.11. Next Steps