9.1.4. Non-NPU Deployment

Devices without a hardware NPU run the compiled model on the CPU. The deployment procedure is the same as for NPU devices: four files from one run go into an SDK example (Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check), CCS Integration Guide). This page lists the differences.

9.1.4.1. Non-NPU Devices

target_device

SDK example folder

Notes

F28004, F28003

C2000Ware libraries/ai/examples/<example>/f28004x/ or f28003x/

C28x CPU

F28P65

C2000Ware .../f28p65x/

C28x CPU

F29H85

F29H85x SDK examples/ai/<example>/f29h85x/

C29x CPU; examples call TI_NPU_init()

MSPM33C32

MSPM33 SDK examples/ai/<example>/mspm33c321a/

Cortex-M33

AM263

MCU-PLUS-SDK examples/ai/<example>/am263x_lp/r5fss0-0_nortos/

Cortex-R5F

MSPM0G3507, CC devices, xWRL6432

Not in tinyml-sdk

1.4.0 guidance: integrate mod.a, tvmgen_default.h and the feature-extraction library into your own project. See MSPM0 Family and Connectivity, AM26x, MSPM33 and Radar Devices.

The complete device list is in Device Overview.

9.1.4.2. Importing an Example That Is Not in Resource Explorer

Some examples are not listed in CCS Resource Explorer. Import them manually:

  1. File -> Import Projects.

File Import Projects menu

Selecting Import Projects from the File menu

  1. Browse to the example’s device folder and click Finish.

Browse to project folder

Browsing to the project folder

Then replace the four files, build, flash and check, exactly as in CCS Integration Guide.

9.1.4.3. CPU Inference Considerations

  • Model size. Without an NPU, cycles grow with the multiply-accumulate count of the model. Use models that list your device and keep them small.

  • Feature extraction runs on the CPU too. The SDK feature-extraction library (FFT, binning, windowing) is configured entirely by user_input_config.h. ModelMaker reports its code and data memory for many devices (Device Overview).

  • Memory. If the linker reports a section that does not fit, start from an example with a similar feature-extraction preset and adjust the lnk.cmd placement.

  • Timing. Measure on target with a CPU timer around tvmgen_default_run and FE_runFeatureExtract in application_main.c. The cycle and energy numbers of the 1.4.0 guide are not carried over because they were not re-measured for 1.5.0.

  • Integer types. If SKIP_NORMALIZE or OUTPUT_INT is defined in user_input_config.h, model_input_t and model_output_t are int8_t. Keep that file matched to mod.a.

9.1.4.4. Non-NPU vs NPU

Aspect

NPU devices

Non-NPU devices

Inference

Hardware accelerated, waits on tvmgen_default_finished

CPU only

Initialization

NPU module in SysConfig (or TI_NPU_init())

None needed for the model

Compile preset

default_preset / compress_npu_layer_data

default_preset

Models

NPU-compatible (*_NPU)

Any model that lists the device

9.1.4.5. Next Steps