7.10.13. Gas Sensor

Identify gases from a metal-oxide sensor array, and learn how the output_int option changes the model output format (quantized integer vs. dequantized float).

Example folder: examples/gas_sensor (GitHub)

7.10.13.1. Overview

The “Gas Sensor Array under Low Concentration” dataset from the UCI Machine Learning Repository contains 30-minute recordings sampled at 1 Hz from 10 metal-oxide semiconductor (MOS) sensors exposed to low concentrations of six gases. The example uses three of them, each at 100 ppb: ethyl acetate, isopropanol and hexane.

  • Application: environmental monitoring, industrial safety, air quality

  • Task: classification (generic_timeseries_classification), 3 classes

  • Data: 10 variables (Sensor_0 to Sensor_9), 64-sample windows

  • Device: F28P55

  • Model: CLS_1k_NPU

7.10.13.2. Preparing the Dataset

The config downloads https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/gas_sensor_dataset.zip automatically. To regenerate the zip from the UCI source run the helper script and point dataset.input_data_path to examples/gas_sensor/gas_sensor_dataset.zip:

cd examples/gas_sensor
python gas_sensor.py

7.10.13.3. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/gas_sensor/config.yaml

7.10.13.4. Configuration

common:
  task_type: generic_timeseries_classification
  target_device: F28P55
dataset:
  dataset_name: gas_sensor
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/gas_sensor_dataset.zip
  split_type: within_files
data_processing_feature_extraction:
  data_proc_transforms: ['SimpleWindow']
  frame_size: 64
  stride_size: 0.02
  variables: 10
  scale: 0.00390625   # 1/256
training:
  model_name: CLS_1k_NPU
  num_gpus: 0
  epochs: 20
  early_stopping: true
  early_stopping_patience: 5
  output_int: true
testing: {}
compilation: {}

7.10.13.5. Quantized vs. Dequantized Output (output_int)

After float training the model goes through quantization-aware or post-training quantization. The example demonstrates the difference between the output of native PyTorch quantization and the TI quantization wrappers (TINPUTinyMLQATFxModule / TINPUTinyMLPTQFxModule):

  • output_int: true (default): no multiply block is added to the last layer, so the model output stays in quantized INT8 format. This is faster because everything stays in the integer domain.

  • output_int: false: a multiply block is added to the last layer of the ONNX model that dequantizes the output to floating point.

Quantized vs dequantized outputs

Quantized vs. dequantized model outputs

The effect can be inspected in training/quantization/golden_vectors/test_vector.c of the run folder. With output_int: false the scaling factor learned for this model is 0.03125, so a dequantized output of {0.875, -0.4375, -0.40625} corresponds to the quantized output {28, -14, -13}.

7.10.13.6. Performance on Device

The example readme benchmarks CLS_1k_NPU on the F28P55x, on the CPU and on the NPU (TINPU). These numbers come from the example readme (they were measured with an earlier release):

Configuration

AI model cycles

Inference time (us)

Flash (B)

SRAM (B)

CPU, output_int true

665,234

4,434.89

4,143

3,880

CPU, output_int false

665,801

4,438.67

4,169

3,880

NPU, output_int true

80,339

535.59

3,529

1,680

NPU, output_int false

80,354

535.69

3,560

1,682

7.10.13.7. Results from the 1.5.0 Test Run

In the automated 1.5.0 config test run, config.yaml reached a test accuracy of 100.00% with an AUC ROC of 1.000 (CLS_1k_NPU, 1,271 parameters).

7.10.13.8. See Also