7.10.32. Wake Word Detection

Always-on detection of the wake word “OK Kilby” on the MSPM0G5187 with NPU, using a learned filterbank front-end and a TCDS-ResNet classifier. New in 1.5.0.

Example folder: examples/wake_word_detection (GitHub)

7.10.32.1. Overview

  • Task: audio classification (audio_classification, target_module: audio), 2 classes

  • Application: low-power, privacy-preserving voice interfaces for smart home, industrial and wearable devices. The wake word is detected on the device so no audio leaves it, and downstream voice-command processing is triggered only after a detection.

  • Device: MSPM0G5187 (config_MSPM0.yaml, the only config in the folder)

  • Model: TCDS_ResNet_FB_NPU

  • Targets in the readme: under 200 ms detection latency from the end of the utterance, a high detection rate with a low false-accept rate, and low average power for always-on, battery-operated listening

7.10.32.2. The Dataset

The wake word is “OK Kilby”. The data is a TI-internal dataset collected for this application and is not derived from a public dataset. It contains multiple speakers saying the wake word with varying tone, distance and speaking rate, background noise (household, office, ambient) and non-wake-word speech to reduce false accepts.

Class

Files in this example

Wake word (“OK Kilby”)

6000

Non-wake-word / background

4600

The subset used by the example is downloaded by the config from https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/wake_word_detection.zip. The readme notes that it is a small part of an internal dataset of more than 50 GB, so for a production-quality model you should collect and add your own wake word and background data (speakers, accents, distances, microphones and noise conditions).

7.10.32.3. Feature Extraction: Learned Filterbank

Instead of a fixed MFCC or FFT front-end, the model learns its filterbank jointly with the classifier. The config uses the preset WakeWordDetection_Filterbank_Default.

  1. Audio is sampled at 8 kHz with a 2-second window per inference (16,000 samples).

  2. A strided Conv1D filterbank (kernel 64, stride 4) slides over the raw audio and projects it into 32 channels (fb_output_channel of the WakeWordDetection_Filterbank_Default preset).

  3. A max-pool over each 20 ms context (160 samples) produces one feature vector per frame.

  4. Filterbank weights are quantized to 2 bits and the input audio to 16 bits.

  5. The features feed directly into the TCDS-ResNet backbone.

The commented lines in the config show the underlying preset keys (audio_feature: "FB", fb_conv_kernel, fb_output_channel, fb_bitwidth, fb_context_ms, fb_conv_stride, input_bit_depth).

7.10.32.4. Model

TCDS_ResNet_FB_NPU combines the learned filterbank with a Temporal Channel-Decoupled Separable ResNet:

  • Stem: Conv3x1, BatchNorm, ReLU (32 channels)

  • Backbone: 3 TCDS basic blocks (channels 32, 48, 64, 96). Each block has a main branch of depthwise 9x1, pointwise 1x1, depthwise 9x1, pointwise 1x1, and a skip branch (1x1 projection when the stride or channel count changes). The output is ReLU(main + skip).

  • Head: Dropout, Flatten, Fully Connected, 2 outputs

  • Mixed precision: stem and head at 8 bits, residual blocks at 2 bits

The non-filterbank variant TCDS_ResNet_NPU is also available. The audio models enabled in 1.5.0 are DSCNN_NPU, DSCNN_32K_NPU, DSCNN_GB_NPU, TCDS_ResNet_NPU and TCDS_ResNet_FB_NPU.

7.10.32.5. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/wake_word_detection/config_MSPM0.yaml

7.10.32.6. Configuration

common:
  target_module: audio
  task_type: audio_classification
  target_device: MSPM0G5187
dataset:
  dataset_name: wake_word_detection
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/wake_word_detection.zip
data_processing_feature_extraction:
  feature_extraction_name: WakeWordDetection_Filterbank_Default
  sampling_rate: 8000
  audio_duration_ms: 2000
training:
  model_name: TCDS_ResNet_FB_NPU
  batch_size: 4096
  training_epochs: 100
  num_gpus: 1
  quantization: 2
  learning_rate: 0.01
  weight_decay: 1e-5
  auto_quantization: False
testing: {}
compilation: {}

quantization: 2 with auto_quantization: False runs quantization-aware training with the mixed-precision scheme above. The example uses a batch size of 4096 and a learning rate of 0.01, as in the config shown here. num_gpus: 1 expects a GPU; use 0 for CPU. For the audio task type see Audio Classification.

7.10.32.7. Results

The example readme does not publish accuracy numbers. In the automated 1.5.0 config test run (test set of 1080 samples: 600 wake word, 480 others) the quantized model reached a test accuracy of 96.20% and an AUC ROC of 0.991. Treat these as indicative results from a short test run on the small subset.

7.10.32.8. Output Location

Results are written to ./data/projects/wake_word_detection/run/<date-time>/TCDS_ResNet_FB_NPU/. The compiled model and interface headers are in compilation/artifacts/. See Understanding the Run Output and Project Compilation Guide: Timeseries Classification Examples.

7.10.32.9. Running on Device

Build the deployment with the MSPM0 SDK (2.08.00 or later) and Code Composer Studio, with a microphone as audio input. The compiler flow uses the TI Neural Network Compiler; see Supported Devices for MSPM0G5187.

7.10.32.10. See Also