7.10.12. Grid Fault Detection

Detect AC grid faults for single-phase on-board chargers (OBC) of electric vehicles, running on an F29x MCU.

Example folder: examples/grid_fault_detection (GitHub)

7.10.12.1. Overview

Nearly all EVs and PHEVs have an on-board charger that must be robust to faults and abnormal conditions of the AC grid. Grid faults have highly variable signatures and are hard to detect with traditional threshold based heuristics. An edge-AI model running on the same MCU that controls the OBC power stage can protect the OBC against adverse grid events, log abnormal events, and potentially save the OBC.

TI’s approach uses a CNN trained on a proprietary grid fault dataset and running on the F29x MCU.

Variation of AC grid fault waveforms

Grid fault waveforms vary strongly between events

  • Application: EV on-board charger protection, grid event logging, power-stage safety

  • Task: classification (generic_timeseries_classification)

  • Data: univariate AC grid current, 16 samples per file

  • Device: F29H85

  • Model: CLS_1k_NPU

7.10.12.2. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/grid_fault_detection/config.yaml

7.10.12.3. Configuration

common:
  task_type: generic_timeseries_classification
  target_device: F29H85
dataset:
  dataset_name: grid_fault_detection
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/grid_fault_dataset.zip
data_processing_feature_extraction:
  data_proc_transforms: ['SimpleWindow']
  frame_size: 16
  stride_size: 1
  variables: 1
training:
  model_name: CLS_1k_NPU
  num_gpus: 0
  batch_size: 512
  training_epochs: 250
  early_stopping: true
  early_stopping_patience: 5
testing: {}
compilation: {}

7.10.12.4. Dataset and Feature Extraction

There are no well-defined fault categories for AC grid faults. The categories were defined with a hybrid annotation technique that combines human annotation and unsupervised annotation using hierarchical density based clustering; the quality of the annotation was evaluated with dimensionality reduction and manual QC.

For this example the feature extraction presets of ModelZoo are bypassed: SimpleWindow only frames the pre-processed data. The dataset has only 16 values per file, so frame_size must not exceed 16.

7.10.12.5. Results

The example readme does not publish accuracy numbers. In the automated 1.5.0 config test run the config finished quickly (early stopping is enabled with patience 5) with a test accuracy of 47.31% and an AUC ROC of 0.563, so the shipped configuration should be treated as a starting point that needs tuning (for example a longer patience or a different model) rather than a validated accuracy reference.

7.10.12.6. Deployment

See Project Compilation Guide: Timeseries Classification Examples and Deploying a ModelZoo Run to an SDK Example (Golden-Vector Check).

7.10.12.7. See Also