7.10.36. Machine Readable Code Classification

Classify a 28x28 image as a QR code, a barcode or something else, on the MSPM0G5187 with a LeNet-5 CNN.

Example folder: examples/machine_readable_code_classification (GitHub)

7.10.36.1. Overview

  • Task: image classification (image_classification, target_module: vision), 3 classes

  • Application: tiny visual pre-classification of machine readable codes on low-memory, low-power edge devices. The goal is not to decode the code, only to classify its visual structure. At 28x28 many generated codes would not be scannable by a real decoder, which is acceptable here.

  • Device: MSPM0G5187 (config_MSPM0.yaml, the only config in the folder)

  • Model: Lenet5

7.10.36.2. The Dataset

A synthetic dataset similar in size and format to MNIST: 28x28, one channel, binary black and white PNG images. The default size is 3000 images per class, 9000 in total.

Class

How it is generated

qr

QR codes from the Python qrcode package (version 1, error correction L, box size 4, border 1) with a random alphanumeric payload

barcode

Code128 barcodes from the python-barcode package with the text under the barcode disabled, so the model learns the line structure and not printed text

other

Blank white, blank black, random binary noise, random line patterns and random block patterns, so the class is not a single trivial pattern

All images go through the same conversion: grayscale, nearest-neighbor resize to 28x28 (to keep hard edges), threshold at 127, pixels set to 0 or 255. The script uses a fixed seed (42), so the dataset is reproducible with the same package versions.

The config downloads https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/machine_readable_code_classification.zip. To regenerate the data, install the dependencies and run the generator:

python -m pip install "qrcode[pil]" "python-barcode" pillow numpy
cd examples/machine_readable_code_classification
python generate_machine_readable_code_28x28.py

The dataset layout is one folder per class (qr, barcode, other). Point dataset.input_data_path at the generated zip or folder to use it.

7.10.36.3. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/machine_readable_code_classification/config_MSPM0.yaml

7.10.36.4. Configuration

common:
  target_module: vision
  task_type: image_classification
  target_device: MSPM0G5187
dataset:
  dataset_name: machine_readable_code_classification
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/machine_readable_code_classification.zip
data_processing_feature_extraction:
  feature_extraction_name: MachineReadable_Default
training:
  model_name: Lenet5
  batch_size: 64
  training_epochs: 10
  num_gpus: 0
  quantization: 2
  learning_rate: 0.1
  weight_decay: 1e-5
testing: {}
compilation: {}

The preset MachineReadable_Default converts to grayscale, resizes to 28x28 and normalizes with mean 0.5 and scale 0.5. The image models enabled in 1.5.0 are Lenet5, MobileNetV1_28k_NPU and MobileNetV2_58k_NPU. For the image task type see Image Classification.

7.10.36.5. Results

The readme does not publish accuracy numbers. In the automated 1.5.0 config test run (test set of 900 images, 300 per class) the quantized model reached 100.00% accuracy and an AUC ROC of 1.000. The classes are visually very distinct and the data is synthetic, so expect lower accuracy on photographs of real codes.

7.10.36.6. Output Location

Results are written to ./data/projects/machine_readable_code_classification/run/<date-time>/Lenet5/. See Understanding the Run Output and Project Compilation Guide: Timeseries Classification Examples for deployment.

7.10.36.7. See Also