7.10.27. PMSM Rotor Temperature Forecasting
Forecast the permanent magnet (rotor) temperature of a permanent magnet synchronous motor (PMSM) one step ahead, without a temperature sensor inside the motor.
Example folder: examples/forecasting_pmsm_rotor_temp
(GitHub)
7.10.27.1. Overview
Task: timeseries forecasting (
generic_timeseries_forecasting)Application: motor protection and derating. Magnets can lose strength permanently above about 150 C, and motor life shortens as temperature rises, but sensors deep inside a running motor are costly and fragile.
Configs and devices:
config.yaml: F28P55config_MSPM0.yaml: MSPM0G5187
Model:
FCST_LSTM8(an LSTM, 393 parameters according to the readme)Target:
pm(permanent magnet surface temperature), one step ahead
7.10.27.2. The Dataset
The data are measurements from a PMSM prototype on a test bench (German OEM motor, recorded by the LEA department at Paderborn University), sampled at 2 Hz: Electric Motor Temperature (Kaggle).
From the original columns the example keeps signals that are easy to measure: ambient temperature (ambient),
coolant temperature (coolant), the voltage components (u_d, u_q) and the phase current magnitude
i_a = sqrt(i_d^2 + i_q^2). Using past values of these and of the permanent magnet temperature pm, the
model forecasts pm for the next time step. The config uses variables: 6 (i_a, u_d, u_q,
ambient, coolant, pm) and target_variables: [5] (pm).
The dataset is downloaded from https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/pmsm_rotor_temp.zip. It
follows the forecasting layout (files/ plus annotations/), see Forecasting Dataset Format.
7.10.27.3. Running the Example
Install Tiny ML ModelZoo first (Installation, Quickstart), then run from
the tinyml-modelzoo folder:
./run_tinyml_modelzoo.sh examples/forecasting_pmsm_rotor_temp/config.yaml
# MSPM0G5187 variant
./run_tinyml_modelzoo.sh examples/forecasting_pmsm_rotor_temp/config_MSPM0.yaml
See Running Examples for all launchers, for example:
run_tinyml_modelzoo.bat examples\forecasting_pmsm_rotor_temp\config.yaml
7.10.27.4. Configuration
common:
task_type: generic_timeseries_forecasting
target_device: F28P55
dataset:
dataset_name: forecasting_pmsm_rotor_temp
input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/pmsm_rotor_temp.zip
data_processing_feature_extraction:
data_proc_transforms:
- SimpleWindow
frame_size: 3
stride_size: 0.4
forecast_horizon: 1
variables: 6
target_variables:
- 5
training:
model_name: FCST_LSTM8
model_config: ''
batch_size: 256
training_epochs: 20
early_stopping: true
early_stopping_patience: 5
num_gpus: 0
quantization: 2
optimizer: adam
learning_rate: 0.005
output_int: false
testing: {}
compilation: {}
SimpleWindowandframe_sizeare mandatory for forecasting; feature extraction is not supported.output_intmust befalse.config_MSPM0.yamldiffers only in the target device (MSPM0G5187) and in having no early stopping.
7.10.27.5. Evaluation
The metrics are SMAPE (0 to 200%, lower is better) and R2 (higher is better). The epoch with the lowest SMAPE
across all targets and predicted time steps is the best epoch. Per-epoch plots and CSV files are written to the
best_epoch_<n>_results and test_results folders (see below).
7.10.27.6. Results
Results of the example readme (best epoch statistics, SMAPE and R2 of pm, time step 1):
Stage |
SMAPE |
R2 |
|---|---|---|
Float train, best epoch 19 |
0.09% |
1.0000 |
Quantized train, best epoch 10 |
0.26% |
0.9999 |
Test set |
0.25% |
0.9998 |
The automated 1.5.0 config test run of config.yaml gave a quantized best epoch SMAPE of 0.11% (R2 0.9999) and
a test SMAPE of 0.13% (R2 0.9999), consistent with the readme.
Predicted versus actual permanent magnet temperature (black dotted line is the ideal x = y)
7.10.27.7. Output Location
Results are written to ./data/projects/forecasting_pmsm_rotor_temp/run/<date-time>/FCST_LSTM8/:
training/base/best_epoch_<n>_results: float modeltraining/quantization/best_epoch_<n>_resultsandtraining/quantization/test_results: quantized model, each withprediction_plotsandpredictions_csvcompilation/artifacts/:mod.aandtvmgen_default.htraining/quantization/golden_vectors/:test_vector.canduser_input_config.h
7.10.27.8. Running on Device
The readme compiled the example with the TI-NPU software preset for F28P55 and ran it on a LAUNCHXL-F28P55X (C2000Ware 6.0.1, CCS 20.2.0). Follow Deploying Forecasting Models from ModelMaker to Device. After flashing, the model output matches the golden vectors.
On-device output matching the golden vectors
Measured on the device (example readme, written for 1.3):
Metric |
Value |
|---|---|
Cycles |
102307 |
Inference time |
682.05 us |
Code size |
4375 bytes |
Results match golden vectors |
TRUE |