7.10.28. HVAC Indoor Temperature Forecasting

Forecast the indoor temperature of a room from compressor frequency and outdoor temperature, as an input to predictive HVAC control.

Example folder: examples/hvac_indoor_temp_forecast (GitHub)

7.10.28.1. Overview

Traditional HVAC controllers react to temperature deviations after they occur, which causes delayed corrections, unnecessary compressor activity and higher energy use. A forecast of the indoor temperature lets a higher-level controller plan smoother, more energy-efficient compressor actions. This example trains a small LSTM offline and compiles it to run fully on the device.

  • Task: timeseries forecasting (generic_timeseries_forecasting)

  • Device: F28P55 (config.yaml), compiled with the forced_soft_npu_preset (software emulation of the NPU)

  • Model: FCST_LSTM10

  • Target: indoorTemperature at the next time step (set forecast_horizon for a longer horizon)

7.10.28.2. The Dataset

A synthetic dataset that emulates indoor thermal behavior. It has uniformly sampled values of:

  1. compressorFrequency

  2. outdoorTemperature

  3. indoorTemperature

The model input is the past 5 values of each of the three signals (frame_size: 5, variables: 3) and the target is indoorTemperature (column index 2, counting from 0 after the time column). The config downloads https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/hvac_indoor_temp_forecast_dataset.zip. The layout is the forecasting layout described in Forecasting Dataset Format.

Note

In the automated 1.5.0 config test run this config failed while extracting the download (“File is not a zip file”). If you see the same error, check that the dataset URL returns a valid zip before debugging the pipeline.

7.10.28.3. Running the Example

Install Tiny ML ModelZoo first (Installation, Quickstart), then run from the tinyml-modelzoo folder:

./run_tinyml_modelzoo.sh examples/hvac_indoor_temp_forecast/config.yaml

7.10.28.4. Configuration

common:
  task_type: generic_timeseries_forecasting
  target_device: F28P55
dataset:
  dataset_name: hvac_indoor_temp_forecast
  input_data_path: https://software-dl.ti.com/C2000/esd/mcu_ai/datasets/hvac_indoor_temp_forecast_dataset.zip
data_processing_feature_extraction:
  data_proc_transforms:
  - SimpleWindow
  frame_size: 5
  stride_size: 0.2
  forecast_horizon: 1
  variables: 3
  target_variables:
  - 2
training:
  model_name: FCST_LSTM10
  model_config: ''
  batch_size: 6
  training_epochs: 10
  early_stopping: true
  early_stopping_patience: 5
  num_gpus: 0
  quantization: 1
  optimizer: adamw
  learning_rate: 0.003
  weight_decay: 0.001
  lr_scheduler: none
  output_int: false
testing: {}
compilation:
  compile_preset_name: forced_soft_npu_preset

target_variables also accepts column names or several indices. output_int must be false for forecasting.

7.10.28.5. Results

The example readme reports these results for the indoor temperature (time step 1):

Stage

SMAPE

R2

Float train, best epoch

0.30%

0.9971

Quantized train, best epoch 4

0.80%

0.9893

Test set

0.73%

0.9857

Warning

These numbers come from the example readme and were not reproduced in 1.5.0 because the test run could not download the dataset. Quantized FCST_LSTM10 models have shown a large accuracy drop in other 1.5.0 runs (see Generic Timeseries Forecasting), so compare the float and quantized results of your own run.

Predicted versus actual indoor temperature

Predicted versus actual indoor temperature

7.10.28.6. Output Location

Results are written to ./data/projects/hvac_indoor_temp_forecast/run/<date-time>/FCST_LSTM10/. The device files are compilation/artifacts/mod.a, compilation/artifacts/tvmgen_default.h and the golden vectors in training/quantization/golden_vectors/.

7.10.28.7. Running on Device

Follow Deploying Forecasting Models from ModelMaker to Device. After flashing, the model output matches the golden vectors.

On-device results

On-device output matching the golden vectors

Device measurements from the readme (F28P55x, written for an earlier release):

Metric

Value

AI model cycles

199432

Inference time

1329.55 us

Model size (flash / SRAM)

9174 bytes / 278 bytes

Results match golden vectors

TRUE

7.10.28.8. See Also