2.4. Windows Setup

Windows-specific notes for Tiny ML ModelZoo 1.6.0. Both native Windows and WSL2 work; Linux is the primary development platform.

2.4.1. Native Windows

  1. Install Python 3.10 (see Prerequisites).

  2. Enable long paths in Git (only for the clone install), once per system:

    git config --global core.longpaths true
    
  3. Create a virtual environment and install, using one of the two install paths:

    python -m venv venv
    .\venv\Scripts\Activate.ps1
    python -m pip install --upgrade pip setuptools wheel
    
    # Wheel install
    pip install http://software-dl.ti.com/C2000/esd/mcu_ai/wheel/tinyml_modelzoo-1.5.0-py3-none-any.whl
    
    # or clone install
    git clone https://github.com/TexasInstruments/tinyml-modelzoo.git
    cd tinyml-modelzoo
    pip install -e .
    
  4. Set the compiler variable for your device (Environment Variables).

  5. Run the hello world example from the cloned folder:

    run_tinyml_modelzoo.bat examples\generic_timeseries_classification\config.yaml
    

    or in PowerShell: ./run_tinyml_modelzoo.ps1 examples/generic_timeseries_classification/config.yaml. With the wheel install, use python -m tinyml_modelmaker.run_tinyml_modelmaker config.yaml (see Wheel Installation).

ti_mcu_nnc (the compiler) is published for Windows x86_64 on Python 3.10.

2.4.2. WSL2

WSL2 gives a full Linux environment. See the WSL documentation.

wsl --install --web-download --distribution Ubuntu-22.04

Restart when prompted and run the command again to create the UNIX user. Then follow Linux Setup inside the WSL shell.

Tip

Keep project files inside the WSL filesystem (/home/<user>), not on /mnt/c, for much better performance. Browse WSL files from Windows at \\wsl.localhost\Ubuntu-22.04.

2.4.2.1. Behind a Proxy (WSL)

If apt or pip cannot reach the network, set proxy variables, for example in /etc/profile.d/proxy.sh:

export http_proxy="http://your.proxy.address:port"
export https_proxy="http://your.proxy.address:port"
export no_proxy="localhost,127.0.0.1"

and Acquire::http::proxy / Acquire::https::proxy in /etc/apt/apt.conf. Run wsl --shutdown afterwards. If DNS fails, set a nameserver in /etc/resolv.conf and generateResolvConf = false under [network] in /etc/wsl.conf.

USB devices (such as LaunchPads) can be attached to WSL with usbipd-win.

2.4.3. Common Windows Issues

Path too long

Enable Git long paths (above) and clone to a short path such as C:\dev. System-wide: set LongPathsEnabled to 1 in HKLM:\SYSTEM\CurrentControlSet\Control\FileSystem (as Administrator).

Running scripts is disabled

Set-ExecutionPolicy -ExecutionPolicy RemoteSigned -Scope CurrentUser

Virtual environment activation fails

Use .\venv\Scripts\activate.bat or call .\venv\Scripts\python.exe directly.

CUDA GPU

Install the NVIDIA driver, then set training.num_gpus: 1 in the config. Check with python -c "import torch; print(torch.cuda.is_available())".

2.4.4. Next Steps