SDL STOG Example

Introduction

This example demonstrates the usage of the TOG module. The example shows how to listen for TOG error events using the ESM, and also forcing an error in order to demonstrate application notification of a timeout event.

The example demonstrates:

  1. Setting a timeout for TOG instance

  2. Error injection for an TOG instance

  3. Error event detection for a timeout event

Use Cases

  • The TOG is programmed with a timeout that is small enough to trigger a timeout event on any access. Error event is triggered and application is notified of the event.

Supported Combinations

Parameter

Value

CPU + OS

mcu-r5fss0-0 nortos

Toolchain

ti-arm-clang

Board

am62px-sk

Example folder

examples/sdl/stog/

Steps to Run the Example

See Also

STOG

Sample Output

[MCU_R5FSS0_0]
TOG Sample Example

Init MCU ESM complete

SDL_TOG_setIntrEnable complete

SDL_TOG_init.timeout complete

SDL_TOG_start complete

SDL_TOG_stop complete

All tests have passed.