PANEL
The Panel driver provides API to control I2C based display bridge driver present in the board. The display bridge can be a DPI/DSI based bridge that can convert DPI/DSI signals to HDMI output or any other output format.
The AM62P-sk board has a SII9022A bridge (Lattice semiconductor), I2C based DPI to HDMI output bridge, that takes DPI output from SoC and converts them to HDMI signals. The panel driver allows configuration over sysconfig and integrates a I2C based driver for SII9022A bridge.
Features Supported
Configurable I2C address for bridge.
Configurable I2C address for specific GPIO pin control for bridge.
Video timing parameters configuration for SII9022A bridge.
Configuration for output resolution for SII9022A bridge.
SysConfig Features
Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
Option to specify I2C address for the bridge and bridge pin control.
Configuration for SII9022A bridge.
Features NOT Supported
DSI bridge.
Example Usage
Include the below file to access the APIs
//! [include]
#include <board/panel/panel_i2c.h>
BridgeSii9022a_Object gBridgeSii9022aObj =
{
.modeInfo = {
.standard = FVID2_STD_1080P_60,
.modeCode = 16,
.pixClk = 14850,
.vFreq = 60,
.pixels = 2200,
.lines = 1125,
.embSyncPrms = {
.hBitToHSync = 88,
.field2Offset = 0,
.hWidth = 44,
.vBitToVSync = 4,
.vWidth = 5.
},
.extSyncPrms = {
.deDelay = 192,
.deTop = 41,
.deCnt = 1920,
.deLine = 1080,
}
}
};
/* PANEL Driver handles - opened during Board_panelOpen() */
Panel_Handle gPanelHandle[CONFIG_PANEL_NUM_INSTANCES];
Panel_Params gPanelParams[CONFIG_PANEL_NUM_INSTANCES] =
{
{
.bridgeParams = {
.deviceI2cInstId = HDMI_I2C_CONFIG,
.deviceI2cAddr = 0x3B,
.inpClk = 0U,
.hotPlugGpioIntrLine = 0U,
.clkEdge = FALSE,
.outputFormat = BRIDGE_SII9022A_HDMI_RGB,
},
.vidOutParams = {
.standard = FVID2_STD_1080P_60,
.videoDataFormat = FVID2_DF_RGB24_888,
.videoIfMode = FVID2_VIFM_SCH_DS_AVID_VSYNC,
.videoIfWidth = FVID2_VIFW_24BIT,
}
},
};
Panel_PinCtrl gPinCtrlConfig[CONFIG_PANEL_NUM_INSTANCES] =
{
{
.pinCtrlI2cInstance = HDMI_I2C_CONFIG,
.pinCtrlI2cAddr = 0x23,
.numPins = 1,
.pinConf = {
{
.pinIoNum = 21,
.pinType = TCA6424_MODE_OUTPUT,
.pinVal = TCA6424_OUT_STATE_HIGH,
}
},
},
};
/* PANEL Config */
Panel_Config gPanelConfig[CONFIG_PANEL_NUM_INSTANCES] =
{
{
.panelType = CONFIG_PANEL_TYPE_I2C,
.fxns = &gPanelBridgeSii9022aFxns,
.object = (void *)&gBridgeSii9022aObj,
.pinConfig = &gPinCtrlConfig[0],
},
};
uint32_t gPanelConfigNum = CONFIG_PANEL_NUM_INSTANCES;
//! [include]
Instance Open Example
//! [open]
gPanelHandle[CONFIG_PANEL0] = NULL;
gPanelHandle[CONFIG_PANEL0] = Panel_open(CONFIG_PANEL0, &gPanelParams[CONFIG_PANEL0]);
if (!gPanelHandle[CONFIG_PANEL0])
{
DebugP_assert(FALSE);
}
//! [open]
Instance Close Example
//! [close]
Panel_close(gPanelHandle[CONFIG_PANEL0]);
//! [close]
API Reference
Unnamed Group
-
CONFIG_PANEL_TYPE_I2C
Panel type supported.
-
CONFIG_PANEL_TYPE_DSI
-
CONFIG_PANEL_TYPE_INVALID
Panel driver implementation callbacks
-
typedef int32_t (*Panel_OpenFxn)(Panel_Config *config, Panel_Params *params)
Driver implementation to open a specific panel driver.
Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.
- Param config:
[in] Panel configuration for the specific panel device
- Param params:
[in] User controllable parameters when opening the panel device
- Return:
SystemP_SUCCESS on success, else failure
-
typedef void (*Panel_CloseFxn)(Panel_Config *config, Panel_Params *params)
Driver implementation to close a specific panel driver.
Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.
- Param config:
[in] Panel configuration for the specific panel device.
- Param params:
[in] User controllable parameters when opening the panel device.
- Return:
SystemP_SUCCESS on success, else failure.
-
typedef int32_t (*Panel_ControlFxn)(Panel_Config *config, Panel_Params *params, uint32_t cmd, void *cmdArgs)
Driver implementation to control panel using a specific panel driver.
Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.
- Param config:
[in] Panel configuration for the specific panel device.
- Param params:
[in] User controllable parameters.
- Param cmd:
[in] Specific command to panel control.
- Param cmdArgs:
[in] Pointer to arguments associated with command.
- Return:
SystemP_SUCCESS on success, else failure
-
typedef int32_t (*Panel_ResetFxn)(Panel_Config *config, Panel_Params *params)
Driver implementation to soft reset the panel.
Typically this callback is hidden from the end application and is implemented when a new type of panel device needs to be implemented.
- Param config:
[in] Panel configuration for the specific panel device.
- Param params:
[in] User controllable parameters when opening the panel device.
- Return:
SystemP_SUCCESS on success, else failure.
Defines
-
PANEL_INVALID_VALUE
-
PANEL_MAX_NUM_PINS_CTRL
Max number pins configured for panel pin control.
Typedefs
-
typedef void *Panel_Handle
Handle to the FLash driver returned by Panel_open()
Functions
-
Panel_Handle Panel_open(uint32_t instanceId, Panel_Params *params)
Open panel driver.
Global variables
Panel_Config gPanelConfig[]anduint32_t gPanelConfigNumis instantiated by SysCfg to describe the panel configuration based on user selection in SysCfg.- Parameters:
instanceId – [in] Index within
Panel_Config gPanelConfig[]denoting the panel driver to open.params – [in] Open parameters.
- Returns:
Handle to panel driver which should be used in subsequent API call.
- Returns:
NULL in case of failure.
-
void Panel_close(Panel_Handle handle)
Close panel driver.
- Parameters:
handle – [in] Panel driver handle from Panel_open.
-
Panel_Handle Panel_getHandle(uint32_t instanceId)
Get handle to panel driver.
- Parameters:
instanceId – [in] Index within
Panel_Config gPanelConfig[].- Returns:
Handle to panel driver.
- Returns:
NULL in case of failure.
-
int32_t Panel_control(Panel_Handle handle, uint32_t cmd, void *cmdArgs)
Control Panel operation using panel specific commands.
Commands can be refered from specific panel interface layer.
- Parameters:
handle – [in] Panel driver handle from Panel_open.
cmd – [in] Input command to control panel.
cmdArgs – [in] Pointer to command arguments.
- Returns:
SystemP_SUCCESS on success, else failure.
-
int32_t Panel_reset(Panel_Handle handle)
Do a reset of the panel.
- Parameters:
handle – [in] Panel driver handle from Panel_open.
- Returns:
SystemP_SUCCESS on success, else failure.
-
uint32_t Panel_getPanelInterfaceIndex(uint32_t panelType)
Return panel index based on type of panel.
- Parameters:
panelType – [in] Panel type.
- Returns:
Panel driver instance index corresponding to the panel type.
-
void Panel_init(void)
This function initializes the Panel module.
-
void Panel_deinit(void)
This function de-initializes the Panel module.
-
struct Panel_BridgeParams
- #include <panel.h>
Bridge configuration parameters.
Public Members
-
uint32_t deviceI2cInstId
I2C device instance ID to use.
-
uint32_t deviceI2cAddr
I2C device address for each device
-
uint32_t inpClk
input clock.
-
uint32_t hotPlugGpioIntrLine
Hot plug GPIO interrupt line no - if supported by bridge.
-
uint32_t clkEdge
Specifies the clock edge to be used to latch data on. FALSE spacifies to latch on falling edge, raising edge otherwise.
-
uint32_t outputFormat
-
uint32_t deviceI2cInstId
-
struct Panel_vidOutputParams
- #include <panel.h>
Configuration paramters for bridge encoder.
Public Members
-
uint32_t standard
Video standard. For valid values see Fvid2_Standard.
-
uint32_t videoIfMode
Select the video mode, like Embedded sync, different type of Discrete sync modes. For valid values see Fvid2_VideoIfMode.
-
uint32_t videoIfWidth
videoIfWidth
:
Video Interface width , valid options are
FVID2_VIFW_8BIT,
FVID2_VIFW_10BIT,
FVID2_VIFW_16BIT,
FVID2_VIFW_24BIT,
For valid values see Fvid2_VideoIfWidth.
.
-
uint32_t videoDataFormat
RGB or YUV data format. valid values are given below
For valid values see
Fvid2_DataFormat. For Sil9022a bridge following data formats are supported videoDataFormat:
Output Data format, valid options are
FVID2_DF_YUV422I_YUYV,
FVID2_DF_RGB24_888,
-
uint32_t standard
-
struct Panel_PinConfig
- #include <panel.h>
Panel pin control data.
-
struct Panel_PinCtrl
- #include <panel.h>
Configuration paramters for panel pin control.
-
struct Panel_Params
- #include <panel.h>
Parameters passed during Panel_open()
-
struct Panel_Fxns
- #include <panel.h>
Driver implementation callbacks.
Public Members
-
Panel_OpenFxn openFxn
Panel driver implementation specific callback
-
Panel_CloseFxn closeFxn
Panel driver implementation specific callback
-
Panel_ControlFxn controlFxn
Panel driver implementation specific callback
-
Panel_ResetFxn resetFxn
Panel driver implementation specific callback
-
Panel_OpenFxn openFxn
-
struct Panel_Config
- #include <panel.h>
Panel driver configuration, these are filled by SysCfg based on the panel device that is selected.
Public Members
-
uint32_t panelType
Type of Panel interface
-
Panel_Fxns *fxns
Panel device implementation functions
-
void *object
Panel driver object, used to maintain driver implementation state
-
void *inputParams
Pointer to Panel params used for Panel config
-
Panel_PinCtrl *pinConfig
Pointer to Panel pin control structure
-
SemaphoreP_Object lockSem
Semaphore to protect the panel layer calls per instance.
-
uint32_t panelType