SBL UART
Introduction
This bootloader does SOC initializations and attempts to boot a multicore appimage received over UART via XMODEM. The image file is sent using a python script (See UART Bootloader Python Script). Once image is received, the SBL then parses it, splits it into RPRCs for each core applicable. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
wkup-r5fss0-0 nortos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/boot/sbl_uart |
Refer Enabling DDR inline ECC enablig inline ECC
Steps to Run the Example
Build the example
Since this is a bootloader and is used as a SOC initialization binary, the example will be run every time you boot an application using this example. It is generally run from a boot media (OSPI Flash, SD Card or over UART) unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles).
Run the example
Note
For HS-SE device, use default_sbl_uart_hs.cfg as the cfg file.
Note
For HS-FS device, use default_sbl_uart_hs_fs.cfg as the cfg file.
Run the following command from the {MCU_PLUS_SDK_INSTALLATION_PATH}/tools/boot
For am62px-sk
python uart_bootloader.py -p /dev/ttyUSB0 --cfg=sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_uart.cfg
Here /dev/ttyUSB0 can be changed to COM port like’COM4’ incase of Windows.
See Also
Sample Output
Since this SBL receives the appimage over UART using XMODEM protocol, it doesn’t print anything to the console so as not to corrupt the XMODEM transport.