Firewall Isolation - MCU Domain
Introduction
The example demonstrates the MCU firewall isolation in the use case when the MCU domain is running a safety application. The MCU-R5 application configures a firewall to the MAIN domain I2C by allowing access only to the MCU-R5 core and locks this firewall configuration ownership to the MCU core. After configuring the firewall, it reads data from the main domain I2C to check the access from MCU-R5 core. Then it will a send a ipc notify message to the Wkup-R5 core to trigger a firewall exception. The Wkup-R5 application waits for ipc notify message from the MCU core. Upon receiving the message, it triggers a firewall exception by accessing the I2C0 register config and it will go to data abort. The MCU-R5 receives a interrupt for firewall exception. If the interrupt is not received the test fails.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
mcu-r5fss0-0 nortos |
CPU + OS |
wkup-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/safety/fwl_isolation |
Steps
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Sample Output
Shown below is a sample output when the application is run,
################################ Wakeup R5 Log #######################################
Sciserver Testapp Built On: Nov 15 2023 10:51:56
Sciserver Version: v2023.09.0.0-REL.MCUSDK.09.00.01.01+
RM_PM_HAL Version: w09.00.01-am62p
Starting Sciserver..... PASSED
Waiting for ipc notify message to trigger firewall exception....
################################ MCU R5 Log #######################################
Configure I2C0 firewall to allow access only to MCU core... DONE !!!
Readback the firewall configuration ... DONE !!!
Retrieved Firewall data:
Fwl ID: 8
Region No: 1
Control: 0x0000000A
No of permission regs: 3
Permission[0]: 0x0060FFFF
Permission[1]: 0x0060FFFF
Permission[2]: 0x0060FFFF
Start address: 0x0000000020000000
End address: 0x0000000020000FFF
I2C read data through MCU core... !!!
Sample 0: 170
Sample 1: 85
Sample 2: 51
Sample 3: 238
Sample 4: 1
I2C read data through MCU core... DONE !!!
Waiting for firewall exception trigger from the other core...
Firewall exception occurred...
All tests have passed!!