Hello World Project

Introduction

This example just does driver and board initialization and prints the string, Hello World! on UART console.

Supported Combinations

Parameter

Value

CPU + OS

mcu-r5fss0-0 nortos

CPU + OS

mcu-r5fss0-0 freertos

CPU + OS

wkup-r5fss0-0 freertos

Toolchain

ti-arm-clang

Toolchain

arm.gnu.aarch64-none

Board

am62px-sk

Example folder

examples/hello_world/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Attention

As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.

Sample Output

Shown below is a sample output when the application is run,

Hello World!