Cache
Features Supported
APIs to perform below cache operations
region based writeback
region based invalidate
region based writeback invalidate
enable and disable APIs for I cache and D cache
full cache writeback, write invalidte
Features NOT Supported
NA
Important Usage Guidelines
The region based cache APIs,
CacheP_wb,CacheP_wbInv,CacheP_inv, operate on a CPU cache line, hence its strongly recommended to make sure ‘addr’ is cache line aliged and ‘size` is a multiple of cache line sizeStart address is calculated as follows, start_addr = floor(addr, CPU_CACHE_LINE)
End address is calculated as follows, end_addr = ceil(addr + size, CPU_CACHE_LINE)
No error is returned, for unaligned addr and size
On R5F,
Valid values for
CacheP_TypeforCacheP_enableandCacheP_disableareCacheP_TYPE_L1D,CacheP_TYPE_L1P,CacheP_TYPE_ALLValid values for
CacheP_TypeforCacheP_wb,CacheP_wbInv,CacheP_inv,CacheP_wbAll,CacheP_wbInvAllareCacheP_TYPE_L1D,CacheP_TYPE_ALL
CPU cache lines sizes for reference
R5F: 32B
A53: 64B
On R5F, It is recommended to enable both program and data cache in R5F in all applications. In R5F for cache to be enabled MPU needs to be enabled.
On M4F, the CPU does not support cache so these APIs when used with M4F, will be blank and will have no effect
Example Usage
Include the below file to access the APIs,
Example usage for cache write back invalidate:
Example usage for cache invalidate:
API Reference
Cache Type
Values defined for CacheP types
-
CacheP_TYPE_L1P
L1 program cache
-
CacheP_TYPE_L1D
L1 data cache
-
CacheP_TYPE_L2P
L2 program cache
-
CacheP_TYPE_L2D
L2 data cache
-
CacheP_TYPE_L1
All L1 cache’s
-
CacheP_TYPE_L2
All L2 cache’s
-
CacheP_TYPE_ALLP
All program cache’s
-
CacheP_TYPE_ALLD
All data cache’s
-
CacheP_TYPE_ALL
All cache’s
Defines
-
CacheP_CACHELINE_ALIGNMENT
Cache line size for alignment of buffers. Actual CPU defined cache line can be smaller that this value, this define is a utility macro to keep application portable across different CPU’s.
Functions
-
void CacheP_enable(uint32_t type)
Cache enable.
- Parameters:
type –
[in] cache type’s to enable
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
void CacheP_disable(uint32_t type)
Cache disable.
- Parameters:
type –
[in] cache type’s to disable
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
uint32_t CacheP_getEnabled(void)
Get cache enabled bits.
- Returns:
cache type’s that are enabled
-
void CacheP_wbAll(uint32_t type)
Cache writeback for full cache.
- Parameters:
type –
[in] cache type’s to writeback
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
void CacheP_wbInvAll(uint32_t type)
Cache writeback and invalidate for full cache.
- Parameters:
type –
[in] cache type’s to writeback and invalidate
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
void CacheP_wb(void *addr, uint32_t size, uint32_t type)
Cache writeback for a specified region.
- Parameters:
addr – [in] region address. Recommend to specify address that is cache line aligned
size – [in] region size in bytes. Recommend to specify size that is multiple of cache line size
type –
[in] cache type’s to writeback
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
void CacheP_inv(void *addr, uint32_t size, uint32_t type)
Cache invalidate for a specified region.
- Parameters:
addr – [in] region address. Recommend to specify address that is cache line aligned
size – [in] region size in bytes. Recommend to specify size that is multiple of cache line size
type –
[in] cache type’s to invalidate
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
void CacheP_wbInv(void *addr, uint32_t size, uint32_t type)
Cache writeback and invalidate for a specified region.
- Parameters:
addr – [in] region address. Recommend to specify address that is cache line aligned
size – [in] region size in bytes. Recommend to specify size that is multiple of cache line size
type –
[in] cache type’s to writeback and invalidate
R5: Supports CacheP_TYPE_L1P, CacheP_TYPE_L1D, A53: Supports CacheP_TYPE_L1P , CacheP_TYPE_L2P, CacheP_TYPE_L1D and CacheP_TYPE_L2D, C66x: Not used assumes CacheP_TYPE_ALL, M4: Not supported
-
void CacheP_init(void)
Initialize Cache sub-system, called by SysConfig, not to be called by end users.
Variables
-
CacheP_Config gCacheConfig
Externally defined Cache configuration.
-
struct CacheP_Config
- #include <CacheP.h>
Cache config structure, this used by SysConfig and not to be used by end-users directly.