SDL RTI

Introduction

The following shows an example of SDL RTI API usage by the application to set up the RTI as a watchdog and usage of the various APIs. Events can be monitored by enabling the events in the associated ESM instance.

Use Cases

Use Case

Description

UC-1

WINDOWSIZE_100_PERCENT

UC-2

WINDOWSIZE_50_PERCENT

UC-3

Latency/Propagation timing error(early)(50% window)

UC-4

Latency/Propagation timing error(late)(50% window)

Supported Combinations

Parameter

Value

CPU + OS

mcu-r5fss0-0 nortos

Toolchain

ti-arm-clang

Board

am62px-sk

Example folder

examples/sdl/rti/uc1/

Example folder

examples/sdl/rti/uc2/

Example folder

examples/sdl/rti/uc3/

Example folder

examples/sdl/rti/uc4/

Steps to Run the Example

See Also

RTI

Sample Output

Shown below is a sample output when the application is run,

Shown below is a sample output when the application is run,

UC1:

  RTI Example Test Application

RTI_Test_init: Init MCU ESM complete

RTI Example code UC-1 started
   DWWD configured to 100 percent window size
   DWWD is configured for 10000 ms time-out

RTI DWWD proper servicing test running.
   Please wait for max 10000 ms.

RTI DWWD proper servicing test successful.


RTI permanent failure test running.
   DWWD will generate interrupt after 10 seconds
   Wait for 10 sec for interrupt to be generated by DWWD.

RTI Window End time violation test successful.

Test Name: RTI EXAMPLE TEST  PASSED

 All tests have passed.

UC2:

 RTI Example Test Application

RTI_Test_init: Init MCU ESM complete

RTI Example code UC-2 started
   DWWD configured to 50 percent window size
   DWWD is configured for 10000 ms time-out

RTI DWWD proper servicing test running.
   Please wait for max 10000 ms.

RTI DWWD proper servicing test successful.


RTI permanent failure test running.
   DWWD will generate interrupt after 10 seconds
   Wait for 10 sec for interrupt to be generated by DWWD.

RTI Window End time violation test successful.

Test Name: RTI EXAMPLE TEST  PASSED

 All tests have passed.

UC3:

 RTI Example Test Application

RTI_Test_init: Init MCU ESM complete

RTI Example code UC-3 started
    DWWD configured to 50 percent window size
    DWWD is configured for 10000 ms time-out


RTI DWWD Early Trigger violation test running.


Servicing before the window open.


RTI DWWD Early Trigger violation test successful.

Test Name: RTI EXAMPLE TEST  PASSED

 All tests have passed.

UC4:

 RTI Example Test Application

RTI_Test_init: Init MCU ESM complete

RTI Example code UC-4 started
    DWWD configured to 50 percent window size
    DWWD is configured for 10000 ms time-out
    DWWD will generate interrupt after 10 seconds

Waiting for window to expire

Wait for 10 sec for interrupt to be generated by DWWD.


RTI Late trigger servicing test running.

   Re-Opening the window to service after previous feed
   RTI Late trigger servicing test successful.

Test Name: RTI EXAMPLE TEST  PASSED

 All tests have passed.