UART Echo DMA Multi-Instance
Introduction
This example demonstrates the UART RX and TX operation in blocking, DMA-PKTDMA mode of operation for two UART instances. Two uart instances runs parallely asking the user to input 8 characters and once both the transfer is completed successfully, the application ends.
The user should input 8 characters in UART0 and UART1.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
wkup-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/uart/uart_echo_dma_multi_instance |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Please select the UART port used for console as mentioned in Setup UART Terminal
See Also
Sample Output
Shown below is a sample output when the application is run, Please note that application prints in two UART consoles one after the other as two UART instances are configured. In UART console you need to enter 8 characters.
UART Console:
This is uart echo test DMA blocking mode
Receives 8 characters then echo's back. Please input..
12345678
All tests have passed!!