IPC RP Message Linux Echo
Introduction
This example shows usage of RP Message APIs to exchange messages between RTOS/NORTOS CPUs as well as exchange message with Linux on Cortex-A CPU.
In this example,
We create two RP Message end points
One end point to exchange messages with Linux kernel
One end point to exchange messages with Linux user space and other RTOS/NORTOS CPUs
All cores on startup after driver initialization first wait for Linux to be ready
Then they
announcethe end points on which they are waiting for messages to Linux.This is needed to be done else Linux cannot initiate message exchange with RTOS/NORTOS CPUs.
In case of remotecores, suspend task is created to enable graceful suspend in low power mode.
Two tasks are then created which listen for incoming messages and echo it back to the sender. The sender can be Linux CPU or other RTOS/NORTOS CPUs.
Meanwhile Linux kernel and user space test applications initiate message exchange with RTOS/NORTOS CPUs and wait for the echoed message.
The example also shows a “main” RTOS/NORTOS CPU exchanging message with other RTOS/NORTOS CPUs by sending messages to the same end point as that where LInux sends messages.
This shows that all CPUs can exchange messages with each other, no matter which OS or RTOS or NORTOS is running on the sender or receiver CPUs.
This example provides support for graceful shutdown of the remote core (MCU R5F). Refer Graceful shutdown of remote cores from Linux
This example provides support for MCU only low power mode support on the MCU core (MCU R5F)
This example provides support for other low power modes on the remote core (MCU R5F)
The example integrates bootloading functionality with SBL on OSPI bootmedia. It also integrates Device manager functionality. The SBL stage 2 thread boots all the cores along with HLOS like Linux. Refer SBL Booting Linux From OSPI for boot flow sequence.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
mcu-r5fss0-0 freertos |
CPU + OS |
wkup-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/ipc/ipc_rpmsg_echo_linux |
Steps to Run the Example
MCU only LPM
Attention
Low power mode is supported only on the Linux SPL boot flow. SBL bootflow does not support low power mode (LPM)
The following steps shows how to run MCU-only low power mode.
Set the wake up resume latency as 100ms for CPU0 on the linux kernel by running the following command. When the resume latency value is less, suspending the kernel will go to
MCU only sleep mode.$ echo 100000 > /sys/devices/system/cpu/cpu0/power/pm_qos_resume_latency_us
- Go to MCU only low power mode by running the following command on the linux.
$ echo mem > /sys/power/state
- After this the following message will appear on the MCU UART.
[IPC RPMSG ECHO] Next MCU mode is 1
[IPC RPMSG ECHO] Suspend request to MCU-only mode received [IPC RPMSG ECHO] Press a single key on this terminal to resume the kernel from MCU only mode
- Then type any key on the MCU UART to resume the kernel from LPM.
[IPC RPMSG ECHO] Key pressed. Notifying DM to wakeup main domain
[IPC RPMSG ECHO] Main domain resumed due to MCU UART
For detailed implementation of low power modes, refer Low power mode implementation of remote cores
This example integrates SBL on OSPI bootmedia which needs to be flashed on the EVM flash, along with sample application images for MCU R5 CPUs, HSM M4F and Linux Appimage.
For HS-FS device, use default_sbl_ospi_linux_hs_fs.cfg as the cfg file.
To flash to the EVM, refer to Flash a Hello World example .
Example, assuming SDK is installed at
C:/ti/mcu_plus_sdkand this example and IPC application is built using makefiles, and Linux Appimage is already created, in Windows,cd C:/ti/mcu_plus_sdk/tools/boot python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_ospi_linux_hs_fs.cfgIf Linux PC is used, assuming SDK is installed at
~/ti/mcu_plus_sdkcd ~/ti/mcu_plus_sdk python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_ospi_linux_hs_fs.cfgSwitch to OSPI NOR BOOT MODE and power on the EVM.
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
See Also
Sample Output
There is no direct output from the RTOS/NORTOS CPUs on the UART or CCS console. The output is seen on the Linux console on Cortex-A CPU.