Buildsheet

Introduction

Build Sheet of supported features and modules for this SDK release. The following table lists the supported features and modules for the corresponding category, along with the support status for RTOS on all the cores.

The support status is indicated by the following codes:

Code Note
Yes The feature or module is supported
No The feature or module is not supported
SDKx.y The feature or module will be supported in a future version of the SDK
NA The feature or module is not applicable in the hardware

Software Buildsheet

Category Module SubModule RTOS on MCU R5F RTOS on WKUP R5F
System Interconnect Bandwidth regulator No No
CBASS auto-clock gating No No
Initialization I2C Bootloader Operation No No
SPI Bootloader Operation No No
QSPI Bootloader Operation NOR NA No
NAND NA No
OSPI Bootloader Operation NOR NA Yes
NAND (1-bit mode) NA No
NAND (8-bit mode) NA No
GPMC Bootloader Operation NOR NA No
NAND NA No
Ethernet Bootloader Operation NA No
USB Bootloader Operation Host NA No
Device NA No
MMCSD Bootloader Operation SD Card (no UHS) NA Yes
eMMC NA Yes
UART Bootloader Operation NA Yes
Device Configuration Power Supply Modules POK No Yes
POR No No
PRG No No
PGD No No
VTM Yes Yes
PMIC (Power Management IC) Yes NA
Power Management Deep Sleep Low Power Mode NA NA
Deep Sleep LPM Wakeup Events RTC Timer NA NA
GT Timers NA NA
WKUP UART NA NA
I2C NA NA
MCU GPIO NA NA
I/O Daisy Chain NA NA
USB Connect/Disconnect NA NA
USB Remote Wakeup NA NA
MCU-Only Low Power Mode NA NA
Standby Low Power Mode NA NA
IO + DDR Low power mode NA NA
Partial I/O Low Power Mode NA NA
Boot-time OPP configurations No No
Runtime Power Management NA NA
DFS/CPUFreq NA NA
CPUIdle (A53 WFI) NA NA
CPUIdle (DDR in Self-Refresh) NA NA
Interprocessor Communication Mailbox Yes Yes
Spinlock No No
Memory Controllers DDR Subsystem (DDRSS) DDR4 No No
LPDDR4 No Yes
Inline ECC (1bit err) No Yes
Inline ECC (mbit err) No Yes
Region-based Address Translation Yes Yes
Time Sync Time Sync Module (CPTS) No No
Timer Manager No No
Time Sync and Compare Events No No
Data Movement Architecture (DMA) Data Movement Subsystem (DMSS) Yes Yes
Peripheral DMA (PDMA) No No
RingAcc Yes Yes
BCDMA Yes Yes
Packet Streaming Interface Link No No
General Connectivity Peripherals (MAIN domain) Multichannel Audio Serial Port (McASP) Input NA Yes
Output NA Yes
HDMI Output NA NA
General-Purpose Interface (GPIO) Yes Yes
Inter-Integrated Circuit (I2C) Controller Yes Yes
Target Yes Yes
Multichannel Serial Peripheral Interface (McSPI) Controller Yes Yes
Peripheral Yes Yes
Universal Asynchronous Receiver/Transmitter (UART) UART Yes Yes
RS-485 No No
IrDA No No
General Connectivity Peripherals (MCU domain) General-Purpose Interface (GPIO) Yes Yes
Inter-Integrated Circuit (I2C) Controller Yes Yes
Target Yes Yes
Multichannel Serial Peripheral Interface (McSPI) Controller Yes Yes
Peripheral Yes Yes
Universal Asynchronous Receiver/Transmitter (UART) UART Yes Yes
RS-485 No No
IrDA No No
General Connectivity Peripherals (WKUP domain) Inter-Integrated Circuit (I2C) Controller Yes Yes
Target Yes Yes
Universal Asynchronous Receiver/Transmitter (UART) UART No Yes
RS-485 No No
IrDA No No
High-speed Serial Interfaces Gigabit Ethernet Switch (CPSW3G) Switch No No
EndPoint No No
TSN No No
TSN - VLAN No No
Universal Serial Bus Subsystem (USBSS) Host 3.1 No No
Device 3.1 No No
Host 2.0 No No
Device 2.0 No No
Memory Interfaces Flash Subsystem (FSS) No No
Quad Serial Peripheral Interface (QSPI) NOR No No
NAND No No
Octal Serial Peripheral Interface (OSPI) NOR No Yes
NAND No No
Expanded Serial Peripheral Interface (xSPI) No No
General-Purpose Memory Controller (GPMC) FPGA No No
NAND No No
NOR No No
etc. No No
Error Location Module (ELM) No No
Multimedia Card Secure Digital (MMCSD) Interface SD Card Yes Yes
eMMC Yes Yes
Industrial & Control Interfaces Controller Area Network (MCAN) - MAIN domain CAN No Yes
CAN FD No Yes
Controller Area Network (MCAN) - MCU domain CAN Yes No
CAN FD Yes No
Enhanced Capture (ECAP) Module Capture No No
PWM Yes No
Enhanced Pulse Width Modulation (EPWM) Module Yes No
Enhanced Quadrature Encoder Pulse (EQEP) Module No No
Camera Subsystem Camera Streaming Interface Receiver (CSI_RX_IF) NA NA
MIPI D-PHY Receiver (DPHY_RX) NA NA
Multiple Camera NA NA
Timer Modules Global Timebase Cunter (GTC) No Yes
Windowed Watchdog Timer (WWDT) - MAIN domain No No
Windowed Watchdog Timer (WWDT) - MCU domain No No
Windowed Watchdog Timer (WWDT) - WKUP domain No Yes
Real-Time Clock (RTC) Yes Yes
Timers - MAIN domain Timer NA NA
Capture NA NA
Compare NA NA
PWM NA NA
Timers - MCU domain Timer Yes NA
Capture No NA
Compare No NA
PWM No NA
Timers - WKUP domain Timer NA Yes
Capture NA No
Compare NA No
PWM NA No
Internal Diagnostics Modules Dual Clock Comparator (DCC) Yes No
Error Signaling Module (ESM) Yes No
Memory Cyclic Redundancy Check (MCRC) Controller Yes No
SDL Driver Porting Layer(SDL DPL) Yes No
RTI(WWDG) Yes No
Voltage and Thermal Management(VTM) Yes No
Interconnect Isolation Gasket(STOG) Yes No
Interconnect Isolation Gasket(MTOG) Yes No
Power OK(POK) Yes No
PBIST(Built In Self Test) Yes No
ECC Aggregator Yes No
DISPLAY Subsystem Open LVDS Display Interface Transmitter (OLDITX) NA Yes
DISPLAY Parallel Interface (DPI) NA Yes
DSI (display serial interface) NA No
Triple Display NA No
Video Processing Unit Cnm Wave521CL NA No
Graphics Processing Unit IMG BXS NA No
On-Die Temperature sensor NA NA
On-Chip Debug NA NA
Crypto Accelerator (SA3UL) Advanced Encryption Standard (AES) AES-CBC NA NA
AES-ECB NA NA
SHA/MD5 Crypto Hardware-Accelerated Module (SHA/MD5) SHA-256 NA NA
SHA-512 NA NA
True Random Number Generator (TRNG) NA NA