MCAN Loopback Interrupt
Introduction
This example demonstrates the CAN message transmission and reception in digital loop back mode with the following configuration.
CAN FD Message Format.
Message ID Type is Standard, Msg Id 0xC0.
MCAN is configured in Interrupt Mode.
MCAN Interrupt Line Number 0.
Arbitration Bit Rate 1Mbps.
Data Bit Rate 5Mbps.
Buffer mode is used for Tx and RX to store message in message RAM.
Message is transmitted and received back internally using internal loopback mode. When the received message id and the data matches with the transmitted one, then the example is completed.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
mcu-r5fss0-0 freertos |
CPU + OS |
mcu-r5fss0-0 nortos |
CPU + OS |
wkup-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Boards |
am62px-sk |
Example folder |
examples/drivers/mcan/mcan_loopback_interrupt |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
Refer Flash a Hello World example for flashing the application.
See Also
Sample Output
Shown below is a sample output when the application is run,
[MCAN] Loopback Interrupt mode, application started ...
All tests have passed!!